<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [MX8QM]  HDMI Rx max resolution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX8QM-HDMI-Rx-max-resolution/m-p/1467321#M191054</link>
    <description>&lt;P&gt;Hi NXP Teams,&lt;/P&gt;&lt;P&gt;I saw following sharing about enabling HDMI Rx in iMX8QM platform :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-mx8qm-HDMI-RX/ta-p/1111058" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-mx8qm-HDMI-RX/ta-p/1111058&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX8QM-How-to-enable-the-HDMI-RX-on-L5-10-52-2-1-0-BSP/ta-p/1366982" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX8QM-How-to-enable-the-HDMI-RX-on-L5-10-52-2-1-0-BSP/ta-p/1366982&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I have a use-case to read 4K HDMI camera input and I would like to know if this could be supported by the aforementioned platform, please ?&lt;/P&gt;&lt;P&gt;Thanks in advance and best regards,&lt;/P&gt;&lt;P&gt;Khang&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Jun 2022 08:19:16 GMT</pubDate>
    <dc:creator>khang_letruong</dc:creator>
    <dc:date>2022-06-01T08:19:16Z</dc:date>
    <item>
      <title>[MX8QM]  HDMI Rx max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8QM-HDMI-Rx-max-resolution/m-p/1467321#M191054</link>
      <description>&lt;P&gt;Hi NXP Teams,&lt;/P&gt;&lt;P&gt;I saw following sharing about enabling HDMI Rx in iMX8QM platform :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-mx8qm-HDMI-RX/ta-p/1111058" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-mx8qm-HDMI-RX/ta-p/1111058&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX8QM-How-to-enable-the-HDMI-RX-on-L5-10-52-2-1-0-BSP/ta-p/1366982" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX8QM-How-to-enable-the-HDMI-RX-on-L5-10-52-2-1-0-BSP/ta-p/1366982&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I have a use-case to read 4K HDMI camera input and I would like to know if this could be supported by the aforementioned platform, please ?&lt;/P&gt;&lt;P&gt;Thanks in advance and best regards,&lt;/P&gt;&lt;P&gt;Khang&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Jun 2022 08:19:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8QM-HDMI-Rx-max-resolution/m-p/1467321#M191054</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2022-06-01T08:19:16Z</dc:date>
    </item>
    <item>
      <title>Re: [MX8QM]  HDMI Rx max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8QM-HDMI-Rx-max-resolution/m-p/1468946#M191159</link>
      <description>&lt;P&gt;Hi again,&lt;/P&gt;&lt;P&gt;I read from the RM of iMX8QM that HDMI Rx can support 4K2K 60Hz :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MX8QM_HDMI_Rx.png" style="width: 859px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/182236i8EB14498FEDB7656/image-size/large?v=v2&amp;amp;px=999" role="button" title="MX8QM_HDMI_Rx.png" alt="MX8QM_HDMI_Rx.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;MX8QM_HDMI_Rx.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But I am not sure what is the current status of BSP.&lt;/P&gt;&lt;P&gt;Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;As author of one of previous sharing about the subject, would you have any additional information to provide, please ?&lt;/P&gt;&lt;P&gt;Thanks in advance and best regards,&lt;/P&gt;&lt;P&gt;Khang.&lt;/P&gt;</description>
      <pubDate>Sat, 04 Jun 2022 06:37:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8QM-HDMI-Rx-max-resolution/m-p/1468946#M191159</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2022-06-04T06:37:35Z</dc:date>
    </item>
    <item>
      <title>Re: [MX8QM]  HDMI Rx max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8QM-HDMI-Rx-max-resolution/m-p/1468961#M191163</link>
      <description>&lt;P&gt;current bsp can support 4k@30&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 04 Jun 2022 14:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8QM-HDMI-Rx-max-resolution/m-p/1468961#M191163</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-06-04T14:22:03Z</dc:date>
    </item>
    <item>
      <title>Re: [MX8QM]  HDMI Rx max resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX8QM-HDMI-Rx-max-resolution/m-p/1468979#M191164</link>
      <description>&lt;P&gt;Thanks &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt; for the confirmation!&lt;/P&gt;&lt;P&gt;K.&lt;/P&gt;</description>
      <pubDate>Sun, 05 Jun 2022 05:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX8QM-HDMI-Rx-max-resolution/m-p/1468979#M191164</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2022-06-05T05:36:19Z</dc:date>
    </item>
  </channel>
</rss>