<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Kernel panic with vFat mount in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-with-vFat-mount/m-p/1467165#M191035</link>
    <description>&lt;P&gt;I use i.MX 8M Mini LPDDR4 EVK.&lt;/P&gt;&lt;P&gt;I use&amp;nbsp;Linux 5.4.70_2.3.6(BSP).&lt;/P&gt;&lt;P&gt;I'm booting with eMMC.&lt;/P&gt;&lt;P&gt;When I insert the vFat USB stick, I get the following kernel panic.&lt;/P&gt;&lt;P&gt;--------------------&lt;/P&gt;&lt;P&gt;[ 1911.296573] usb 1-1: new high-speed USB device number 2 using ci_hdrc&lt;BR /&gt;[ 1911.461156] usb-storage 1-1:1.0: USB Mass Storage device detected&lt;BR /&gt;[ 1911.468154] scsi host0: usb-storage 1-1:1.0&lt;BR /&gt;[ 1912.479225] scsi 0:0:0:0: Direct-Access BUFFALO USB Flash Disk 4000 PQ: 0 ANSI: 0 CCS&lt;BR /&gt;[ 1912.490919] sd 0:0:0:0: [sda] 4041728 512-byte logical blocks: (2.07 GB/1.93 GiB)&lt;BR /&gt;[ 1912.499167] sd 0:0:0:0: [sda] Write Protect is off&lt;BR /&gt;[ 1912.504658] sd 0:0:0:0: [sda] No Caching mode page found&lt;BR /&gt;[ 1912.510050] sd 0:0:0:0: [sda] Assuming drive cache: write through&lt;BR /&gt;[ 1912.643512] sda:&lt;BR /&gt;[ 1912.652791] sd 0:0:0:0: [sda] Attached SCSI removable disk&lt;BR /&gt;[ 1913.358298] sda:&lt;BR /&gt;[ 1913.438218] ------------[ cut here ]------------&lt;BR /&gt;[ 1913.442848] kernel BUG at arch/arm64/kernel/traps.c:405!&lt;BR /&gt;[ 1913.448165] Internal error: Oops - BUG: 0 [#1] PREEMPT SMP&lt;BR /&gt;[ 1913.453652] Modules linked in: crct10dif_ce gpio_ir_recv rc_core&lt;BR /&gt;[ 1913.459666] CPU: 2 PID: 544 Comm: mount Not tainted 5.4.70-2.3.2+g5693275abe2a #1&lt;BR /&gt;[ 1913.467147] Hardware name: FSL i.MX8MM EVK board (DT)&lt;BR /&gt;[ 1913.472196] pstate: 00000005 (nzcv daif -PAN -UAO)&lt;BR /&gt;[ 1913.476993] pc : do_undefinstr+0x2e4/0x308&lt;BR /&gt;[ 1913.481087] lr : do_undefinstr+0x1d8/0x308&lt;BR /&gt;[ 1913.485180] sp : ffff800012053b30&lt;BR /&gt;[ 1913.488492] x29: ffff800012053b30 x28: ffff00007ad07000&lt;BR /&gt;[ 1913.493802] x27: 0000000000000000 x26: 0000000000000000&lt;BR /&gt;[ 1913.499111] x25: ffff800010382f20 x24: 0000000000000000&lt;BR /&gt;[ 1913.504421] x23: 0000000060000005 x22: ffff800010380720&lt;BR /&gt;[ 1913.509731] x21: ffff800012053cd0 x20: ffff00007ad07000&lt;BR /&gt;[ 1913.515042] x19: ffff800012053b90 x18: 0000000000000000&lt;BR /&gt;[ 1913.520352] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[ 1913.525661] x15: ffffffffffffffff x14: 0000000000000000&lt;BR /&gt;[ 1913.530971] x13: 00000000000002a0 x12: 0000000000000020&lt;BR /&gt;[ 1913.536281] x11: 0101010101010101 x10: 0000000000000040&lt;BR /&gt;[ 1913.541592] x9 : 00000000fffffffe x8 : ffff00007b821bf0&lt;BR /&gt;[ 1913.546902] x7 : 0000000000000003 x6 : ffff800012053b88&lt;BR /&gt;[ 1913.552212] x5 : 00000000d5300000 x4 : ffff800011a14a10&lt;BR /&gt;[ 1913.557521] x3 : 0000000074700000 x2 : 0000000000000000&lt;BR /&gt;[ 1913.562831] x1 : ffff00007ad07000 x0 : 0000000060000005&lt;BR /&gt;[ 1913.568143] Call trace:&lt;BR /&gt;[ 1913.570590] do_undefinstr+0x2e4/0x308&lt;BR /&gt;[ 1913.574339] el1_undef+0x10/0x84&lt;BR /&gt;[ 1913.577568] fat_fill_super+0x0/0xc68&lt;BR /&gt;[ 1913.581230] mount_bdev+0x1a4/0x1d0&lt;BR /&gt;[ 1913.584717] vfat_mount+0x14/0x20&lt;BR /&gt;[ 1913.588032] legacy_get_tree+0x2c/0x58&lt;BR /&gt;[ 1913.591780] vfs_get_tree+0x24/0xe8&lt;BR /&gt;[ 1913.595268] do_mount+0x554/0x938&lt;BR /&gt;[ 1913.598582] ksys_mount+0x8c/0xe8&lt;BR /&gt;[ 1913.601896] __arm64_sys_mount+0x1c/0x28&lt;BR /&gt;[ 1913.605819] el0_svc_common.constprop.0+0x68/0x160&lt;BR /&gt;[ 1913.610608] el0_svc_handler+0x20/0x80&lt;BR /&gt;[ 1913.614355] el0_svc+0x8/0x208&lt;BR /&gt;[ 1913.617412] Code: f9401bf7 17ffff7d a9025bf5 f9001bf7 (d4210000)&lt;BR /&gt;[ 1913.623506] ---[ end trace 50fbefbfe78f1c91 ]---&lt;BR /&gt;[ 1913.628124] note: mount[544] exited with preempt_count 1&lt;BR /&gt;[ 1913.633989] ------------[ cut here ]------------&lt;BR /&gt;[ 1913.638626] WARNING: CPU: 2 PID: 0 at kernel/rcu/tree.c:569 rcu_idle_enter+0x78/0x80&lt;BR /&gt;[ 1913.646371] Modules linked in: crct10dif_ce gpio_ir_recv rc_core&lt;BR /&gt;[ 1913.652385] CPU: 2 PID: 0 Comm: swapper/2 Tainted: G D 5.4.70-2.3.2+g5693275abe2a #1&lt;BR /&gt;[ 1913.661427] Hardware name: FSL i.MX8MM EVK board (DT)&lt;BR /&gt;[ 1913.666478] pstate: 200003c5 (nzCv DAIF -PAN -UAO)&lt;BR /&gt;[ 1913.671270] pc : rcu_idle_enter+0x78/0x80&lt;BR /&gt;[ 1913.675280] lr : do_idle+0x1d0/0x280&lt;BR /&gt;[ 1913.678853] sp : ffff800011c83f20&lt;BR /&gt;[ 1913.682165] x29: ffff800011c83f20 x28: 0000000000000000&lt;BR /&gt;[ 1913.687475] x27: 0000000000000000 x26: ffff00007ac9c000&lt;BR /&gt;[ 1913.692785] x25: ffff00007fba2c00 x24: ffff800011a09218&lt;BR /&gt;[ 1913.698094] x23: ffff00007a0aaa00 x22: ffff800011804bf8&lt;BR /&gt;[ 1913.703404] x21: ffff800011a091f0 x20: 0000000000000002&lt;BR /&gt;[ 1913.708717] x19: ffff800011a09118 x18: 0000000000000010&lt;BR /&gt;[ 1913.714025] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[ 1913.719336] x15: 0000000000000073 x14: 0000000000000000&lt;BR /&gt;[ 1913.724646] x13: 0000000000000002 x12: 0000000000000073&lt;BR /&gt;[ 1913.729956] x11: 0000000000000001 x10: 000000000000089d&lt;BR /&gt;[ 1913.735267] x9 : ffff800011c83e80 x8 : ffff00007a0ab420&lt;BR /&gt;[ 1913.740577] x7 : 00000000000003fe x6 : 0000000392c65628&lt;BR /&gt;[ 1913.745887] x5 : 0000000000000dbb x4 : ffff80006e39e000&lt;BR /&gt;[ 1913.751198] x3 : 4000000000000002 x2 : 4000000000000000&lt;BR /&gt;[ 1913.756508] x1 : ffff800011808080 x0 : ffff00007fba6080&lt;BR /&gt;[ 1913.761818] Call trace:&lt;BR /&gt;[ 1913.764265] rcu_idle_enter+0x78/0x80&lt;BR /&gt;[ 1913.767924] do_idle+0x1d0/0x280&lt;BR /&gt;[ 1913.771151] cpu_startup_entry+0x20/0x80&lt;BR /&gt;[ 1913.775074] secondary_start_kernel+0x154/0x190&lt;BR /&gt;[ 1913.779603] ---[ end trace 50fbefbfe78f1c92 ]---&lt;/P&gt;&lt;P&gt;--------------------&lt;/P&gt;&lt;P&gt;When I insert the ext4 USB stick, there is no kernel panic.&lt;BR /&gt;Also, when the SD card is booted, the kernel panic does not occur even if the vFat USB memory is inserted.&lt;/P&gt;&lt;P&gt;Do you know what the cause is?&lt;/P&gt;</description>
    <pubDate>Wed, 01 Jun 2022 04:57:26 GMT</pubDate>
    <dc:creator>hiroki363</dc:creator>
    <dc:date>2022-06-01T04:57:26Z</dc:date>
    <item>
      <title>Kernel panic with vFat mount</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-with-vFat-mount/m-p/1467165#M191035</link>
      <description>&lt;P&gt;I use i.MX 8M Mini LPDDR4 EVK.&lt;/P&gt;&lt;P&gt;I use&amp;nbsp;Linux 5.4.70_2.3.6(BSP).&lt;/P&gt;&lt;P&gt;I'm booting with eMMC.&lt;/P&gt;&lt;P&gt;When I insert the vFat USB stick, I get the following kernel panic.&lt;/P&gt;&lt;P&gt;--------------------&lt;/P&gt;&lt;P&gt;[ 1911.296573] usb 1-1: new high-speed USB device number 2 using ci_hdrc&lt;BR /&gt;[ 1911.461156] usb-storage 1-1:1.0: USB Mass Storage device detected&lt;BR /&gt;[ 1911.468154] scsi host0: usb-storage 1-1:1.0&lt;BR /&gt;[ 1912.479225] scsi 0:0:0:0: Direct-Access BUFFALO USB Flash Disk 4000 PQ: 0 ANSI: 0 CCS&lt;BR /&gt;[ 1912.490919] sd 0:0:0:0: [sda] 4041728 512-byte logical blocks: (2.07 GB/1.93 GiB)&lt;BR /&gt;[ 1912.499167] sd 0:0:0:0: [sda] Write Protect is off&lt;BR /&gt;[ 1912.504658] sd 0:0:0:0: [sda] No Caching mode page found&lt;BR /&gt;[ 1912.510050] sd 0:0:0:0: [sda] Assuming drive cache: write through&lt;BR /&gt;[ 1912.643512] sda:&lt;BR /&gt;[ 1912.652791] sd 0:0:0:0: [sda] Attached SCSI removable disk&lt;BR /&gt;[ 1913.358298] sda:&lt;BR /&gt;[ 1913.438218] ------------[ cut here ]------------&lt;BR /&gt;[ 1913.442848] kernel BUG at arch/arm64/kernel/traps.c:405!&lt;BR /&gt;[ 1913.448165] Internal error: Oops - BUG: 0 [#1] PREEMPT SMP&lt;BR /&gt;[ 1913.453652] Modules linked in: crct10dif_ce gpio_ir_recv rc_core&lt;BR /&gt;[ 1913.459666] CPU: 2 PID: 544 Comm: mount Not tainted 5.4.70-2.3.2+g5693275abe2a #1&lt;BR /&gt;[ 1913.467147] Hardware name: FSL i.MX8MM EVK board (DT)&lt;BR /&gt;[ 1913.472196] pstate: 00000005 (nzcv daif -PAN -UAO)&lt;BR /&gt;[ 1913.476993] pc : do_undefinstr+0x2e4/0x308&lt;BR /&gt;[ 1913.481087] lr : do_undefinstr+0x1d8/0x308&lt;BR /&gt;[ 1913.485180] sp : ffff800012053b30&lt;BR /&gt;[ 1913.488492] x29: ffff800012053b30 x28: ffff00007ad07000&lt;BR /&gt;[ 1913.493802] x27: 0000000000000000 x26: 0000000000000000&lt;BR /&gt;[ 1913.499111] x25: ffff800010382f20 x24: 0000000000000000&lt;BR /&gt;[ 1913.504421] x23: 0000000060000005 x22: ffff800010380720&lt;BR /&gt;[ 1913.509731] x21: ffff800012053cd0 x20: ffff00007ad07000&lt;BR /&gt;[ 1913.515042] x19: ffff800012053b90 x18: 0000000000000000&lt;BR /&gt;[ 1913.520352] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[ 1913.525661] x15: ffffffffffffffff x14: 0000000000000000&lt;BR /&gt;[ 1913.530971] x13: 00000000000002a0 x12: 0000000000000020&lt;BR /&gt;[ 1913.536281] x11: 0101010101010101 x10: 0000000000000040&lt;BR /&gt;[ 1913.541592] x9 : 00000000fffffffe x8 : ffff00007b821bf0&lt;BR /&gt;[ 1913.546902] x7 : 0000000000000003 x6 : ffff800012053b88&lt;BR /&gt;[ 1913.552212] x5 : 00000000d5300000 x4 : ffff800011a14a10&lt;BR /&gt;[ 1913.557521] x3 : 0000000074700000 x2 : 0000000000000000&lt;BR /&gt;[ 1913.562831] x1 : ffff00007ad07000 x0 : 0000000060000005&lt;BR /&gt;[ 1913.568143] Call trace:&lt;BR /&gt;[ 1913.570590] do_undefinstr+0x2e4/0x308&lt;BR /&gt;[ 1913.574339] el1_undef+0x10/0x84&lt;BR /&gt;[ 1913.577568] fat_fill_super+0x0/0xc68&lt;BR /&gt;[ 1913.581230] mount_bdev+0x1a4/0x1d0&lt;BR /&gt;[ 1913.584717] vfat_mount+0x14/0x20&lt;BR /&gt;[ 1913.588032] legacy_get_tree+0x2c/0x58&lt;BR /&gt;[ 1913.591780] vfs_get_tree+0x24/0xe8&lt;BR /&gt;[ 1913.595268] do_mount+0x554/0x938&lt;BR /&gt;[ 1913.598582] ksys_mount+0x8c/0xe8&lt;BR /&gt;[ 1913.601896] __arm64_sys_mount+0x1c/0x28&lt;BR /&gt;[ 1913.605819] el0_svc_common.constprop.0+0x68/0x160&lt;BR /&gt;[ 1913.610608] el0_svc_handler+0x20/0x80&lt;BR /&gt;[ 1913.614355] el0_svc+0x8/0x208&lt;BR /&gt;[ 1913.617412] Code: f9401bf7 17ffff7d a9025bf5 f9001bf7 (d4210000)&lt;BR /&gt;[ 1913.623506] ---[ end trace 50fbefbfe78f1c91 ]---&lt;BR /&gt;[ 1913.628124] note: mount[544] exited with preempt_count 1&lt;BR /&gt;[ 1913.633989] ------------[ cut here ]------------&lt;BR /&gt;[ 1913.638626] WARNING: CPU: 2 PID: 0 at kernel/rcu/tree.c:569 rcu_idle_enter+0x78/0x80&lt;BR /&gt;[ 1913.646371] Modules linked in: crct10dif_ce gpio_ir_recv rc_core&lt;BR /&gt;[ 1913.652385] CPU: 2 PID: 0 Comm: swapper/2 Tainted: G D 5.4.70-2.3.2+g5693275abe2a #1&lt;BR /&gt;[ 1913.661427] Hardware name: FSL i.MX8MM EVK board (DT)&lt;BR /&gt;[ 1913.666478] pstate: 200003c5 (nzCv DAIF -PAN -UAO)&lt;BR /&gt;[ 1913.671270] pc : rcu_idle_enter+0x78/0x80&lt;BR /&gt;[ 1913.675280] lr : do_idle+0x1d0/0x280&lt;BR /&gt;[ 1913.678853] sp : ffff800011c83f20&lt;BR /&gt;[ 1913.682165] x29: ffff800011c83f20 x28: 0000000000000000&lt;BR /&gt;[ 1913.687475] x27: 0000000000000000 x26: ffff00007ac9c000&lt;BR /&gt;[ 1913.692785] x25: ffff00007fba2c00 x24: ffff800011a09218&lt;BR /&gt;[ 1913.698094] x23: ffff00007a0aaa00 x22: ffff800011804bf8&lt;BR /&gt;[ 1913.703404] x21: ffff800011a091f0 x20: 0000000000000002&lt;BR /&gt;[ 1913.708717] x19: ffff800011a09118 x18: 0000000000000010&lt;BR /&gt;[ 1913.714025] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[ 1913.719336] x15: 0000000000000073 x14: 0000000000000000&lt;BR /&gt;[ 1913.724646] x13: 0000000000000002 x12: 0000000000000073&lt;BR /&gt;[ 1913.729956] x11: 0000000000000001 x10: 000000000000089d&lt;BR /&gt;[ 1913.735267] x9 : ffff800011c83e80 x8 : ffff00007a0ab420&lt;BR /&gt;[ 1913.740577] x7 : 00000000000003fe x6 : 0000000392c65628&lt;BR /&gt;[ 1913.745887] x5 : 0000000000000dbb x4 : ffff80006e39e000&lt;BR /&gt;[ 1913.751198] x3 : 4000000000000002 x2 : 4000000000000000&lt;BR /&gt;[ 1913.756508] x1 : ffff800011808080 x0 : ffff00007fba6080&lt;BR /&gt;[ 1913.761818] Call trace:&lt;BR /&gt;[ 1913.764265] rcu_idle_enter+0x78/0x80&lt;BR /&gt;[ 1913.767924] do_idle+0x1d0/0x280&lt;BR /&gt;[ 1913.771151] cpu_startup_entry+0x20/0x80&lt;BR /&gt;[ 1913.775074] secondary_start_kernel+0x154/0x190&lt;BR /&gt;[ 1913.779603] ---[ end trace 50fbefbfe78f1c92 ]---&lt;/P&gt;&lt;P&gt;--------------------&lt;/P&gt;&lt;P&gt;When I insert the ext4 USB stick, there is no kernel panic.&lt;BR /&gt;Also, when the SD card is booted, the kernel panic does not occur even if the vFat USB memory is inserted.&lt;/P&gt;&lt;P&gt;Do you know what the cause is?&lt;/P&gt;</description>
      <pubDate>Wed, 01 Jun 2022 04:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-with-vFat-mount/m-p/1467165#M191035</guid>
      <dc:creator>hiroki363</dc:creator>
      <dc:date>2022-06-01T04:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel panic with vFat mount</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-with-vFat-mount/m-p/1474087#M191500</link>
      <description>&lt;P&gt;Can you try the L5.15.5 BSP? This issue could releate to kernel process schedule.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 05:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-with-vFat-mount/m-p/1474087#M191500</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-06-15T05:10:12Z</dc:date>
    </item>
  </channel>
</rss>