<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MMC init failed while rebooting i.mx6ull in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMC-init-failed-while-rebooting-i-mx6ull/m-p/1466754#M191007</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;MMC init is failing in uboot, when reboot is done by software.&lt;/P&gt;&lt;P&gt;Logs are as follows,&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;P&gt;Rebooting... reboot: Restarting system&lt;/P&gt;&lt;P&gt;U-Boot 2016.03-g0365239-dirty (Sep 14 2021 - 12:25:51 +0530)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6ULL rev1.1 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 46C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;u-boot revision: 9.00.04 compiled on 20-July-2021&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;board_init&lt;BR /&gt;MMC: board_mmc_init&lt;BR /&gt;FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;*** Warning - MMC init failed, using default environment&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;**********do_enable_parallel_lcd*****************&lt;BR /&gt;Display: TFT43AB (1024x600)&lt;BR /&gt;Video: 1024x600x24&lt;BR /&gt;CONFIG_SPLASH_SCREEN&lt;BR /&gt;In CONFIG_SPLASH_SCREEN_ALIGN&lt;BR /&gt;In CONFIG_SPLASH_SCREEN_ALIGN&lt;BR /&gt;CONFIG_SPLASH_SCREEN_ALIGN&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;board_late_init&lt;BR /&gt;Net: FEC1&lt;BR /&gt;Error: FEC1 address not set.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;Not valid image format for Authentication, Please check&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Tue, 31 May 2022 10:59:05 GMT</pubDate>
    <dc:creator>nikhilmm</dc:creator>
    <dc:date>2022-05-31T10:59:05Z</dc:date>
    <item>
      <title>MMC init failed while rebooting i.mx6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMC-init-failed-while-rebooting-i-mx6ull/m-p/1466754#M191007</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;MMC init is failing in uboot, when reboot is done by software.&lt;/P&gt;&lt;P&gt;Logs are as follows,&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;P&gt;Rebooting... reboot: Restarting system&lt;/P&gt;&lt;P&gt;U-Boot 2016.03-g0365239-dirty (Sep 14 2021 - 12:25:51 +0530)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6ULL rev1.1 528 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 46C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;u-boot revision: 9.00.04 compiled on 20-July-2021&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;board_init&lt;BR /&gt;MMC: board_mmc_init&lt;BR /&gt;FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;*** Warning - MMC init failed, using default environment&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;**********do_enable_parallel_lcd*****************&lt;BR /&gt;Display: TFT43AB (1024x600)&lt;BR /&gt;Video: 1024x600x24&lt;BR /&gt;CONFIG_SPLASH_SCREEN&lt;BR /&gt;In CONFIG_SPLASH_SCREEN_ALIGN&lt;BR /&gt;In CONFIG_SPLASH_SCREEN_ALIGN&lt;BR /&gt;CONFIG_SPLASH_SCREEN_ALIGN&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;board_late_init&lt;BR /&gt;Net: FEC1&lt;BR /&gt;Error: FEC1 address not set.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;board_mmc_getcd&lt;BR /&gt;MMC: no card present&lt;BR /&gt;Not valid image format for Authentication, Please check&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 31 May 2022 10:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMC-init-failed-while-rebooting-i-mx6ull/m-p/1466754#M191007</guid>
      <dc:creator>nikhilmm</dc:creator>
      <dc:date>2022-05-31T10:59:05Z</dc:date>
    </item>
  </channel>
</rss>