<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 USB Video class Composite Device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Video-class-Composite-Device/m-p/1466374#M190983</link>
    <description>&lt;P&gt;Hello community! I got a question. For a UVC composite device with Color and sensor Camera, do I need more than 1 Video Control Descriptor? Im not sure If I simply can add the inteface and endpoint for the second camera and still use one video control of if it is needed to use two video control descriptor.&lt;/P&gt;</description>
    <pubDate>Mon, 30 May 2022 17:29:13 GMT</pubDate>
    <dc:creator>Ismael_dz</dc:creator>
    <dc:date>2022-05-30T17:29:13Z</dc:date>
    <item>
      <title>USB Video class Composite Device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Video-class-Composite-Device/m-p/1466374#M190983</link>
      <description>&lt;P&gt;Hello community! I got a question. For a UVC composite device with Color and sensor Camera, do I need more than 1 Video Control Descriptor? Im not sure If I simply can add the inteface and endpoint for the second camera and still use one video control of if it is needed to use two video control descriptor.&lt;/P&gt;</description>
      <pubDate>Mon, 30 May 2022 17:29:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Video-class-Composite-Device/m-p/1466374#M190983</guid>
      <dc:creator>Ismael_dz</dc:creator>
      <dc:date>2022-05-30T17:29:13Z</dc:date>
    </item>
    <item>
      <title>Re: USB Video class Composite Device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Video-class-Composite-Device/m-p/1467005#M191024</link>
      <description>&lt;P&gt;Hello, Ismael_dz&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you mean UVC class device streaming two videos simultaneously? UVC class allows many video sensors (sources) in one device but streaming just a single one at a time. Selector interface allows switching among sources. But there are no means to define two or more simultaneous video streams. That's for standard UVC device, which is recognized by built-in Windows driver.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 31 May 2022 21:09:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Video-class-Composite-Device/m-p/1467005#M191024</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2022-05-31T21:09:33Z</dc:date>
    </item>
  </channel>
</rss>