<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT106 MII Ethernet Interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-MII-Ethernet-Interface/m-p/1465794#M190921</link>
    <description>&lt;P&gt;i want to start working with ethernet interface on my mimxrt106 board.&lt;/P&gt;&lt;P&gt;i am using LAN8720 ethernet IC.&lt;/P&gt;&lt;P&gt;could you suggest me a starting point?&amp;nbsp; which SDK example can i use for a simple MII interface communication.&lt;/P&gt;</description>
    <pubDate>Sat, 28 May 2022 06:53:21 GMT</pubDate>
    <dc:creator>accatpaliz</dc:creator>
    <dc:date>2022-05-28T06:53:21Z</dc:date>
    <item>
      <title>MIMXRT106 MII Ethernet Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-MII-Ethernet-Interface/m-p/1465794#M190921</link>
      <description>&lt;P&gt;i want to start working with ethernet interface on my mimxrt106 board.&lt;/P&gt;&lt;P&gt;i am using LAN8720 ethernet IC.&lt;/P&gt;&lt;P&gt;could you suggest me a starting point?&amp;nbsp; which SDK example can i use for a simple MII interface communication.&lt;/P&gt;</description>
      <pubDate>Sat, 28 May 2022 06:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-MII-Ethernet-Interface/m-p/1465794#M190921</guid>
      <dc:creator>accatpaliz</dc:creator>
      <dc:date>2022-05-28T06:53:21Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT106 MII Ethernet Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-MII-Ethernet-Interface/m-p/1465888#M190940</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Could you suggest me a starting point? which SDK example can i use for a simple MII interface communication.&lt;BR /&gt;-- Unfortunately, there's no similar demo in the SDK library for you to refer to directly actually, and you may need to refer to its datasheet as a start to design either hardware connection or software driver.&lt;BR /&gt;In my opinion, I'd like to suggest you choose the RMII interface instead of the MII interface, then it definitely can accelerate the design process, as there are many tutorials for referring to.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 30 May 2022 02:17:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-MII-Ethernet-Interface/m-p/1465888#M190940</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-05-30T02:17:10Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT106 MII Ethernet Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-MII-Ethernet-Interface/m-p/1466217#M190972</link>
      <description>&lt;P&gt;thanks. yes actually i used RMII . after i posted the question, i found an example named evkmimxrt106_enet_rxtx_transfer . i guess it can help me. now i am working on this project to migrate from QSPI flash to hyper flash . so it could run on my dev board with a hyper flash ic.&lt;/P&gt;</description>
      <pubDate>Mon, 30 May 2022 10:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-MII-Ethernet-Interface/m-p/1466217#M190972</guid>
      <dc:creator>accatpaliz</dc:creator>
      <dc:date>2022-05-30T10:35:36Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT106 MII Ethernet Interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-MII-Ethernet-Interface/m-p/1466458#M190988</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;I hope the &lt;A href="https://community.nxp.com/t5/i-MX-RT/Porting-LAN8720-to-IMXRT1060-but-AutoNegotiation-is-failed/td-p/1459643" target="_self"&gt;post&lt;/A&gt; can provide some insight for you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 31 May 2022 01:54:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106-MII-Ethernet-Interface/m-p/1466458#M190988</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-05-31T01:54:08Z</dc:date>
    </item>
  </channel>
</rss>