<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic is there any example code for using opengl in i.mx6 platform, especially involving galcore module? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/is-there-any-example-code-for-using-opengl-in-i-mx6-platform/m-p/1464779#M190871</link>
    <description>&lt;P&gt;Hello, I try to write a simple demo for opengl learning with libEGL and libGLESv2.&lt;/P&gt;&lt;P&gt;When I nm the libEGL.so, I found the there are some functions, e.g: gcoOS_GetDisplayByIndex, defined in the galcore module (/usr/include/HAL/gc_hal_eglplatform.h). What is this module usefor?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can use /dev/fb0, and I know there is a fbdev EGL implementation which contains functions like fbXxx, e.g: fbGetDisplayByIndex(int index). What's the difference between fbGetDisplayByIndex and&amp;nbsp;gcoOS_GetDisplayByIndex？&lt;/P&gt;</description>
    <pubDate>Thu, 26 May 2022 12:30:57 GMT</pubDate>
    <dc:creator>doerthous</dc:creator>
    <dc:date>2022-05-26T12:30:57Z</dc:date>
    <item>
      <title>is there any example code for using opengl in i.mx6 platform, especially involving galcore module?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/is-there-any-example-code-for-using-opengl-in-i-mx6-platform/m-p/1464779#M190871</link>
      <description>&lt;P&gt;Hello, I try to write a simple demo for opengl learning with libEGL and libGLESv2.&lt;/P&gt;&lt;P&gt;When I nm the libEGL.so, I found the there are some functions, e.g: gcoOS_GetDisplayByIndex, defined in the galcore module (/usr/include/HAL/gc_hal_eglplatform.h). What is this module usefor?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can use /dev/fb0, and I know there is a fbdev EGL implementation which contains functions like fbXxx, e.g: fbGetDisplayByIndex(int index). What's the difference between fbGetDisplayByIndex and&amp;nbsp;gcoOS_GetDisplayByIndex？&lt;/P&gt;</description>
      <pubDate>Thu, 26 May 2022 12:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/is-there-any-example-code-for-using-opengl-in-i-mx6-platform/m-p/1464779#M190871</guid>
      <dc:creator>doerthous</dc:creator>
      <dc:date>2022-05-26T12:30:57Z</dc:date>
    </item>
  </channel>
</rss>