<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx8mp ecspi slave mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ecspi-slave-mode/m-p/1464541#M190852</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi All&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am currently working on imx8mp ECSPI-Slave and&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;I am able to communicate with Master.&lt;/STRONG&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;My test program runs on the M7 core side, the SDK version I use is SDK_2_11_1_EVK-MIMx8mp. I am suitable to configure imx8MP ecspi2(bursh_length=8) with the default slave parameter and enable RxFifoReady interrupt to ECSPI.&lt;/SPAN&gt;&lt;SPAN class=""&gt; When the master sends eight bytes (0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88) to the slave,&lt;/SPAN&gt;&lt;SPAN class=""&gt; The data received by the slave is 0x00,0x00,0x00,0x11, 0x22, 0x33, 0x44, 0x55. The first three bytes received are all 0x00.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;When I change the default configuration of the slave(set bursh_length to 32), the data received by the slave is 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88.&lt;/SPAN&gt;&lt;SPAN class=""&gt; I do not know why can appear this kind of circumstance, hope the expert gives explanation, thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;If I want to configure slave to receive byte by byte, how should I configure it?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 26 May 2022 07:00:51 GMT</pubDate>
    <dc:creator>guangwei</dc:creator>
    <dc:date>2022-05-26T07:00:51Z</dc:date>
    <item>
      <title>imx8mp ecspi slave mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ecspi-slave-mode/m-p/1464541#M190852</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi All&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am currently working on imx8mp ECSPI-Slave and&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;I am able to communicate with Master.&lt;/STRONG&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;My test program runs on the M7 core side, the SDK version I use is SDK_2_11_1_EVK-MIMx8mp. I am suitable to configure imx8MP ecspi2(bursh_length=8) with the default slave parameter and enable RxFifoReady interrupt to ECSPI.&lt;/SPAN&gt;&lt;SPAN class=""&gt; When the master sends eight bytes (0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88) to the slave,&lt;/SPAN&gt;&lt;SPAN class=""&gt; The data received by the slave is 0x00,0x00,0x00,0x11, 0x22, 0x33, 0x44, 0x55. The first three bytes received are all 0x00.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;When I change the default configuration of the slave(set bursh_length to 32), the data received by the slave is 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88.&lt;/SPAN&gt;&lt;SPAN class=""&gt; I do not know why can appear this kind of circumstance, hope the expert gives explanation, thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;If I want to configure slave to receive byte by byte, how should I configure it?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 May 2022 07:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ecspi-slave-mode/m-p/1464541#M190852</guid>
      <dc:creator>guangwei</dc:creator>
      <dc:date>2022-05-26T07:00:51Z</dc:date>
    </item>
  </channel>
</rss>