<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8 PWM source clock frequency</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-PWM-source-clock-frequency/m-p/1464478#M190848</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/132235"&gt;@eoin_oconnell&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The behavior you mentioned is odd. But from the device tree node, it looks like the node is defined properly and the PWM should work fine.&lt;/P&gt;
&lt;P&gt;There might be a few possible reasons for this kind of behavior. To debug more, can you provide me with the following details?&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;What values are you setting in the period and duty_cycle values?&lt;/LI&gt;
&lt;LI&gt;How are you measuring the frequency at the PWM_OUT pin?&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
    <pubDate>Thu, 26 May 2022 05:15:54 GMT</pubDate>
    <dc:creator>Dhruvit</dc:creator>
    <dc:date>2022-05-26T05:15:54Z</dc:date>
    <item>
      <title>IMX8 PWM source clock frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-PWM-source-clock-frequency/m-p/1462532#M190725</link>
      <description>&lt;P&gt;I am using the Toradex Verdin IMX8MP module and I need to generate a clock frequency of&amp;nbsp; 1-3MHz from the PWM output pin.&lt;/P&gt;&lt;P&gt;I can currently get it to aroud 500kHz but after that the PWM peripheral does not behave at all even though the correct numbers are being written to the period and duty cycle registers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why am I observing this behaviour? For example when I try to put duty cycle to 10 and period to 20 in the registers I suddenly get a period of around 20ms and not 1-2us.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My PWM has a source clock of 24MHz, how can I change the PWM clock frequency, the datasheet shows it supports a number of different input sources, but where can I edit this source in the device tree?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My dt base for the pwm looks like this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;			pwm2: pwm@30670000 {
				compatible = "fsl,imx8mp-pwm", "fsl,imx27-pwm";
				reg = &amp;lt;0x30670000 0x10000&amp;gt;;
				interrupts = &amp;lt;GIC_SPI 82 IRQ_TYPE_LEVEL_HIGH&amp;gt;;
				clocks = &amp;lt;&amp;amp;clk IMX8MP_CLK_PWM2_ROOT&amp;gt;,
					 &amp;lt;&amp;amp;clk IMX8MP_CLK_PWM2_ROOT&amp;gt;;
				clock-names = "ipg", "per";
				#pwm-cells = &amp;lt;2&amp;gt;;
				status = "disabled";
			};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The pwm get enabled higher in the DT, how can I select the other sources it supports?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;According to the reference manual page 242 i can select these with a max of 66MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="372"&gt;&lt;SPAN class=""&gt;000 - 24M_REF_CLK&lt;BR /&gt;010 - SYSTEM_PLL1_DIV5&lt;BR /&gt;110 - SYSTEM_PLL1_DIV10&lt;BR /&gt;011 - SYSTEM_PLL1_DIV20&lt;BR /&gt;001 - SYSTEM_PLL2_DIV10&lt;BR /&gt;100 - SYSTEM_PLL3_CLK&lt;BR /&gt;111 - VIDEO_PLL_CLK&lt;BR /&gt;101 - EXT_CLK_1&lt;/SPAN&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 14:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-PWM-source-clock-frequency/m-p/1462532#M190725</guid>
      <dc:creator>eoin_oconnell</dc:creator>
      <dc:date>2022-05-23T14:44:23Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 PWM source clock frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-PWM-source-clock-frequency/m-p/1464478#M190848</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/132235"&gt;@eoin_oconnell&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The behavior you mentioned is odd. But from the device tree node, it looks like the node is defined properly and the PWM should work fine.&lt;/P&gt;
&lt;P&gt;There might be a few possible reasons for this kind of behavior. To debug more, can you provide me with the following details?&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;What values are you setting in the period and duty_cycle values?&lt;/LI&gt;
&lt;LI&gt;How are you measuring the frequency at the PWM_OUT pin?&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Dhruvit.&lt;/P&gt;</description>
      <pubDate>Thu, 26 May 2022 05:15:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-PWM-source-clock-frequency/m-p/1464478#M190848</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2022-05-26T05:15:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 PWM source clock frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-PWM-source-clock-frequency/m-p/1526072#M195456</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/132235"&gt;@eoin_oconnell&lt;/a&gt;, I am running into the same issue you were. Did you find a solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is greatly appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 18:28:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-PWM-source-clock-frequency/m-p/1526072#M195456</guid>
      <dc:creator>embeddeddan</dc:creator>
      <dc:date>2022-09-21T18:28:18Z</dc:date>
    </item>
    <item>
      <title>回复： IMX8 PWM source clock frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-PWM-source-clock-frequency/m-p/1961384#M228886</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Greetings,&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;I have a similar problem.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;After I set the PWM output, if the frequency is set to 8KHZ, period = 125000, duty_cycle = 62000, then the output is a square wave. If set to 8MHZ then the output is sine wave,period = 125, duty_cycle = 62.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;Can you help me find out what the reason is? Thank you!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Sep 2024 06:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-PWM-source-clock-frequency/m-p/1961384#M228886</guid>
      <dc:creator>lpheni</dc:creator>
      <dc:date>2024-09-25T06:30:26Z</dc:date>
    </item>
  </channel>
</rss>