<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: fail during Mfgtool download in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/fail-during-Mfgtool-download/m-p/1463993#M190828</link>
    <description>&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;the board stop "starting kernel......" in serial console during download by mfgtool.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Boot from USB for mfgtools&lt;BR /&gt;Use default environment for mfgtools&lt;BR /&gt;Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt; run bootcmd_mfg&lt;BR /&gt;Kernel image @ 0x12000000 [ 0x000000 - 0x53d8d0 ]&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 12c00000 ...&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-imx6&lt;BR /&gt;Image Type: ARM Linux RAMDisk Image (gzip compressed)&lt;BR /&gt;Data Size: 18729449 Bytes = 17.9 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 18000000&lt;BR /&gt;Booting using the fdt blob at 0x18000000&lt;BR /&gt;Using Device Tree in place at 18000000, end 1800d22d&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;I burn other boards(different circuits and same DDR,PM）with same mfgtools.they are fine&lt;/P&gt;</description>
    <pubDate>Wed, 25 May 2022 12:02:55 GMT</pubDate>
    <dc:creator>sethhorus</dc:creator>
    <dc:date>2022-05-25T12:02:55Z</dc:date>
    <item>
      <title>fail during Mfgtool download</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fail-during-Mfgtool-download/m-p/1463244#M190774</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; I design a imx6q&amp;nbsp;circuit board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; I try firmware download by mfgtool,but stop "Jumping to OS Image".I can see uboot information and board stop "starting kernel......" in serial console. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; I use "DDR test tool V3" to stress test.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; Pass DDR Stress test.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; I really don't know whats wrong and need help.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 12:26:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fail-during-Mfgtool-download/m-p/1463244#M190774</guid>
      <dc:creator>sethhorus</dc:creator>
      <dc:date>2022-05-24T12:26:23Z</dc:date>
    </item>
    <item>
      <title>Re: fail during Mfgtool download</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fail-during-Mfgtool-download/m-p/1463986#M190827</link>
      <description>&lt;P&gt;THE DDR STRESS TEST IS FINE&lt;/P&gt;&lt;P&gt;enter desired START freq (135 to 672 MHz), then hit enter.&lt;BR /&gt;Note: DDR3 minimum is ~333MHz, do not recommend to go too much below this.&lt;BR /&gt;528&lt;BR /&gt;The freq you entered was: 528&lt;/P&gt;&lt;P&gt;Enter desired END freq (135 to 672 MHz), then hit enter.&lt;BR /&gt;Make sure this is equal to or greater than start freq&lt;BR /&gt;528&lt;BR /&gt;The freq you entered was: 528&lt;/P&gt;&lt;P&gt;Beginning stress test&lt;/P&gt;&lt;P&gt;loop: 1&lt;BR /&gt;DDR Freq: 528 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;t0: memcpy10 SSN x64 test&lt;BR /&gt;t1: memcpy8 SSN x64 test&lt;BR /&gt;t2: byte-wise SSN x64 test&lt;BR /&gt;t3: memcpy11 random pattern test&lt;BR /&gt;t4: IRAM_to_DDRv2 test&lt;BR /&gt;t5: IRAM_to_DDRv1 test&lt;BR /&gt;t6: read noise walking ones and zeros test&lt;/P&gt;&lt;P&gt;loop: 2&lt;BR /&gt;DDR Freq: 528 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;t0: memcpy10 SSN x64 test&lt;BR /&gt;t1: memcpy8 SSN x64 test&lt;BR /&gt;t2: byte-wise SSN x64 test&lt;BR /&gt;t3: memcpy11 random pattern test&lt;BR /&gt;t4: IRAM_to_DDRv2 test&lt;BR /&gt;t5: IRAM_to_DDRv1 test&lt;BR /&gt;t6: read noise walking ones and zeros test&lt;/P&gt;&lt;P&gt;loop: 3&lt;BR /&gt;DDR Freq: 528 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;t0: memcpy10 SSN x64 test&lt;BR /&gt;t1: memcpy8 SSN x64 test&lt;BR /&gt;t2: byte-wise SSN x64 test&lt;BR /&gt;t3: memcpy11 random pattern test&lt;BR /&gt;t4: IRAM_to_DDRv2 test&lt;BR /&gt;t5: IRAM_to_DDRv1 test&lt;BR /&gt;t6: read noise walking ones and zeros test&lt;/P&gt;&lt;P&gt;loop: 4&lt;BR /&gt;DDR Freq: 528 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;t0: memcpy10 SSN x64 test&lt;BR /&gt;t1: memcpy8 SSN x64 test&lt;BR /&gt;t2: byte-wise SSN x64 test&lt;BR /&gt;t3: memcpy11 random pattern test&lt;BR /&gt;t4: IRAM_to_DDRv2 test&lt;BR /&gt;t5: IRAM_to_DDRv1 test&lt;BR /&gt;t6: read noise walking ones and zeros test&lt;/P&gt;&lt;P&gt;loop: 5&lt;BR /&gt;DDR Freq: 528 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;t0: memcpy10 SSN x64 test&lt;BR /&gt;t1: memcpy8 SSN x64 test&lt;BR /&gt;t2: byte-wise SSN x64 test&lt;BR /&gt;t3: memcpy11 random pattern test&lt;BR /&gt;t4: IRAM_to_DDRv2 test&lt;BR /&gt;t5: IRAM_to_DDRv1 test&lt;BR /&gt;t6: read noise walking ones and zeros test&lt;/P&gt;&lt;P&gt;loop: 6&lt;BR /&gt;DDR Freq: 528 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;t0: memcpy10 SSN x64 test&lt;BR /&gt;t1: memcpy8 SSN x64 test&lt;BR /&gt;t2: byte-wise SSN x64 test&lt;BR /&gt;t3: memcpy11 random pattern test&lt;BR /&gt;t4: IRAM_to_DDRv2 test&lt;BR /&gt;t5: IRAM_to_DDRv1 test&lt;BR /&gt;t6: read noise walking ones and zeros test&lt;/P&gt;&lt;P&gt;loop: 7&lt;BR /&gt;DDR Freq: 528 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;t0: memcpy10 SSN x64 test&lt;BR /&gt;t1: memcpy8 SSN x64 test&lt;BR /&gt;t2: byte-wise SSN x64 test&lt;BR /&gt;t3: memcpy11 random pattern test&lt;BR /&gt;t4: IRAM_to_DDRv2 test&lt;BR /&gt;t5: IRAM_to_DDRv1 test&lt;BR /&gt;t6: read noise walking ones and zeros test&lt;/P&gt;</description>
      <pubDate>Wed, 25 May 2022 11:55:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fail-during-Mfgtool-download/m-p/1463986#M190827</guid>
      <dc:creator>sethhorus</dc:creator>
      <dc:date>2022-05-25T11:55:37Z</dc:date>
    </item>
    <item>
      <title>Re: fail during Mfgtool download</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fail-during-Mfgtool-download/m-p/1463993#M190828</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;the board stop "starting kernel......" in serial console during download by mfgtool.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Boot from USB for mfgtools&lt;BR /&gt;Use default environment for mfgtools&lt;BR /&gt;Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt; run bootcmd_mfg&lt;BR /&gt;Kernel image @ 0x12000000 [ 0x000000 - 0x53d8d0 ]&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 12c00000 ...&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-imx6&lt;BR /&gt;Image Type: ARM Linux RAMDisk Image (gzip compressed)&lt;BR /&gt;Data Size: 18729449 Bytes = 17.9 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 18000000&lt;BR /&gt;Booting using the fdt blob at 0x18000000&lt;BR /&gt;Using Device Tree in place at 18000000, end 1800d22d&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;I burn other boards(different circuits and same DDR,PM）with same mfgtools.they are fine&lt;/P&gt;</description>
      <pubDate>Wed, 25 May 2022 12:02:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fail-during-Mfgtool-download/m-p/1463993#M190828</guid>
      <dc:creator>sethhorus</dc:creator>
      <dc:date>2022-05-25T12:02:55Z</dc:date>
    </item>
  </channel>
</rss>