<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX8QXP secure boot using emmc</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-secure-boot-using-emmc/m-p/1463934#M190816</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/136564"&gt;@guilhermes&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This DOC can be applicable for emmc, except that if you use RPMB partition for emmc.&lt;/P&gt;
&lt;P&gt;There is no such DOC like 8m. The Link that you attached above works fine.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 25 May 2022 10:13:35 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2022-05-25T10:13:35Z</dc:date>
    <item>
      <title>i.MX8QXP secure boot using emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-secure-boot-using-emmc/m-p/1455889#M190216</link>
      <description>&lt;P&gt;Hello NXP team,&lt;BR /&gt;&lt;BR /&gt;We're designing a custom board based on the i.MX8QXP-MEK, but with boot option from emmc only. We'd like to add a Secure Boot functionality in the future for OTA updates. Regarding this:&lt;BR /&gt;&lt;BR /&gt;Are the steps described in this document (&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/ahab/guides/mx8_mx8x_secure_boot.txt?h=imx_v2019.04_5.4.3_2.0.0" target="_self"&gt;i.MX 8, i.MX 8X Secure Boot guide using AHAB&lt;/A&gt;) also applicable when booting from emmc? I'm assuming the steps for SD/MMC interfaces are the same regardless of boot media. Is this correct?&lt;BR /&gt;&lt;BR /&gt;Also, is there a guide like this one: (&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Steps-to-enable-secure-boot-in-i-MX8M-Nano/ta-p/1246417" target="_self"&gt;Steps to enable secure boot in i.MX8M Nano&lt;/A&gt;) targeting i.MX8X processors?&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 May 2022 20:38:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-secure-boot-using-emmc/m-p/1455889#M190216</guid>
      <dc:creator>guilhermes</dc:creator>
      <dc:date>2022-05-10T20:38:01Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP secure boot using emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-secure-boot-using-emmc/m-p/1463934#M190816</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/136564"&gt;@guilhermes&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This DOC can be applicable for emmc, except that if you use RPMB partition for emmc.&lt;/P&gt;
&lt;P&gt;There is no such DOC like 8m. The Link that you attached above works fine.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 May 2022 10:13:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-secure-boot-using-emmc/m-p/1463934#M190816</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2022-05-25T10:13:35Z</dc:date>
    </item>
  </channel>
</rss>