<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWhy separate vfat partition for boot?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Why-separate-vfat-partition-for-boot/m-p/1463220#M190771</link>
    <description>&lt;P&gt;The standard sabresd image has a separate boot partition which is formatted as a vfat filesystem&lt;/P&gt;&lt;P&gt;Why is this? Why vfat?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've read that the reason for separate boot partitions was that older BIOS's could only read small partitions. However why format it as vfat?&lt;/P&gt;&lt;P&gt;Is there any reason not to use a single ext4 partition for the rootfs and boot?&lt;/P&gt;</description>
    <pubDate>Tue, 24 May 2022 11:53:06 GMT</pubDate>
    <dc:creator>diarmuidcollins</dc:creator>
    <dc:date>2022-05-24T11:53:06Z</dc:date>
    <item>
      <title>Why separate vfat partition for boot?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-separate-vfat-partition-for-boot/m-p/1463220#M190771</link>
      <description>&lt;P&gt;The standard sabresd image has a separate boot partition which is formatted as a vfat filesystem&lt;/P&gt;&lt;P&gt;Why is this? Why vfat?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've read that the reason for separate boot partitions was that older BIOS's could only read small partitions. However why format it as vfat?&lt;/P&gt;&lt;P&gt;Is there any reason not to use a single ext4 partition for the rootfs and boot?&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 11:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-separate-vfat-partition-for-boot/m-p/1463220#M190771</guid>
      <dc:creator>diarmuidcollins</dc:creator>
      <dc:date>2022-05-24T11:53:06Z</dc:date>
    </item>
  </channel>
</rss>