<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックincluding utee in core-image-minimal boot folder</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/including-utee-in-core-image-minimal-boot-folder/m-p/1463213#M190770</link>
    <description>&lt;P&gt;I have a fully working environment in which I can build the an image for a custom board based on the imx6. The image uses the core-image-minimal distro and is very closely based on the sabresd image.&lt;/P&gt;&lt;P&gt;So far I've used the standard partition scheme where a separate boot partition is used based on vfat filesystem&lt;/P&gt;&lt;P&gt;However I want to change it to a single ext4 partition with the device tree and kernel image in the /boot folder&lt;/P&gt;&lt;P&gt;I am also there. I have the device tree and zimage in the boot folder which I achieved by setting this in the core image bbappend&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;IMAGE_INSTALL += " \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;swupdate \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;swupdate-www \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;kernel-image \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;kernel-devicetree \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;"&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;However I cannot figure how to include the&amp;nbsp; optee file uTee-6dlsdb in the boot folder&lt;/P&gt;&lt;P&gt;I've tried including optee-os in the IMAGE_INSTALL but it didn't work.&lt;/P&gt;&lt;P&gt;Anyone know how to include this specifically in the image?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 24 May 2022 11:50:04 GMT</pubDate>
    <dc:creator>diarmuidcollins</dc:creator>
    <dc:date>2022-05-24T11:50:04Z</dc:date>
    <item>
      <title>including utee in core-image-minimal boot folder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/including-utee-in-core-image-minimal-boot-folder/m-p/1463213#M190770</link>
      <description>&lt;P&gt;I have a fully working environment in which I can build the an image for a custom board based on the imx6. The image uses the core-image-minimal distro and is very closely based on the sabresd image.&lt;/P&gt;&lt;P&gt;So far I've used the standard partition scheme where a separate boot partition is used based on vfat filesystem&lt;/P&gt;&lt;P&gt;However I want to change it to a single ext4 partition with the device tree and kernel image in the /boot folder&lt;/P&gt;&lt;P&gt;I am also there. I have the device tree and zimage in the boot folder which I achieved by setting this in the core image bbappend&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;IMAGE_INSTALL += " \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;swupdate \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;swupdate-www \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;kernel-image \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;kernel-devicetree \&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;"&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;However I cannot figure how to include the&amp;nbsp; optee file uTee-6dlsdb in the boot folder&lt;/P&gt;&lt;P&gt;I've tried including optee-os in the IMAGE_INSTALL but it didn't work.&lt;/P&gt;&lt;P&gt;Anyone know how to include this specifically in the image?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 11:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/including-utee-in-core-image-minimal-boot-folder/m-p/1463213#M190770</guid>
      <dc:creator>diarmuidcollins</dc:creator>
      <dc:date>2022-05-24T11:50:04Z</dc:date>
    </item>
  </channel>
</rss>