<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Audio device dual support in Android 6.0.1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Audio-device-dual-support-in-Android-6-0-1/m-p/1462813#M190736</link>
    <description>&lt;P&gt;Driver work in the kernel has been completed.&lt;BR /&gt;In android, wm8960 makes sound, tlv320dac does not. dts is modified as follows.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Android error when running tlv320dac is as follows.&lt;BR /&gt;05-24 01:22:46.675 734 974 I vol.Events: writeEvent level_changed STREAM_MUSIC 12&lt;BR /&gt;05-24 01:22:46.769 734 974 I vol.Events: writeEvent level_changed STREAM_MUSIC 11&lt;BR /&gt;05-24 01:22:46.994 232 1958 D NuPlayerDriver: notifyListener_l(0xb41060c0), (1, 0, 0)&lt;BR /&gt;05-24 01:22:46.995 1310 1625 D MediaPlayer: setSubtitleAnchor in MediaPlayer&lt;BR /&gt;05-24 01:22:46.999 1310 1625 D Ringtone: Successfully created local player&lt;BR /&gt;05-24 01:22:47.002 232 557 D NuPlayerDriver: start(0xb41060c0), state is 4, eos is 0&lt;BR /&gt;05-24 01:22:47.002 232 1958 I GenericSource: start&lt;BR /&gt;05-24 01:22:47.014 232 1963 E OMXNodeInstance: setConfig(33:google.vorbis.decoder, ConfigPriority(0x6f800002)) ERROR: Undefined(0x80001001)&lt;BR /&gt;05-24 01:22:47.014 232 1963 I ACodec : codec does not support config priority (err -2147483648)&lt;BR /&gt;05-24 01:22:47.016 232 1963 I MediaCodec: MediaCodec will operate in async mode&lt;BR /&gt;05-24 01:22:47.027 232 1961 W APM::AudioPolicyManager: getOutput() could not find output for stream 3, samplingRate 0,format 0, channels 3, flags 0&lt;BR /&gt;05-24 01:22:47.027 232 1961 W NuPlayerRenderer: openAudioSink: non offloaded open failed status: -19&lt;BR /&gt;05-24 01:22:47.028 232 1958 E NuPlayer: received error(0xffffffed) from audio decoder, flushing(0), now shutting down&lt;BR /&gt;05-24 01:22:47.028 232 1961 W NuPlayerRenderer: onDrainAudioQueue(): audio sink is not ready&lt;BR /&gt;05-24 01:22:47.028 232 1958 D NuPlayerDriver: notifyListener_l(0xb41060c0), (100, 1, -19)&lt;BR /&gt;05-24 01:22:47.028 1310 1323 E MediaPlayer: error (1, -19)&lt;BR /&gt;05-24 01:22:47.028 232 1961 W NuPlayerRenderer: onDrainAudioQueue(): audio sink is not ready&lt;BR /&gt;05-24 01:22:47.028 232 1961 W NuPlayerRenderer: onDrainAudioQueue(): audio sink is not ready&lt;BR /&gt;05-24 01:22:47.029 1310 1625 E MediaPlayer: Error (1,-19)&lt;BR /&gt;05-24 01:22:47.033 232 1958 W AMessage: failed to post message as target looper for handler 0 is gone.&lt;/P&gt;</description>
    <pubDate>Tue, 24 May 2022 02:37:07 GMT</pubDate>
    <dc:creator>jonginjeon</dc:creator>
    <dc:date>2022-05-24T02:37:07Z</dc:date>
    <item>
      <title>Audio device dual support in Android 6.0.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-device-dual-support-in-Android-6-0-1/m-p/1462813#M190736</link>
      <description>&lt;P&gt;Driver work in the kernel has been completed.&lt;BR /&gt;In android, wm8960 makes sound, tlv320dac does not. dts is modified as follows.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Android error when running tlv320dac is as follows.&lt;BR /&gt;05-24 01:22:46.675 734 974 I vol.Events: writeEvent level_changed STREAM_MUSIC 12&lt;BR /&gt;05-24 01:22:46.769 734 974 I vol.Events: writeEvent level_changed STREAM_MUSIC 11&lt;BR /&gt;05-24 01:22:46.994 232 1958 D NuPlayerDriver: notifyListener_l(0xb41060c0), (1, 0, 0)&lt;BR /&gt;05-24 01:22:46.995 1310 1625 D MediaPlayer: setSubtitleAnchor in MediaPlayer&lt;BR /&gt;05-24 01:22:46.999 1310 1625 D Ringtone: Successfully created local player&lt;BR /&gt;05-24 01:22:47.002 232 557 D NuPlayerDriver: start(0xb41060c0), state is 4, eos is 0&lt;BR /&gt;05-24 01:22:47.002 232 1958 I GenericSource: start&lt;BR /&gt;05-24 01:22:47.014 232 1963 E OMXNodeInstance: setConfig(33:google.vorbis.decoder, ConfigPriority(0x6f800002)) ERROR: Undefined(0x80001001)&lt;BR /&gt;05-24 01:22:47.014 232 1963 I ACodec : codec does not support config priority (err -2147483648)&lt;BR /&gt;05-24 01:22:47.016 232 1963 I MediaCodec: MediaCodec will operate in async mode&lt;BR /&gt;05-24 01:22:47.027 232 1961 W APM::AudioPolicyManager: getOutput() could not find output for stream 3, samplingRate 0,format 0, channels 3, flags 0&lt;BR /&gt;05-24 01:22:47.027 232 1961 W NuPlayerRenderer: openAudioSink: non offloaded open failed status: -19&lt;BR /&gt;05-24 01:22:47.028 232 1958 E NuPlayer: received error(0xffffffed) from audio decoder, flushing(0), now shutting down&lt;BR /&gt;05-24 01:22:47.028 232 1961 W NuPlayerRenderer: onDrainAudioQueue(): audio sink is not ready&lt;BR /&gt;05-24 01:22:47.028 232 1958 D NuPlayerDriver: notifyListener_l(0xb41060c0), (100, 1, -19)&lt;BR /&gt;05-24 01:22:47.028 1310 1323 E MediaPlayer: error (1, -19)&lt;BR /&gt;05-24 01:22:47.028 232 1961 W NuPlayerRenderer: onDrainAudioQueue(): audio sink is not ready&lt;BR /&gt;05-24 01:22:47.028 232 1961 W NuPlayerRenderer: onDrainAudioQueue(): audio sink is not ready&lt;BR /&gt;05-24 01:22:47.029 1310 1625 E MediaPlayer: Error (1,-19)&lt;BR /&gt;05-24 01:22:47.033 232 1958 W AMessage: failed to post message as target looper for handler 0 is gone.&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 02:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-device-dual-support-in-Android-6-0-1/m-p/1462813#M190736</guid>
      <dc:creator>jonginjeon</dc:creator>
      <dc:date>2022-05-24T02:37:07Z</dc:date>
    </item>
  </channel>
</rss>