<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Ram Size Increase - Android imx8mm</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ram-Size-Increase-Android-imx8mm/m-p/1462069#M190689</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Am I going to get into any trouble without updating the device tree?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;--&amp;gt;No, The DRAM has been&amp;nbsp;initialized in&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;SPL. It doesn't use dts in this stage.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 23 May 2022 03:00:51 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2022-05-23T03:00:51Z</dc:date>
    <item>
      <title>Ram Size Increase - Android imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ram-Size-Increase-Android-imx8mm/m-p/1461136#M190590</link>
      <description>&lt;P&gt;We are working on a product that is closely modeled after the imx8mm_evk. Due to increased memory demand, we decided to increase the amount of RAM from 2GB to 3GB. Android is able to boot with only one change within uboot.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;include/configs/imx8mm_evk.h&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp; #define PHYS_SDRAM_SIZE 0x80000000 /* 2GB DDR */&lt;BR /&gt;+ #define PHYS_SDRAM_SIZE 0xC0000000 /* 3GB DDR */&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was wondering why I didn't need to make any changes to the device tree itself? Shouldn't this have crashed or failed to compile if the deivce tree was not updated? Am I going to get into any trouble without updating the device tree?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Section to update in question&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;arch/arm/dts/imx8mm-evk.dts&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;memory@40000000 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; device_type = "memory";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0x0 0x40000000 0 0x80000000&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 May 2022 22:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ram-Size-Increase-Android-imx8mm/m-p/1461136#M190590</guid>
      <dc:creator>seanlink</dc:creator>
      <dc:date>2022-05-19T22:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: Ram Size Increase - Android imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ram-Size-Increase-Android-imx8mm/m-p/1462069#M190689</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Am I going to get into any trouble without updating the device tree?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;--&amp;gt;No, The DRAM has been&amp;nbsp;initialized in&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;SPL. It doesn't use dts in this stage.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 03:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ram-Size-Increase-Android-imx8mm/m-p/1462069#M190689</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-05-23T03:00:51Z</dc:date>
    </item>
  </channel>
</rss>