<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMXRT1060 - Load app directly to SDRAM without Debug in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1060-Load-app-directly-to-SDRAM-without-Debug/m-p/1461977#M190677</link>
    <description>&lt;P&gt;Hi，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is there a tool from NXP to achieve this?&lt;BR /&gt;-- Please follow the &lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Generating-a-Bootable-Image-for-the-RT1050/ta-p/1123079" target="_self"&gt;post&lt;/A&gt; to generate a boot image that is executed in the SDRAM finally.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Mon, 23 May 2022 00:41:55 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2022-05-23T00:41:55Z</dc:date>
    <item>
      <title>IMXRT1060 - Load app directly to SDRAM without Debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1060-Load-app-directly-to-SDRAM-without-Debug/m-p/1461726#M190652</link>
      <description>&lt;P&gt;I'm looking for a way to load my application directly into SDRAM and then run it. Is there a way to do this without using the Debug feature on MCUxpresso?&lt;/P&gt;&lt;P&gt;I'm using a jlink programmer and It looks like it can be done through the jlink command line but it would take me a while to figure out the commands I need to use to load the file. I also need to load a script to configure the SDRAM which I already use successfully in the debugger of MCUxpresso.&lt;/P&gt;&lt;P&gt;Is there a tool from NXP to achieve this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 14:46:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1060-Load-app-directly-to-SDRAM-without-Debug/m-p/1461726#M190652</guid>
      <dc:creator>pauricacre</dc:creator>
      <dc:date>2022-05-20T14:46:06Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1060 - Load app directly to SDRAM without Debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1060-Load-app-directly-to-SDRAM-without-Debug/m-p/1461977#M190677</link>
      <description>&lt;P&gt;Hi，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is there a tool from NXP to achieve this?&lt;BR /&gt;-- Please follow the &lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Generating-a-Bootable-Image-for-the-RT1050/ta-p/1123079" target="_self"&gt;post&lt;/A&gt; to generate a boot image that is executed in the SDRAM finally.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 00:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1060-Load-app-directly-to-SDRAM-without-Debug/m-p/1461977#M190677</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-05-23T00:41:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1060 - Load app directly to SDRAM without Debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1060-Load-app-directly-to-SDRAM-without-Debug/m-p/1463052#M190754</link>
      <description>&lt;P&gt;I'm already able to make the image successfully. I'm looking for an alternative way to load the bin file into the SDRAM and execute. At this stage I don't want to write the file to flash, just load the program to SDRAM.&lt;/P&gt;&lt;P&gt;I can do this through MCUxpresso already but I want an easier option of loading the program. I don't want to debug, just execute the application in SDRAM.&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 08:32:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1060-Load-app-directly-to-SDRAM-without-Debug/m-p/1463052#M190754</guid>
      <dc:creator>pauricacre</dc:creator>
      <dc:date>2022-05-24T08:32:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1060 - Load app directly to SDRAM without Debug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1060-Load-app-directly-to-SDRAM-without-Debug/m-p/1463590#M190790</link>
      <description>&lt;P&gt;Hi，&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;I'm afraid it's too hard to implement your purpose.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 25 May 2022 01:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1060-Load-app-directly-to-SDRAM-without-Debug/m-p/1463590#M190790</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-05-25T01:49:10Z</dc:date>
    </item>
  </channel>
</rss>