<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ar6k_wlan issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ar6k-wlan-issue/m-p/1461707#M190649</link>
    <description>&lt;P&gt;had u solved the issue ? facing the same&lt;/P&gt;</description>
    <pubDate>Fri, 20 May 2022 14:05:52 GMT</pubDate>
    <dc:creator>manojsai</dc:creator>
    <dc:date>2022-05-20T14:05:52Z</dc:date>
    <item>
      <title>ar6k_wlan issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ar6k-wlan-issue/m-p/946833#M141611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using mfgtool to partition and flash my image. In the process. I migrated from one partition to 3 larger partitions. Now it seems the emmc is not being erased completely, so i get wlan driver failures. In the begining of bad boot up i see readonly fs on my primary partition and then later when the wlan driver probing emmc, it fails to load.&lt;/P&gt;&lt;P&gt;Below are the logs,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;EXT4-fs (mmcblk1p1): INFO: recovery required on readonly filesystem&lt;BR /&gt;EXT4-fs (mmcblk1p1): write access will be enabled during recovery&lt;BR /&gt;EXT4-fs (mmcblk1p1): recovery complete&lt;BR /&gt;EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;VFS: Mounted root (ext4 filesystem) readonly on device 179:1.&lt;BR /&gt;devtmpfs: mounted&lt;BR /&gt;Freeing unused kernel memory: 1024K&lt;BR /&gt;EXT4-fs (mmcblk1p3): recovery complete&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;R0: wlan: [114:E :SAP] dfs_reset_alldelaylines[95]: pl==NULL, b5radars=00000000&lt;BR /&gt;rx_completion_task: rx completion task stopping&lt;BR /&gt;mmc0: queuing unknown CIS tuple 0x01 (3 bytes)&lt;BR /&gt;mmc0: queuing unknown CIS tuple 0x1a (5 bytes)&lt;BR /&gt;mmc0: queuing unknown CIS tuple 0x1b (8 bytes)&lt;BR /&gt;mmc0: queuing unknown CIS tuple 0x14 (0 bytes)&lt;BR /&gt;R0: wlan: [114:F :HIF] hdd_wlan_startup failed&lt;BR /&gt;AR6000: SDIO bus operation failed! MMC stack returned : -84 &lt;BR /&gt;__HIFReadWrite, addr:0X000868, len:00000004, Write, Sync &lt;BR /&gt;ar6k_wlan: probe of mmc0:0001:1 failed with error -1&lt;BR /&gt;ath_hif_sdio: HIF (Atheros/multi-bss)&lt;BR /&gt;R0: wlan: [114:E :HDD] hdd_hif_register_driver: 17660: hdd_wlan_startup failed status:-11 jiffies_left:14000&lt;BR /&gt;R0: wlan: [114:F :HDD] hdd_driver_init: WLAN Driver Initialization failed&lt;BR /&gt;AR6000: Unregistering with the bus driver&lt;BR /&gt;AR6000: Unregistered!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Oct 2019 16:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ar6k-wlan-issue/m-p/946833#M141611</guid>
      <dc:creator>pankajjoshi</dc:creator>
      <dc:date>2019-10-21T16:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: ar6k_wlan issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ar6k-wlan-issue/m-p/946834#M141612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pankaj&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for erasing emmc partitions one can try suggestions on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://developer.toradex.com/knowledge-base/how-to-erase-emmc-flash-memory" title="https://developer.toradex.com/knowledge-base/how-to-erase-emmc-flash-memory"&gt;How to Erase the eMMC Flash Memory on Toradex Apalis or Colibri Modules&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/435725"&gt;https://community.nxp.com/thread/435725&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Oct 2019 00:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ar6k-wlan-issue/m-p/946834#M141612</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-10-22T00:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: ar6k_wlan issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ar6k-wlan-issue/m-p/1461707#M190649</link>
      <description>&lt;P&gt;had u solved the issue ? facing the same&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 14:05:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ar6k-wlan-issue/m-p/1461707#M190649</guid>
      <dc:creator>manojsai</dc:creator>
      <dc:date>2022-05-20T14:05:52Z</dc:date>
    </item>
  </channel>
</rss>