<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: flexspi in rtos</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/flexspi-in-rtos/m-p/1458911#M190435</link>
    <description>&lt;P&gt;Hi，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1）Is there any example code available where flexspi is used with TCP/IP stack in an RTOS environment?&lt;BR /&gt;-- The above issue is related to the FlexSPI driver, I guess you forgot to relocate the driver into the RAM, so to provide the fastest possible support, I'd like to suggest you refer to the freertos_hello_flash_operation which resides in ~\boards\evkmimxrt1020\rtos_examples of SDK library&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Tue, 17 May 2022 01:47:48 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2022-05-17T01:47:48Z</dc:date>
    <item>
      <title>flexspi in rtos</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/flexspi-in-rtos/m-p/1458165#M190365</link>
      <description>&lt;P&gt;Can I use flexspi driver provided in MCUXpresso with the RTOS application?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am running evkmimxrt1020_lwip_tcpecho_freertos example code with evk-1020 board. But when I add the flexspi driver with the project and try to initialize the flexspi_nor_flash_init, the code is stuck in the following marked line. Is there any example code available where flexspi is used with TCP/IP stack in an RTOS environment?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="partha4sarathe_0-1652474809133.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179798i392E8D69DD389DF3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="partha4sarathe_0-1652474809133.png" alt="partha4sarathe_0-1652474809133.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 May 2022 20:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/flexspi-in-rtos/m-p/1458165#M190365</guid>
      <dc:creator>partha4sarathe</dc:creator>
      <dc:date>2022-05-13T20:50:55Z</dc:date>
    </item>
    <item>
      <title>Re: flexspi in rtos</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/flexspi-in-rtos/m-p/1458911#M190435</link>
      <description>&lt;P&gt;Hi，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1）Is there any example code available where flexspi is used with TCP/IP stack in an RTOS environment?&lt;BR /&gt;-- The above issue is related to the FlexSPI driver, I guess you forgot to relocate the driver into the RAM, so to provide the fastest possible support, I'd like to suggest you refer to the freertos_hello_flash_operation which resides in ~\boards\evkmimxrt1020\rtos_examples of SDK library&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 17 May 2022 01:47:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/flexspi-in-rtos/m-p/1458911#M190435</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-05-17T01:47:48Z</dc:date>
    </item>
  </channel>
</rss>