<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic enable wdt in u-boot and then have it still enabled in linux for i.mx8mp in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/enable-wdt-in-u-boot-and-then-have-it-still-enabled-in-linux-for/m-p/1458788#M190427</link>
    <description>&lt;P&gt;I'd like to enable the watchdog in u-boot and then have it still enabled once I boot into linux. The motivation is that I want to make sure the kernel comes up ok.&lt;/P&gt;&lt;P&gt;I can enable the watchdog and see it reset in uboot just fine with manual register writes&lt;/P&gt;&lt;P&gt;mw.w 30280000 0f74 1&lt;/P&gt;&lt;P&gt;but once I boot into linux it doesn't seem to reboot and I don't think there is anything that is servicing it because I can manually enable in linux and watch it reboot&lt;/P&gt;&lt;P&gt;echo "1" &amp;gt; /dev/watchdog0&lt;/P&gt;</description>
    <pubDate>Mon, 16 May 2022 17:21:02 GMT</pubDate>
    <dc:creator>richc128</dc:creator>
    <dc:date>2022-05-16T17:21:02Z</dc:date>
    <item>
      <title>enable wdt in u-boot and then have it still enabled in linux for i.mx8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/enable-wdt-in-u-boot-and-then-have-it-still-enabled-in-linux-for/m-p/1458788#M190427</link>
      <description>&lt;P&gt;I'd like to enable the watchdog in u-boot and then have it still enabled once I boot into linux. The motivation is that I want to make sure the kernel comes up ok.&lt;/P&gt;&lt;P&gt;I can enable the watchdog and see it reset in uboot just fine with manual register writes&lt;/P&gt;&lt;P&gt;mw.w 30280000 0f74 1&lt;/P&gt;&lt;P&gt;but once I boot into linux it doesn't seem to reboot and I don't think there is anything that is servicing it because I can manually enable in linux and watch it reboot&lt;/P&gt;&lt;P&gt;echo "1" &amp;gt; /dev/watchdog0&lt;/P&gt;</description>
      <pubDate>Mon, 16 May 2022 17:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/enable-wdt-in-u-boot-and-then-have-it-still-enabled-in-linux-for/m-p/1458788#M190427</guid>
      <dc:creator>richc128</dc:creator>
      <dc:date>2022-05-16T17:21:02Z</dc:date>
    </item>
  </channel>
</rss>