<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAdding NOR Flash driver to rt1051 Project</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Adding-NOR-Flash-driver-to-rt1051-Project/m-p/1458735#M190425</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm creating a project using an RT1051DVJ6B and MCUXpresso. When adding components to the project I cannot add any nor_flash components, I can however add them if the processor is changed to an rt1052. Looking at the data sheet, I see no reason why nor flash components will be excluded from the rt1051 processor.&lt;/P&gt;&lt;P&gt;Thanks in advanced,&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;</description>
    <pubDate>Mon, 16 May 2022 15:23:49 GMT</pubDate>
    <dc:creator>nick_j</dc:creator>
    <dc:date>2022-05-16T15:23:49Z</dc:date>
    <item>
      <title>Adding NOR Flash driver to rt1051 Project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-NOR-Flash-driver-to-rt1051-Project/m-p/1458735#M190425</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm creating a project using an RT1051DVJ6B and MCUXpresso. When adding components to the project I cannot add any nor_flash components, I can however add them if the processor is changed to an rt1052. Looking at the data sheet, I see no reason why nor flash components will be excluded from the rt1051 processor.&lt;/P&gt;&lt;P&gt;Thanks in advanced,&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;</description>
      <pubDate>Mon, 16 May 2022 15:23:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-NOR-Flash-driver-to-rt1051-Project/m-p/1458735#M190425</guid>
      <dc:creator>nick_j</dc:creator>
      <dc:date>2022-05-16T15:23:49Z</dc:date>
    </item>
    <item>
      <title>Re: Adding NOR Flash driver to rt1051 Project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-NOR-Flash-driver-to-rt1051-Project/m-p/1458980#M190440</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178835"&gt;@nick_j&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Please help to check, whether you mentioned the following situation:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1652760701682.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179931iC451C50C8F87D133/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1652760701682.png" alt="kerryzhou_0-1652760701682.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;kerryzhou_0-1652760701682.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_1-1652760710631.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179932i6115F7A74E474206/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_1-1652760710631.png" alt="kerryzhou_1-1652760710631.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;kerryzhou_1-1652760710631.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;In the software component, RT1052 has mflashrt1052, but RT1051 don't have it, right?&lt;/P&gt;
&lt;P&gt;From the component name, we can see it is used for the RT1052.&lt;/P&gt;
&lt;P&gt;But, if you want to use it, I think you can create the project, then add the related source code driver directly in the project.&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 May 2022 04:13:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-NOR-Flash-driver-to-rt1051-Project/m-p/1458980#M190440</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2022-05-17T04:13:31Z</dc:date>
    </item>
    <item>
      <title>Re: Adding NOR Flash driver to rt1051 Project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-NOR-Flash-driver-to-rt1051-Project/m-p/1459160#M190447</link>
      <description>&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;I just checked and yes there's no mflashrt1050 component for the rt1051.&lt;/P&gt;&lt;P&gt;The ones I want to use are the nor components shown below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nick_j_0-1652774824124.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179987iFF3EADD9AFA1C48F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nick_j_0-1652774824124.png" alt="nick_j_0-1652774824124.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;nick_j_0-1652774824124.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;which don't show up for the rt1051.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nick_j_1-1652774862257.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179988iE103A592F5D98983/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nick_j_1-1652774862257.png" alt="nick_j_1-1652774862257.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;nick_j_1-1652774862257.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I just thought it was a bit odd.&lt;/P&gt;&lt;P&gt;I will probably just add in the sources manually, I just wanted to make sure that there won't be an issue with that.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Nick&lt;/P&gt;</description>
      <pubDate>Tue, 17 May 2022 08:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-NOR-Flash-driver-to-rt1051-Project/m-p/1459160#M190447</guid>
      <dc:creator>nick_j</dc:creator>
      <dc:date>2022-05-17T08:11:36Z</dc:date>
    </item>
    <item>
      <title>Re: Adding NOR Flash driver to rt1051 Project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Adding-NOR-Flash-driver-to-rt1051-Project/m-p/1459240#M190455</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178835"&gt;@nick_j&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; You are right, I think sdk when add this component, just consider the RT1052, didn't conside it add to RT1051, but as I know, the flexSPI module is the same, you can use the RT1052 add the component, then copy the source code to your RT1051 directly, it can be used.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Or you also can use the driver-&amp;gt;flexSPI project directly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Tue, 17 May 2022 09:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Adding-NOR-Flash-driver-to-rt1051-Project/m-p/1459240#M190455</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2022-05-17T09:16:31Z</dc:date>
    </item>
  </channel>
</rss>