<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックInitrd built into custom Linux kernel is not running</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Initrd-built-into-custom-Linux-kernel-is-not-running/m-p/1458593#M190412</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am building a custom initrd image that I am building as a CPIO archive into the Linux kernel,The issue is&amp;nbsp; the kernel does not attempt to run from the initrd, and getting kernel panic&amp;nbsp; when booting from imx8qmmek.&lt;/P&gt;&lt;P&gt;The files I have in my CPIO archive:&lt;/P&gt;&lt;P&gt;cpio -ivt &amp;lt; initrd.cpio&lt;BR /&gt;drwx------ 1 root root 0 Jan 1 1970 /proc&lt;BR /&gt;drwx------ 1 root root 0 Jan 1 1970 /sys&lt;BR /&gt;dr-x-w-r-x 1 root root 0 Jan 1 1970 /mnt&lt;BR /&gt;dr-x-w-r-x 1 root root 0 Jan 1 1970 /idex&lt;BR /&gt;dr-x-w-r-x 1 root root 0 Jan 1 1970 /mnt/system&lt;BR /&gt;drwx------ 1 root root 0 Jan 1 1970 /etc&lt;BR /&gt;-r-x------ 1 root root 534376 Jan 1 1970 /init&lt;BR /&gt;-rwx------ 1 root root 460 Jan 1 1970 /etc/fstab&lt;BR /&gt;crwx------ 1 root root 5, 1 Jan 1 1970 /dev/console&lt;BR /&gt;1047 blocks&lt;BR /&gt;In the kernel .config I have :&lt;/P&gt;&lt;P&gt;CONFIG_INITRAMFS_SOURCE="../initramfs.cpio"&lt;/P&gt;&lt;P&gt;I have attached the bootlog below.&lt;/P&gt;&lt;P&gt;Any idea what might be wrong here or where I should start looking to debug?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 16 May 2022 10:32:43 GMT</pubDate>
    <dc:creator>anjalinv8</dc:creator>
    <dc:date>2022-05-16T10:32:43Z</dc:date>
    <item>
      <title>Initrd built into custom Linux kernel is not running</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Initrd-built-into-custom-Linux-kernel-is-not-running/m-p/1458593#M190412</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am building a custom initrd image that I am building as a CPIO archive into the Linux kernel,The issue is&amp;nbsp; the kernel does not attempt to run from the initrd, and getting kernel panic&amp;nbsp; when booting from imx8qmmek.&lt;/P&gt;&lt;P&gt;The files I have in my CPIO archive:&lt;/P&gt;&lt;P&gt;cpio -ivt &amp;lt; initrd.cpio&lt;BR /&gt;drwx------ 1 root root 0 Jan 1 1970 /proc&lt;BR /&gt;drwx------ 1 root root 0 Jan 1 1970 /sys&lt;BR /&gt;dr-x-w-r-x 1 root root 0 Jan 1 1970 /mnt&lt;BR /&gt;dr-x-w-r-x 1 root root 0 Jan 1 1970 /idex&lt;BR /&gt;dr-x-w-r-x 1 root root 0 Jan 1 1970 /mnt/system&lt;BR /&gt;drwx------ 1 root root 0 Jan 1 1970 /etc&lt;BR /&gt;-r-x------ 1 root root 534376 Jan 1 1970 /init&lt;BR /&gt;-rwx------ 1 root root 460 Jan 1 1970 /etc/fstab&lt;BR /&gt;crwx------ 1 root root 5, 1 Jan 1 1970 /dev/console&lt;BR /&gt;1047 blocks&lt;BR /&gt;In the kernel .config I have :&lt;/P&gt;&lt;P&gt;CONFIG_INITRAMFS_SOURCE="../initramfs.cpio"&lt;/P&gt;&lt;P&gt;I have attached the bootlog below.&lt;/P&gt;&lt;P&gt;Any idea what might be wrong here or where I should start looking to debug?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 16 May 2022 10:32:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Initrd-built-into-custom-Linux-kernel-is-not-running/m-p/1458593#M190412</guid>
      <dc:creator>anjalinv8</dc:creator>
      <dc:date>2022-05-16T10:32:43Z</dc:date>
    </item>
  </channel>
</rss>