<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIMXRT1061CVL5B: Run Debugging Session from QSPI NOR Flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1456874#M190282</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200688"&gt;@Lukaz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;As I know, it is related to the IJET, as when I use the CMSIS DAP debugger, which is the RT1060-EVK default debugger in the IAR, it doesn't have this issues.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; So, you can ignore that issue, just use it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; If you have any other issues, welcome to create the new question post.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kerry&lt;/P&gt;</description>
    <pubDate>Thu, 12 May 2022 02:03:49 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2022-05-12T02:03:49Z</dc:date>
    <item>
      <title>MIMXRT1061CVL5B: Run Debugging Session from QSPI NOR Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1455784#M190212</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I intend to use the MCU &lt;STRONG&gt;MIMXRT1061CVL5B,&amp;nbsp;&lt;/STRONG&gt;and now I am examining its compatibility with the product's functions using the &lt;STRONG&gt;MIMRT1060-EVKB&lt;/STRONG&gt;. One limitation that I have is the use of the OpenSDA, therefore I checked if I can boot the external flash with the USB-OGT and I was successful to do so using the flashloader with the&amp;nbsp;elftosb and the MfgTool2. My question is, as in the development phase I need to run debugging sessions, how is it possible to do so from the external QSPI&amp;nbsp;NOR Flash?&lt;BR /&gt;You can also simply refer me to sources that explain such things.&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 10 May 2022 15:18:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1455784#M190212</guid>
      <dc:creator>Lukaz</dc:creator>
      <dc:date>2022-05-10T15:18:46Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1061CVL5B: Run Debugging Session from QSPI NOR Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1455969#M190220</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200688"&gt;@Lukaz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; If you need to debug the RT1061, you need the debugger at first.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; If you are using the MIMXRT1060-EVKB board, it has the on board debugger directly, you can connect the opensda USB port, then the default debugger is CMSIS-DAP, you can open the SDK project, then debug it directly, the board need to enter the internal boot mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; If you are using the customer board, you need to find an external debugger, eg, Segger JLINK, then through the SWD to debug the chip project.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; We also have the application which may useful to you:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kerry&lt;/P&gt;</description>
      <pubDate>Wed, 11 May 2022 02:10:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1455969#M190220</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2022-05-11T02:10:30Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1061CVL5B: Run Debugging Session from QSPI NOR Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1456264#M190251</link>
      <description>&lt;P&gt;Thank you, it worked fine with me using I-JET debugger.&lt;BR /&gt;Just some points to clarify the solution. I have not disconnected any jumper from the board, I have connected J1 3-4 to use the USB-OTG port for power. The important thing was the debugger configurations&amp;nbsp;(see screenshots below)&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179477i374FA6E0510417CB/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 May 2022 09:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1456264#M190251</guid>
      <dc:creator>Lukaz</dc:creator>
      <dc:date>2022-05-11T09:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1061CVL5B: Run Debugging Session from QSPI NOR Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1456361#M190260</link>
      <description>&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;when I run the debugger session I get this message and I press yes to proceed and the debugging session works fine &lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179513i6D685C2A965EE590/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;but I was wondering if you have any idea why am I getting this message (below is the error message from the debug log)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Lukaz_0-1652267027136.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179515iEB991725D6C032B4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Lukaz_0-1652267027136.png" alt="Lukaz_0-1652267027136.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 11 May 2022 11:04:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1456361#M190260</guid>
      <dc:creator>Lukaz</dc:creator>
      <dc:date>2022-05-11T11:04:03Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1061CVL5B: Run Debugging Session from QSPI NOR Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1456874#M190282</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200688"&gt;@Lukaz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;As I know, it is related to the IJET, as when I use the CMSIS DAP debugger, which is the RT1060-EVK default debugger in the IAR, it doesn't have this issues.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; So, you can ignore that issue, just use it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; If you have any other issues, welcome to create the new question post.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kerry&lt;/P&gt;</description>
      <pubDate>Thu, 12 May 2022 02:03:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1061CVL5B-Run-Debugging-Session-from-QSPI-NOR-Flash/m-p/1456874#M190282</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2022-05-12T02:03:49Z</dc:date>
    </item>
  </channel>
</rss>