<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8mm  reserve_memory</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8mm-reserve-memory/m-p/1454795#M190129</link>
    <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;Is there any information?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Koji Okuda&lt;/P&gt;</description>
    <pubDate>Mon, 09 May 2022 07:50:57 GMT</pubDate>
    <dc:creator>okuda</dc:creator>
    <dc:date>2022-05-09T07:50:57Z</dc:date>
    <item>
      <title>iMX8mm  reserve_memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8mm-reserve-memory/m-p/1452093#M189934</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm using a vendor's BSP.(yocto base Linux version 5.4.3-2.0.0)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There are the following definitions in the dts file.&lt;BR /&gt;&lt;SPAN&gt;reserved-memory {&lt;BR /&gt;&lt;/SPAN&gt;　#address-cells = &amp;lt;2&amp;gt;;&lt;BR /&gt;　#size-cells = &amp;lt;2&amp;gt;;&lt;BR /&gt;　ranges;&lt;/P&gt;&lt;P&gt;　m4_reserved: m4@0x80000000 {&lt;BR /&gt;　　no-map;&lt;BR /&gt;　　reg = &amp;lt;0 0x80000000 0 0x1000000&amp;gt;;&lt;BR /&gt;　};&lt;/P&gt;&lt;P&gt;　rpmsg_reserved: rpmsg@0xbdb00000 {&lt;BR /&gt;　　no-map;&lt;BR /&gt;　　reg = &amp;lt;0 0xbdb00000 0 0x400000&amp;gt;;&lt;BR /&gt;　};&lt;/P&gt;&lt;P&gt;　rpmsg_dma_reserved:rpmsg_dma@0xbdf00000 {&lt;BR /&gt;　　compatible = "shared-dma-pool";&lt;BR /&gt;　　no-map;&lt;BR /&gt;　　reg = &amp;lt;0 0xbdf00000 0 0x100000&amp;gt;;&lt;BR /&gt;　};&lt;BR /&gt;};&lt;BR /&gt;&lt;BR /&gt;Also, uboot's printenv is as follows.&lt;BR /&gt;kboot=booti&lt;BR /&gt;loadaddr=0x40480000&lt;BR /&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;BR /&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;BR /&gt;loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}&lt;BR /&gt;m4_image=imx8mm-m4.bin&lt;BR /&gt;m4_ldaddr=0x48000000&lt;BR /&gt;m4_ldimgs=fatload mmc ${mmcdev}:${mmcpart} ${m4_ldaddr} ${m4_image}&lt;BR /&gt;m4_staddr=0x7e0000&lt;BR /&gt;m4_start=run m4_ldimgs &amp;amp;&amp;amp; cp.b ${m4_ldaddr} ${m4_staddr} 0x20000 &amp;amp;&amp;amp; dcache flush &amp;amp;&amp;amp; bootaux ${m4_staddr}&lt;/P&gt;&lt;P&gt;１．Why is it necessary to define each reserve memory area?&lt;BR /&gt;２．Is it possible to change the definition of each reserve memory area?&lt;BR /&gt;３．Since there is only 2GB of memory on the board, I would like to increase the free memory area.&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Is it possible to delete the above memory area?&lt;BR /&gt;４．What is imx8mm-m4.bin a file for processing?&lt;BR /&gt;　　（I want to keep the CPU on the M4 side stopped.）&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Koji Okuda&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 May 2022 02:20:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8mm-reserve-memory/m-p/1452093#M189934</guid>
      <dc:creator>okuda</dc:creator>
      <dc:date>2022-05-06T02:20:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8mm  reserve_memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8mm-reserve-memory/m-p/1454795#M190129</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;Is there any information?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Koji Okuda&lt;/P&gt;</description>
      <pubDate>Mon, 09 May 2022 07:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8mm-reserve-memory/m-p/1454795#M190129</guid>
      <dc:creator>okuda</dc:creator>
      <dc:date>2022-05-09T07:50:57Z</dc:date>
    </item>
  </channel>
</rss>