<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Installing 3.0.35 kernel headers</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237083#M19005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have some code for a USB Ethernet that is delivered to be built as a kernel module.&amp;nbsp; I'd like to compile this code natively on our i.MX6Q platform running Ubuntu 11.10.&amp;nbsp; The root file system does not appear to have the kernel headers installed for the 3.0.35 kernel.&amp;nbsp; How can I install these headers in the root file system so I can have the available natively?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;FM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jan 2014 22:49:41 GMT</pubDate>
    <dc:creator>frankmiller</dc:creator>
    <dc:date>2014-01-15T22:49:41Z</dc:date>
    <item>
      <title>Installing 3.0.35 kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237083#M19005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have some code for a USB Ethernet that is delivered to be built as a kernel module.&amp;nbsp; I'd like to compile this code natively on our i.MX6Q platform running Ubuntu 11.10.&amp;nbsp; The root file system does not appear to have the kernel headers installed for the 3.0.35 kernel.&amp;nbsp; How can I install these headers in the root file system so I can have the available natively?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;FM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2014 22:49:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237083#M19005</guid>
      <dc:creator>frankmiller</dc:creator>
      <dc:date>2014-01-15T22:49:41Z</dc:date>
    </item>
    <item>
      <title>Re: Installing 3.0.35 kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237084#M19006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Frank,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;are you tied to Ubuntu? Using Yocto, it is a matter of adding some IMAGE_FEATURES so packages installed on rootfs included dev and dgb ones.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the other hand, why don't you install the necessary packages using apt-get?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2014 23:32:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237084#M19006</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2014-01-15T23:32:00Z</dc:date>
    </item>
    <item>
      <title>Re: Installing 3.0.35 kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237085#M19007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I presume that Frank's using Freescale's image from one of the L3.0.35 release packages, and as far as I know, these don't point at an apt repository containing kernel sources and headers for i.MX6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We installed our headers manually from a git tree when compiling imx-lib and friends in this post.&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/mx6-video-acceleration/"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; http://boundarydevices.com/mx6-video-acceleration/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Frank, you're going to need the sources anyway, so you can (and probably need to) use 'make headers_install' from the kernel source tree to install the headers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2014 23:41:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237085#M19007</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-01-15T23:41:40Z</dc:date>
    </item>
    <item>
      <title>Re: Installing 3.0.35 kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237086#M19008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&amp;nbsp; I'm using ltib with the 4.0.0 tree.&amp;nbsp; I ran a make headers_install in the rpm/BUILD/linux subtree of the ltib suite so I think they are available.&amp;nbsp; What I need then is to figure out which of them need to be copied where in my rfs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;FM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2014 00:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237086#M19008</guid>
      <dc:creator>frankmiller</dc:creator>
      <dc:date>2014-01-16T00:24:51Z</dc:date>
    </item>
    <item>
      <title>Re: Installing 3.0.35 kernel headers</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237087#M19009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Eric alluded to, they are not available as a native apt-get install from the running rfs on the i.MX6 target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FM&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2014 00:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-3-0-35-kernel-headers/m-p/237087#M19009</guid>
      <dc:creator>frankmiller</dc:creator>
      <dc:date>2014-01-16T00:27:13Z</dc:date>
    </item>
  </channel>
</rss>