<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Ielftool generated binary file size</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ielftool-generated-binary-file-size/m-p/1453614#M190039</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I used the iefltool to generate the .bin file from .out file. The .out file is only around 400kB in size but the .bin file seems to be over 1000kB in size. Why is the .bin file size very high ? How would I be able to reduce the size ?&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
    <pubDate>Thu, 05 May 2022 14:19:11 GMT</pubDate>
    <dc:creator>itsme12_01</dc:creator>
    <dc:date>2022-05-05T14:19:11Z</dc:date>
    <item>
      <title>Ielftool generated binary file size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ielftool-generated-binary-file-size/m-p/1453614#M190039</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I used the iefltool to generate the .bin file from .out file. The .out file is only around 400kB in size but the .bin file seems to be over 1000kB in size. Why is the .bin file size very high ? How would I be able to reduce the size ?&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 05 May 2022 14:19:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ielftool-generated-binary-file-size/m-p/1453614#M190039</guid>
      <dc:creator>itsme12_01</dc:creator>
      <dc:date>2022-05-05T14:19:11Z</dc:date>
    </item>
    <item>
      <title>Re: Ielftool generated binary file size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ielftool-generated-binary-file-size/m-p/1453822#M190050</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;To provide the fastest possible support, I was wondering if you can introduce the steps for replicating the phenomenon.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 06 May 2022 00:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ielftool-generated-binary-file-size/m-p/1453822#M190050</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-05-06T00:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: Ielftool generated binary file size</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ielftool-generated-binary-file-size/m-p/1459380#M190468</link>
      <description>&lt;P&gt;Hello, I apologize for the late reply.&amp;nbsp;&lt;BR /&gt;I found the reason for a huge binary file size.&lt;BR /&gt;When placing a section into memory, if the segment is divided between two memory regions, then while creating a .bin file, the memory region in between the 2 regions will also be considered. Hence results in huge file size.&lt;BR /&gt;For example,&lt;BR /&gt;If I place const SECTIONA at 0x2000 to 0x4000&lt;BR /&gt;place const SECTIONB at 0x8000 to 0xF000&lt;BR /&gt;Then when creating the binary file,&lt;BR /&gt;For segment const, the memory region considered would be (0xF000 - 0x2000). The gaps between would be filled with 0s. Hence results in a huge file size.&lt;BR /&gt;&lt;BR /&gt;Hope this becomes helpful to someone in furture.&lt;BR /&gt;&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 17 May 2022 13:24:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ielftool-generated-binary-file-size/m-p/1459380#M190468</guid>
      <dc:creator>itsme12_01</dc:creator>
      <dc:date>2022-05-17T13:24:37Z</dc:date>
    </item>
  </channel>
</rss>