<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI DMA Transfer Delay in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-DMA-Transfer-Delay/m-p/1453476#M190026</link>
    <description>&lt;P&gt;This is caused by spi driver doing separate 8 bit transfers (ECSPIx_CONREG . BURST_LENGHT = &lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt; instead of doing single transfer with BURST_LENGTH set to total transfer bit count.&amp;nbsp;For the same reason hardware chip select is of no use, forcing nearly everyone to use software toggled CS.&lt;/P&gt;</description>
    <pubDate>Thu, 05 May 2022 11:30:12 GMT</pubDate>
    <dc:creator>kef2</dc:creator>
    <dc:date>2022-05-05T11:30:12Z</dc:date>
    <item>
      <title>SPI DMA Transfer Delay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-DMA-Transfer-Delay/m-p/1444694#M189386</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Does anyone know what causes the ~200ns clock delays between words in a dma spi transfer?&lt;/P&gt;&lt;P&gt;Does it have to do with the latency with of wait_for_completion_timeout for rx/tx in&lt;/P&gt;&lt;P&gt;spi_imx_dma_transfer?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="marcuscastlepeakinc_0-1650065212203.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/177089i8EB6BD310DAAE62F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="marcuscastlepeakinc_0-1650065212203.png" alt="marcuscastlepeakinc_0-1650065212203.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Fri, 15 Apr 2022 23:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-DMA-Transfer-Delay/m-p/1444694#M189386</guid>
      <dc:creator>marcus-castlepeakinc</dc:creator>
      <dc:date>2022-04-15T23:27:39Z</dc:date>
    </item>
    <item>
      <title>Re: SPI DMA Transfer Delay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-DMA-Transfer-Delay/m-p/1453476#M190026</link>
      <description>&lt;P&gt;This is caused by spi driver doing separate 8 bit transfers (ECSPIx_CONREG . BURST_LENGHT = &lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt; instead of doing single transfer with BURST_LENGTH set to total transfer bit count.&amp;nbsp;For the same reason hardware chip select is of no use, forcing nearly everyone to use software toggled CS.&lt;/P&gt;</description>
      <pubDate>Thu, 05 May 2022 11:30:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-DMA-Transfer-Delay/m-p/1453476#M190026</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2022-05-05T11:30:12Z</dc:date>
    </item>
  </channel>
</rss>