<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic To install QT on i.mx53 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/To-install-QT-on-i-mx53/m-p/236972#M18992</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I follow the steps ,&lt;A href="https://support.bluetechnix.at/wiki/Qt_Embedded_on_i.MX53"&gt;https://support.bluetechnix.at/wiki/Qt_Embedded_on_i.MX53&lt;/A&gt; to install QT4 on i.mx53 but failed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find out these OpenVG libraries libgsl.so,libc2d.so, and libpanel2.so for linking options -lgsl, -lc2d, and -lpanel2&amp;nbsp; in the makefile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;After installing the amd-gpu-bin-mx51 or amd-gpu-x11-bin-mx51, there is only one library libgsl-fsl.so like libgsl.so in the rootfs/usr/lib.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;But I can't find out the librayies,c2d and panel2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;What should I do with it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Aher Chen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Aug 2013 04:03:09 GMT</pubDate>
    <dc:creator>aherchen</dc:creator>
    <dc:date>2013-08-02T04:03:09Z</dc:date>
    <item>
      <title>To install QT on i.mx53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/To-install-QT-on-i-mx53/m-p/236972#M18992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I follow the steps ,&lt;A href="https://support.bluetechnix.at/wiki/Qt_Embedded_on_i.MX53"&gt;https://support.bluetechnix.at/wiki/Qt_Embedded_on_i.MX53&lt;/A&gt; to install QT4 on i.mx53 but failed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find out these OpenVG libraries libgsl.so,libc2d.so, and libpanel2.so for linking options -lgsl, -lc2d, and -lpanel2&amp;nbsp; in the makefile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;After installing the amd-gpu-bin-mx51 or amd-gpu-x11-bin-mx51, there is only one library libgsl-fsl.so like libgsl.so in the rootfs/usr/lib.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;But I can't find out the librayies,c2d and panel2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;What should I do with it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Aher Chen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Aug 2013 04:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/To-install-QT-on-i-mx53/m-p/236972#M18992</guid>
      <dc:creator>aherchen</dc:creator>
      <dc:date>2013-08-02T04:03:09Z</dc:date>
    </item>
  </channel>
</rss>