<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8M Nano GPU Profiling running AOSP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Nano-GPU-Profiling-running-AOSP/m-p/1449010#M189695</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using iMX8M Nano and AOSP 9.0.&lt;BR /&gt;I am running the TF Lite application for object detection using a USB camera.&lt;/P&gt;&lt;P&gt;I need to analyze the GPU usage of the application.&lt;/P&gt;&lt;P&gt;I tried the 'dumpsys gfxinfo' with the package name. But I am unable to get GPU usage of the application from the output.&lt;/P&gt;&lt;P&gt;I would need the following information:&lt;BR /&gt;1. runtime GPU usage of specific application&lt;BR /&gt;2. Overall GPU usage&lt;/P&gt;&lt;P&gt;Is there any way to get the overall and/or application-specific GPU usage on AOSP?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sudhir&lt;/P&gt;</description>
    <pubDate>Tue, 26 Apr 2022 07:30:51 GMT</pubDate>
    <dc:creator>sudhir_r</dc:creator>
    <dc:date>2022-04-26T07:30:51Z</dc:date>
    <item>
      <title>iMX8M Nano GPU Profiling running AOSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Nano-GPU-Profiling-running-AOSP/m-p/1449010#M189695</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using iMX8M Nano and AOSP 9.0.&lt;BR /&gt;I am running the TF Lite application for object detection using a USB camera.&lt;/P&gt;&lt;P&gt;I need to analyze the GPU usage of the application.&lt;/P&gt;&lt;P&gt;I tried the 'dumpsys gfxinfo' with the package name. But I am unable to get GPU usage of the application from the output.&lt;/P&gt;&lt;P&gt;I would need the following information:&lt;BR /&gt;1. runtime GPU usage of specific application&lt;BR /&gt;2. Overall GPU usage&lt;/P&gt;&lt;P&gt;Is there any way to get the overall and/or application-specific GPU usage on AOSP?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sudhir&lt;/P&gt;</description>
      <pubDate>Tue, 26 Apr 2022 07:30:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Nano-GPU-Profiling-running-AOSP/m-p/1449010#M189695</guid>
      <dc:creator>sudhir_r</dc:creator>
      <dc:date>2022-04-26T07:30:51Z</dc:date>
    </item>
  </channel>
</rss>