<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to change the default Camera in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-change-the-default-Camera/m-p/236824#M18956</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two EVBs, which are MCiMX6Q-SDP and MCiMX6Q-SDB. I installed the camera, which comes from the MCiMX6Q-SDP, on the front camera port (J9)of the MCiMX6Q-SDB. Because the default camera is the rear camera (J5), I still can't start the camera function after I installed the camera on the MCiMX6Q-SDB. How can I change the default camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Phillip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 May 2013 08:35:27 GMT</pubDate>
    <dc:creator>phillipchen</dc:creator>
    <dc:date>2013-05-14T08:35:27Z</dc:date>
    <item>
      <title>How to change the default Camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-change-the-default-Camera/m-p/236824#M18956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two EVBs, which are MCiMX6Q-SDP and MCiMX6Q-SDB. I installed the camera, which comes from the MCiMX6Q-SDP, on the front camera port (J9)of the MCiMX6Q-SDB. Because the default camera is the rear camera (J5), I still can't start the camera function after I installed the camera on the MCiMX6Q-SDB. How can I change the default camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Phillip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2013 08:35:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-change-the-default-Camera/m-p/236824#M18956</guid>
      <dc:creator>phillipchen</dc:creator>
      <dc:date>2013-05-14T08:35:27Z</dc:date>
    </item>
  </channel>
</rss>