<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKernel panic when using cpio.gz.u-boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-when-using-cpio-gz-u-boot/m-p/1446375#M189522</link>
    <description>&lt;P&gt;Our custom board is using iMX8MM with 1GB LPDDR4. Yocto is HardKnott version. We want to use example_kernel_emmc.uuu to program the custom board. The RAM size and the lpddr4 timing have been updated in both U-boot and kernel. However, the cpio.gz.u-boot produced by "bitbake fsl-image-mfgtool-initramfs" does not work. Below is the log. (We also use NXP pre-built file to test, but get the same kernel panic.) Please advise.&lt;/P&gt;&lt;P&gt;U-Boot SPL 2021.04-5.10.35-2.0.0+g3463140881 (Jan 26 2022 - 13:02:27 +0800)&lt;BR /&gt;Can't find PMIC:PCA9450&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 3000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from USB SDP&lt;BR /&gt;g_dnl_register: g_dnl_driver.name = usb_dnl_sdp&lt;BR /&gt;g_dnl_bind: gadget: 0x7f9398 cdev: 0x42200490&lt;BR /&gt;usb_add_config: adding config #1 'usb_dnload'/42200540&lt;BR /&gt;g_dnl_do_config: configuration: 0x42200540 composite dev: 0x42200490&lt;BR /&gt;adding 'sdp'/42200680 to config 'usb_dnload'/42200540&lt;BR /&gt;cfg 1/42200540 speeds: high full&lt;BR /&gt;usb_add_config: interface 0 = sdp/42200680&lt;BR /&gt;g_dnl_bind: calling usb_gadget_connect for controller 'ci_udc'&lt;BR /&gt;usb_dnl_sdp: ready&lt;BR /&gt;SDP: initialize...&lt;BR /&gt;set_config: high speed config #1: usb_dnload&lt;BR /&gt;non-core control req21.0a v0000 i0000 l0&lt;BR /&gt;non-core control req81.06 v2200 i0000 l140&lt;BR /&gt;SDP: handle requests...&lt;BR /&gt;Downloading file of size 1148688 to 0x40400000... done&lt;BR /&gt;Jumping to header at 0x40400000&lt;BR /&gt;Header Tag is not an IMX image&lt;BR /&gt;Found header at 0x40428ba0&lt;BR /&gt;NOTICE: BL31: v2.2(release):rel_imx_5.4.70_2.3.2_rc1-0-g2a2678646&lt;BR /&gt;NOTICE: BL31: Built : 08:21:41, Jan 20 2022&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2021.04-5.10.35-2.0.0+g3463140881 (Jan 26 2022 - 13:02:27 +0800)&lt;/P&gt;&lt;P&gt;alloc space exhausted&lt;BR /&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 52C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM EVK board&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;tcpc_init: Can't find device id=0x52&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-19&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port1 init failed, err=-19&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... MMC: no card present&lt;BR /&gt;*** Warning - No block device, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;SEC0: RNG instantiated&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF 2a26786&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Net: Could not get PHY for FEC0: addr 0&lt;BR /&gt;Could not get PHY for FEC0: addr 0&lt;BR /&gt;No ethernet found.&lt;/P&gt;&lt;P&gt;Fastboot: Normal&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;*** Warning - Use default environment for mfgtools&lt;BR /&gt;, using default environment&lt;/P&gt;&lt;P&gt;Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;## Checking Image at 43800000 ...&lt;BR /&gt;Legacy image found&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-imx8&lt;BR /&gt;Created: 2011-04-05 23:00:00 UTC&lt;BR /&gt;Image Type: AArch64 Linux RAMDisk Image (uncompressed)&lt;BR /&gt;Data Size: 14921573 Bytes = 14.2 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... Bad Data CRC&lt;BR /&gt;Run fastboot ...&lt;BR /&gt;g_dnl_register: g_dnl_driver.name = usb_dnl_fastboot&lt;BR /&gt;g_dnl_bind: gadget: 0x000000007ffc2b18 cdev: 0x000000007df1af90&lt;BR /&gt;usb_add_config: adding config #1 'usb_dnload'/000000007df1b040&lt;BR /&gt;g_dnl_do_config: configuration: 0x000000007df1b040 composite dev: 0x000000007df1af90&lt;BR /&gt;adding 'f_fastboot'/000000007df1b180 to config 'usb_dnload'/000000007df1b040&lt;BR /&gt;cfg 1/000000007df1b040 speeds: high full&lt;BR /&gt;usb_add_config: interface 0 = f_fastboot/000000007df1b180&lt;BR /&gt;g_dnl_bind: calling usb_gadget_connect for controller 'ci_udc'&lt;BR /&gt;usb_dnl_fastboot: ready&lt;BR /&gt;set_config: high speed config #1: usb_dnload&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;MMC: no card present&lt;BR /&gt;MMC card init failed!&lt;BR /&gt;MMC: no card present&lt;BR /&gt;** Block device MMC 1 not supported&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Starting download of 1341296 bytes&lt;BR /&gt;..........&lt;BR /&gt;downloading of 1341296 bytes finished&lt;BR /&gt;writing to partition 'bootloader'&lt;BR /&gt;Initializing 'bootloader'&lt;BR /&gt;switch to partitions #1, OK&lt;BR /&gt;mmc2(part 1) is current device&lt;BR /&gt;Writing 'bootloader'&lt;/P&gt;&lt;P&gt;MMC write: dev # 2, block # 66, count 2620 ... 2620 blocks written: OK&lt;BR /&gt;Writing 'bootloader' DONE!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Starting download of 29491712 bytes&lt;BR /&gt;..........................................................................&lt;BR /&gt;..........................................................................&lt;BR /&gt;..........................................................................&lt;BR /&gt;...&lt;BR /&gt;downloading of 29491712 bytes finished&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Starting download of 40863 bytes&lt;/P&gt;&lt;P&gt;downloading of 40863 bytes finished&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Starting download of 14921637 bytes&lt;BR /&gt;..........................................................................&lt;BR /&gt;.......................................&lt;BR /&gt;downloading of 14921637 bytes finished&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Moving Image from 0x40480000 to 0x40600000, end=422b0000&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 43800000 ...&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-imx8&lt;BR /&gt;Created: 2011-04-05 23:00:00 UTC&lt;BR /&gt;Image Type: AArch64 Linux RAMDisk Image (uncompressed)&lt;BR /&gt;Data Size: 14921573 Bytes = 14.2 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt;Booting using the fdt blob at 0x43000000&lt;BR /&gt;Using Device Tree in place at 0000000043000000, end 000000004300cf9e&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]&lt;BR /&gt;[ 0.000000] Linux version 5.10.35+gef3f2cfc6010 (micom@micom-ESPRIMO-E420) (aarch64-poky-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.36.1.20210209) #31 SMP PREEMPT Thu Apr 14 17:01:22 HKT 2022&lt;BR /&gt;[ 0.000000] Machine model: FSL i.MX8MM EVK board&lt;BR /&gt;[ 0.000000] efi: UEFI not found.&lt;BR /&gt;[ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma'&lt;BR /&gt;[ 0.000000] cma: Reserved 32 MiB at 0x000000007e000000&lt;BR /&gt;[ 0.000000] NUMA: No NUMA configuration found&lt;BR /&gt;[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x000000007fffffff]&lt;BR /&gt;[ 0.000000] NUMA: NODE_DATA [mem 0x7ddd1700-0x7ddd3fff]&lt;BR /&gt;[ 0.000000] Zone ranges:&lt;BR /&gt;[ 0.000000] DMA [mem 0x0000000040000000-0x000000007fffffff]&lt;BR /&gt;[ 0.000000] DMA32 empty&lt;BR /&gt;[ 0.000000] Normal empty&lt;BR /&gt;[ 0.000000] Movable zone start for each node&lt;BR /&gt;[ 0.000000] Early memory node ranges&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000040000000-0x000000007fffffff]&lt;BR /&gt;[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x000000007fffffff]&lt;BR /&gt;[ 0.000000] psci: probing for conduit method from DT.&lt;BR /&gt;[ 0.000000] psci: PSCIv1.1 detected in firmware.&lt;BR /&gt;[ 0.000000] psci: Using standard PSCI v0.2 function IDs&lt;BR /&gt;[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.&lt;BR /&gt;[ 0.000000] psci: SMC Calling Convention v1.1&lt;BR /&gt;[ 0.000000] percpu: Embedded 23 pages/cpu s56280 r8192 d29736 u94208&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;BR /&gt;[ 0.000000] CPU features: detected: ARM erratum 845719&lt;BR /&gt;[ 0.000000] CPU features: detected: GIC system register CPU interface&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 258048&lt;BR /&gt;[ 0.000000] Policy zone: DMA&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttymxc1,115200,115200 rdinit=/linuxrc clk_ignore_unused&lt;BR /&gt;[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)&lt;BR /&gt;[ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)&lt;BR /&gt;[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off&lt;BR /&gt;[ 0.000000] Memory: 951284K/1048576K available (17536K kernel code, 1472K rwdata, 6780K rodata, 2880K init, 545K bss, 64524K reserved, 32768K cma-reserved)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;[ 0.000000] rcu: Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] rcu: RCU event tracing is enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.&lt;BR /&gt;[ 0.000000] Trampoline variant of Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.&lt;BR /&gt;[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4&lt;BR /&gt;[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0&lt;BR /&gt;[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode&lt;BR /&gt;[ 0.000000] GICv3: 128 SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: 0 Extended SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: Distributor has no Range Selector support&lt;BR /&gt;[ 0.000000] GICv3: 16 PPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000&lt;BR /&gt;[ 0.000000] ITS: No ITS available, not enabling LPIs&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0x330/0x4f4 with crng_init=0&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns&lt;BR /&gt;[ 0.000004] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns&lt;BR /&gt;[ 0.000293] Console: colour dummy device 80x25&lt;BR /&gt;[ 0.000364] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)&lt;BR /&gt;[ 0.000377] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.000442] LSM: Security Framework initializing&lt;BR /&gt;[ 0.000492] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.000504] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.001750] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.002586] EFI services will not be available.&lt;BR /&gt;[ 0.002756] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 0.003106] Detected VIPT I-cache on CPU1&lt;BR /&gt;[ 0.003132] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000&lt;BR /&gt;[ 0.003178] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]&lt;BR /&gt;[ 0.003584] Detected VIPT I-cache on CPU2&lt;BR /&gt;[ 0.003602] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000&lt;BR /&gt;[ 0.003627] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]&lt;BR /&gt;[ 0.004054] Detected VIPT I-cache on CPU3&lt;BR /&gt;[ 0.004072] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000&lt;BR /&gt;[ 0.004094] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]&lt;BR /&gt;[ 0.004150] smp: Brought up 1 node, 4 CPUs&lt;BR /&gt;[ 0.004163] SMP: Total of 4 processors activated.&lt;BR /&gt;[ 0.004172] CPU features: detected: 32-bit EL0 Support&lt;BR /&gt;[ 0.004178] CPU features: detected: CRC32 instructions&lt;BR /&gt;[ 0.004186] CPU features: detected: 32-bit EL1 Support&lt;BR /&gt;[ 0.012510] CPU: All CPU(s) started at EL2&lt;BR /&gt;[ 0.012533] alternatives: patching kernel code&lt;BR /&gt;[ 0.013650] devtmpfs: initialized&lt;BR /&gt;[ 0.018811] KASLR disabled due to lack of seed&lt;BR /&gt;[ 0.018970] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns&lt;BR /&gt;[ 0.018985] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)&lt;BR /&gt;[ 0.020109] pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;[ 0.020619] DMI not present or invalid.&lt;BR /&gt;[ 0.021011] NET: Registered protocol family 16&lt;BR /&gt;[ 0.027856] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations&lt;BR /&gt;[ 0.028754] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations&lt;BR /&gt;[ 0.029628] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations&lt;BR /&gt;[ 0.029721] audit: initializing netlink subsys (disabled)&lt;BR /&gt;[ 0.029954] audit: type=2000 audit(0.028:1): state=initialized audit_enabled=0 res=1&lt;BR /&gt;[ 0.030517] thermal_sys: Registered thermal governor 'step_wise'&lt;BR /&gt;[ 0.030521] thermal_sys: Registered thermal governor 'power_allocator'&lt;BR /&gt;[ 0.030719] cpuidle: using governor menu&lt;BR /&gt;[ 0.030887] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.&lt;BR /&gt;[ 0.030968] ASID allocator initialised with 65536 entries&lt;BR /&gt;[ 0.031757] Serial: AMBA PL011 UART driver&lt;BR /&gt;[ 0.031813] imx mu driver is registered.&lt;BR /&gt;[ 0.031835] imx rpmsg driver is registered.&lt;BR /&gt;[ 0.054775] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/pdmgrp&lt;BR /&gt;[ 0.054803] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai1grp&lt;BR /&gt;[ 0.054819] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai1grp_dsd&lt;BR /&gt;[ 0.054837] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai2grp&lt;BR /&gt;[ 0.054851] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai3grp&lt;BR /&gt;[ 0.054867] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai5grp&lt;BR /&gt;[ 0.054912] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/usdhc2grpgpiogrp&lt;BR /&gt;[ 0.054940] imx8mm-pinctrl 30330000.pinctrl: no fsl,pins and pins property in node /soc@0/bus@30000000/pinctrl@30330000/lexi-imx8mm-gpio&lt;BR /&gt;[ 0.054965] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.071087] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.071101] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.071109] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.071117] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.072033] cryptd: max_cpu_qlen set to 1000&lt;BR /&gt;[ 0.074923] ACPI: Interpreter disabled.&lt;BR /&gt;[ 0.075463] iommu: Default domain type: Translated&lt;BR /&gt;[ 0.075606] vgaarb: loaded&lt;BR /&gt;[ 0.075908] SCSI subsystem initialized&lt;BR /&gt;[ 0.076217] usbcore: registered new interface driver usbfs&lt;BR /&gt;[ 0.076251] usbcore: registered new interface driver hub&lt;BR /&gt;[ 0.076277] usbcore: registered new device driver usb&lt;BR /&gt;[ 0.077251] mc: Linux media interface: v0.10&lt;BR /&gt;[ 0.077291] videodev: Linux video capture interface: v2.00&lt;BR /&gt;[ 0.077356] pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;[ 0.077363] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;giometti@linux.it&amp;gt;&lt;BR /&gt;[ 0.077377] PTP clock support registered&lt;BR /&gt;[ 0.077505] EDAC MC: Ver: 3.0.0&lt;BR /&gt;[ 0.078412] FPGA manager framework&lt;BR /&gt;[ 0.078486] Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;[ 0.079066] Bluetooth: Core ver 2.22&lt;BR /&gt;[ 0.079094] NET: Registered protocol family 31&lt;BR /&gt;[ 0.079100] Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;[ 0.079112] Bluetooth: HCI socket layer initialized&lt;BR /&gt;[ 0.079121] Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;[ 0.079136] Bluetooth: SCO socket layer initialized&lt;BR /&gt;[ 0.079752] clocksource: Switched to clocksource arch_sys_counter&lt;BR /&gt;[ 0.080034] VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;[ 0.080081] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)&lt;BR /&gt;[ 0.080253] pnp: PnP ACPI: disabled&lt;BR /&gt;[ 0.085882] NET: Registered protocol family 2&lt;BR /&gt;[ 0.086255] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)&lt;BR /&gt;[ 0.086280] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)&lt;BR /&gt;[ 0.086366] TCP bind hash table entries: 8192 (order: 5, 131072 bytes, linear)&lt;BR /&gt;[ 0.086480] TCP: Hash tables configured (established 8192 bind 8192)&lt;BR /&gt;[ 0.086559] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.086586] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.086697] NET: Registered protocol family 1&lt;BR /&gt;[ 0.086983] RPC: Registered named UNIX socket transport module.&lt;BR /&gt;[ 0.086989] RPC: Registered udp transport module.&lt;BR /&gt;[ 0.086995] RPC: Registered tcp transport module.&lt;BR /&gt;[ 0.087002] RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;[ 0.087702] PCI: CLS 0 bytes, default 64&lt;BR /&gt;[ 0.087899] Unpacking initramfs...&lt;BR /&gt;[ 0.795563] Freeing initrd memory: 14564K&lt;BR /&gt;[ 0.796278] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available&lt;BR /&gt;[ 0.796858] kvm [1]: IPA Size Limit: 40 bits&lt;BR /&gt;[ 0.798192] kvm [1]: GICv3: no GICV resource entry&lt;BR /&gt;[ 0.798198] kvm [1]: disabling GICv2 emulation&lt;BR /&gt;[ 0.798218] kvm [1]: GIC system register CPU interface enabled&lt;BR /&gt;[ 0.798287] kvm [1]: vgic interrupt IRQ9&lt;BR /&gt;[ 0.798399] kvm [1]: Hyp mode initialized successfully&lt;BR /&gt;[ 0.801376] Initialise system trusted keyrings&lt;BR /&gt;[ 0.801510] workingset: timestamp_bits=42 max_order=18 bucket_order=0&lt;BR /&gt;[ 0.806983] squashfs: version 4.0 (2009/01/31) Phillip Lougher&lt;BR /&gt;[ 0.807567] NFS: Registering the id_resolver key type&lt;BR /&gt;[ 0.807594] Key type id_resolver registered&lt;BR /&gt;[ 0.807600] Key type id_legacy registered&lt;BR /&gt;[ 0.807675] nfs4filelayout_init: NFSv4 File Layout Driver Registering...&lt;BR /&gt;[ 0.807682] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...&lt;BR /&gt;[ 0.807702] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;[ 0.808075] 9p: Installing v9fs 9p2000 file system support&lt;BR /&gt;[ 0.845249] Key type asymmetric registered&lt;BR /&gt;[ 0.845258] Asymmetric key parser 'x509' registered&lt;BR /&gt;[ 0.845293] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)&lt;BR /&gt;[ 0.845301] io scheduler mq-deadline registered&lt;BR /&gt;[ 0.845306] io scheduler kyber registered&lt;BR /&gt;[ 0.850226] EINJ: ACPI disabled.&lt;BR /&gt;[ 0.858724] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2&lt;BR /&gt;[ 0.858740] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin&lt;BR /&gt;[ 0.866343] mxs-dma 33000000.dma-controller: initialized&lt;BR /&gt;[ 0.868105] Bus freq driver module loaded&lt;BR /&gt;[ 0.873263] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled&lt;BR /&gt;[ 0.875356] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 39, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 0.875992] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 40, base_baud = 5000000) is a IMX&lt;BR /&gt;[ 0.876518] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 41, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.963903] printk: console [ttymxc1] enabled&lt;BR /&gt;[ 1.968768] Internal error: synchronous external abort: 96000210 [#1] PREEMPT SMP&lt;BR /&gt;[ 1.976251] Modules linked in:&lt;BR /&gt;[ 1.979314] CPU: 3 PID: 1 Comm: swapper/0 Not tainted 5.10.35+gef3f2cfc6010 #31&lt;BR /&gt;[ 1.986622] Hardware name: FSL i.MX8MM EVK board (DT)&lt;BR /&gt;[ 1.991675] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[ 1.997688] pc : imx_uart_probe+0x2c0/0x7e4&lt;BR /&gt;[ 2.001873] lr : imx_uart_probe+0x2b0/0x7e4&lt;BR /&gt;[ 2.006055] sp : ffff800011cdbb50&lt;BR /&gt;[ 2.009369] x29: ffff800011cdbb50 x28: 0000000000000000&lt;BR /&gt;[ 2.014686] x27: ffff8000117e04e0 x26: ffff00000634b400&lt;BR /&gt;[ 2.020003] x25: 00000000fffffffa x24: 00000000fffffffa&lt;BR /&gt;[ 2.025321] x23: 000000000000002d x22: ffff000006291810&lt;BR /&gt;[ 2.030636] x21: ffff000006291800 x20: 0000000000000000&lt;BR /&gt;[ 2.035951] x19: ffff000006952080 x18: 0000000000000020&lt;BR /&gt;[ 2.041266] x17: 0000000000000000 x16: 0000000000000001&lt;BR /&gt;[ 2.046581] x15: ffff000006080478 x14: ffffffffffffffff&lt;BR /&gt;[ 2.051896] x13: 0000000000000038 x12: 0101010101010101&lt;BR /&gt;[ 2.057214] x11: 0000000000000020 x10: 0101010101010101&lt;BR /&gt;[ 2.062531] x9 : 0000000000000000 x8 : ffff00000634b500&lt;BR /&gt;[ 2.067846] x7 : 0000000000000000 x6 : 000000000000003f&lt;BR /&gt;[ 2.073161] x5 : 0000000000000080 x4 : 0000000000000000&lt;BR /&gt;[ 2.078476] x3 : 0000000000000000 x2 : 0000000000000000&lt;BR /&gt;[ 2.083791] x1 : ffff800012480080 x0 : 0000000000000000&lt;BR /&gt;[ 2.089106] Call trace:&lt;BR /&gt;[ 2.091555] imx_uart_probe+0x2c0/0x7e4&lt;BR /&gt;[ 2.095394] platform_drv_probe+0x54/0xb0&lt;BR /&gt;[ 2.099404] really_probe+0xe4/0x4c0&lt;BR /&gt;[ 2.102981] driver_probe_device+0x58/0xc0&lt;BR /&gt;[ 2.107079] device_driver_attach+0xc0/0xd0&lt;BR /&gt;[ 2.111263] __driver_attach+0x84/0x124&lt;BR /&gt;[ 2.115100] bus_for_each_dev+0x70/0xc0&lt;BR /&gt;[ 2.118938] driver_attach+0x24/0x30&lt;BR /&gt;[ 2.122514] bus_add_driver+0x104/0x1ec&lt;BR /&gt;[ 2.126350] driver_register+0x78/0x130&lt;BR /&gt;[ 2.130186] __platform_driver_register+0x4c/0x60&lt;BR /&gt;[ 2.134893] imx_uart_init+0x3c/0x64&lt;BR /&gt;[ 2.138470] do_one_initcall+0x54/0x1bc&lt;BR /&gt;[ 2.142309] kernel_init_freeable+0x1d4/0x23c&lt;BR /&gt;[ 2.146667] kernel_init+0x14/0x118&lt;BR /&gt;[ 2.150158] ret_from_fork+0x10/0x30&lt;BR /&gt;[ 2.153738] Code: 2a0003f4 35001d40 f9400a61 91020021 (b9400021)&lt;BR /&gt;[ 2.159842] ---[ end trace d132e31f7226938a ]---&lt;BR /&gt;[ 2.164506] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b&lt;BR /&gt;[ 2.172164] SMP: stopping secondary CPUs&lt;BR /&gt;[ 2.176092] Kernel Offset: disabled&lt;BR /&gt;[ 2.179581] CPU features: 0x0240002,2000200c&lt;BR /&gt;[ 2.183850] Memory Limit: none&lt;BR /&gt;[ 2.186908] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b ]---&lt;/P&gt;</description>
    <pubDate>Wed, 20 Apr 2022 11:20:05 GMT</pubDate>
    <dc:creator>raymondman</dc:creator>
    <dc:date>2022-04-20T11:20:05Z</dc:date>
    <item>
      <title>Kernel panic when using cpio.gz.u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-when-using-cpio-gz-u-boot/m-p/1446375#M189522</link>
      <description>&lt;P&gt;Our custom board is using iMX8MM with 1GB LPDDR4. Yocto is HardKnott version. We want to use example_kernel_emmc.uuu to program the custom board. The RAM size and the lpddr4 timing have been updated in both U-boot and kernel. However, the cpio.gz.u-boot produced by "bitbake fsl-image-mfgtool-initramfs" does not work. Below is the log. (We also use NXP pre-built file to test, but get the same kernel panic.) Please advise.&lt;/P&gt;&lt;P&gt;U-Boot SPL 2021.04-5.10.35-2.0.0+g3463140881 (Jan 26 2022 - 13:02:27 +0800)&lt;BR /&gt;Can't find PMIC:PCA9450&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 3000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from USB SDP&lt;BR /&gt;g_dnl_register: g_dnl_driver.name = usb_dnl_sdp&lt;BR /&gt;g_dnl_bind: gadget: 0x7f9398 cdev: 0x42200490&lt;BR /&gt;usb_add_config: adding config #1 'usb_dnload'/42200540&lt;BR /&gt;g_dnl_do_config: configuration: 0x42200540 composite dev: 0x42200490&lt;BR /&gt;adding 'sdp'/42200680 to config 'usb_dnload'/42200540&lt;BR /&gt;cfg 1/42200540 speeds: high full&lt;BR /&gt;usb_add_config: interface 0 = sdp/42200680&lt;BR /&gt;g_dnl_bind: calling usb_gadget_connect for controller 'ci_udc'&lt;BR /&gt;usb_dnl_sdp: ready&lt;BR /&gt;SDP: initialize...&lt;BR /&gt;set_config: high speed config #1: usb_dnload&lt;BR /&gt;non-core control req21.0a v0000 i0000 l0&lt;BR /&gt;non-core control req81.06 v2200 i0000 l140&lt;BR /&gt;SDP: handle requests...&lt;BR /&gt;Downloading file of size 1148688 to 0x40400000... done&lt;BR /&gt;Jumping to header at 0x40400000&lt;BR /&gt;Header Tag is not an IMX image&lt;BR /&gt;Found header at 0x40428ba0&lt;BR /&gt;NOTICE: BL31: v2.2(release):rel_imx_5.4.70_2.3.2_rc1-0-g2a2678646&lt;BR /&gt;NOTICE: BL31: Built : 08:21:41, Jan 20 2022&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2021.04-5.10.35-2.0.0+g3463140881 (Jan 26 2022 - 13:02:27 +0800)&lt;/P&gt;&lt;P&gt;alloc space exhausted&lt;BR /&gt;CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 52C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MM EVK board&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;tcpc_init: Can't find device id=0x52&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-19&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port1 init failed, err=-19&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... MMC: no card present&lt;BR /&gt;*** Warning - No block device, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;SEC0: RNG instantiated&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF 2a26786&lt;/P&gt;&lt;P&gt;MMC: no card present&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Net: Could not get PHY for FEC0: addr 0&lt;BR /&gt;Could not get PHY for FEC0: addr 0&lt;BR /&gt;No ethernet found.&lt;/P&gt;&lt;P&gt;Fastboot: Normal&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;*** Warning - Use default environment for mfgtools&lt;BR /&gt;, using default environment&lt;/P&gt;&lt;P&gt;Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;## Checking Image at 43800000 ...&lt;BR /&gt;Legacy image found&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-imx8&lt;BR /&gt;Created: 2011-04-05 23:00:00 UTC&lt;BR /&gt;Image Type: AArch64 Linux RAMDisk Image (uncompressed)&lt;BR /&gt;Data Size: 14921573 Bytes = 14.2 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... Bad Data CRC&lt;BR /&gt;Run fastboot ...&lt;BR /&gt;g_dnl_register: g_dnl_driver.name = usb_dnl_fastboot&lt;BR /&gt;g_dnl_bind: gadget: 0x000000007ffc2b18 cdev: 0x000000007df1af90&lt;BR /&gt;usb_add_config: adding config #1 'usb_dnload'/000000007df1b040&lt;BR /&gt;g_dnl_do_config: configuration: 0x000000007df1b040 composite dev: 0x000000007df1af90&lt;BR /&gt;adding 'f_fastboot'/000000007df1b180 to config 'usb_dnload'/000000007df1b040&lt;BR /&gt;cfg 1/000000007df1b040 speeds: high full&lt;BR /&gt;usb_add_config: interface 0 = f_fastboot/000000007df1b180&lt;BR /&gt;g_dnl_bind: calling usb_gadget_connect for controller 'ci_udc'&lt;BR /&gt;usb_dnl_fastboot: ready&lt;BR /&gt;set_config: high speed config #1: usb_dnload&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;MMC: no card present&lt;BR /&gt;MMC card init failed!&lt;BR /&gt;MMC: no card present&lt;BR /&gt;** Block device MMC 1 not supported&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Starting download of 1341296 bytes&lt;BR /&gt;..........&lt;BR /&gt;downloading of 1341296 bytes finished&lt;BR /&gt;writing to partition 'bootloader'&lt;BR /&gt;Initializing 'bootloader'&lt;BR /&gt;switch to partitions #1, OK&lt;BR /&gt;mmc2(part 1) is current device&lt;BR /&gt;Writing 'bootloader'&lt;/P&gt;&lt;P&gt;MMC write: dev # 2, block # 66, count 2620 ... 2620 blocks written: OK&lt;BR /&gt;Writing 'bootloader' DONE!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Starting download of 29491712 bytes&lt;BR /&gt;..........................................................................&lt;BR /&gt;..........................................................................&lt;BR /&gt;..........................................................................&lt;BR /&gt;...&lt;BR /&gt;downloading of 29491712 bytes finished&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Starting download of 40863 bytes&lt;/P&gt;&lt;P&gt;downloading of 40863 bytes finished&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Starting download of 14921637 bytes&lt;BR /&gt;..........................................................................&lt;BR /&gt;.......................................&lt;BR /&gt;downloading of 14921637 bytes finished&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Moving Image from 0x40480000 to 0x40600000, end=422b0000&lt;BR /&gt;## Loading init Ramdisk from Legacy Image at 43800000 ...&lt;BR /&gt;Image Name: fsl-image-mfgtool-initramfs-imx8&lt;BR /&gt;Created: 2011-04-05 23:00:00 UTC&lt;BR /&gt;Image Type: AArch64 Linux RAMDisk Image (uncompressed)&lt;BR /&gt;Data Size: 14921573 Bytes = 14.2 MiB&lt;BR /&gt;Load Address: 00000000&lt;BR /&gt;Entry Point: 00000000&lt;BR /&gt;Verifying Checksum ... OK&lt;BR /&gt;## Flattened Device Tree blob at 43000000&lt;BR /&gt;Booting using the fdt blob at 0x43000000&lt;BR /&gt;Using Device Tree in place at 0000000043000000, end 000000004300cf9e&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]&lt;BR /&gt;[ 0.000000] Linux version 5.10.35+gef3f2cfc6010 (micom@micom-ESPRIMO-E420) (aarch64-poky-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.36.1.20210209) #31 SMP PREEMPT Thu Apr 14 17:01:22 HKT 2022&lt;BR /&gt;[ 0.000000] Machine model: FSL i.MX8MM EVK board&lt;BR /&gt;[ 0.000000] efi: UEFI not found.&lt;BR /&gt;[ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma'&lt;BR /&gt;[ 0.000000] cma: Reserved 32 MiB at 0x000000007e000000&lt;BR /&gt;[ 0.000000] NUMA: No NUMA configuration found&lt;BR /&gt;[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x000000007fffffff]&lt;BR /&gt;[ 0.000000] NUMA: NODE_DATA [mem 0x7ddd1700-0x7ddd3fff]&lt;BR /&gt;[ 0.000000] Zone ranges:&lt;BR /&gt;[ 0.000000] DMA [mem 0x0000000040000000-0x000000007fffffff]&lt;BR /&gt;[ 0.000000] DMA32 empty&lt;BR /&gt;[ 0.000000] Normal empty&lt;BR /&gt;[ 0.000000] Movable zone start for each node&lt;BR /&gt;[ 0.000000] Early memory node ranges&lt;BR /&gt;[ 0.000000] node 0: [mem 0x0000000040000000-0x000000007fffffff]&lt;BR /&gt;[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x000000007fffffff]&lt;BR /&gt;[ 0.000000] psci: probing for conduit method from DT.&lt;BR /&gt;[ 0.000000] psci: PSCIv1.1 detected in firmware.&lt;BR /&gt;[ 0.000000] psci: Using standard PSCI v0.2 function IDs&lt;BR /&gt;[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.&lt;BR /&gt;[ 0.000000] psci: SMC Calling Convention v1.1&lt;BR /&gt;[ 0.000000] percpu: Embedded 23 pages/cpu s56280 r8192 d29736 u94208&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;BR /&gt;[ 0.000000] CPU features: detected: ARM erratum 845719&lt;BR /&gt;[ 0.000000] CPU features: detected: GIC system register CPU interface&lt;BR /&gt;[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 258048&lt;BR /&gt;[ 0.000000] Policy zone: DMA&lt;BR /&gt;[ 0.000000] Kernel command line: console=ttymxc1,115200,115200 rdinit=/linuxrc clk_ignore_unused&lt;BR /&gt;[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)&lt;BR /&gt;[ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)&lt;BR /&gt;[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off&lt;BR /&gt;[ 0.000000] Memory: 951284K/1048576K available (17536K kernel code, 1472K rwdata, 6780K rodata, 2880K init, 545K bss, 64524K reserved, 32768K cma-reserved)&lt;BR /&gt;[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;[ 0.000000] rcu: Preemptible hierarchical RCU implementation.&lt;BR /&gt;[ 0.000000] rcu: RCU event tracing is enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.&lt;BR /&gt;[ 0.000000] Trampoline variant of Tasks RCU enabled.&lt;BR /&gt;[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.&lt;BR /&gt;[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4&lt;BR /&gt;[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0&lt;BR /&gt;[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode&lt;BR /&gt;[ 0.000000] GICv3: 128 SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: 0 Extended SPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: Distributor has no Range Selector support&lt;BR /&gt;[ 0.000000] GICv3: 16 PPIs implemented&lt;BR /&gt;[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000&lt;BR /&gt;[ 0.000000] ITS: No ITS available, not enabling LPIs&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0x330/0x4f4 with crng_init=0&lt;BR /&gt;[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).&lt;BR /&gt;[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns&lt;BR /&gt;[ 0.000004] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns&lt;BR /&gt;[ 0.000293] Console: colour dummy device 80x25&lt;BR /&gt;[ 0.000364] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)&lt;BR /&gt;[ 0.000377] pid_max: default: 32768 minimum: 301&lt;BR /&gt;[ 0.000442] LSM: Security Framework initializing&lt;BR /&gt;[ 0.000492] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.000504] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.001750] rcu: Hierarchical SRCU implementation.&lt;BR /&gt;[ 0.002586] EFI services will not be available.&lt;BR /&gt;[ 0.002756] smp: Bringing up secondary CPUs ...&lt;BR /&gt;[ 0.003106] Detected VIPT I-cache on CPU1&lt;BR /&gt;[ 0.003132] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000&lt;BR /&gt;[ 0.003178] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]&lt;BR /&gt;[ 0.003584] Detected VIPT I-cache on CPU2&lt;BR /&gt;[ 0.003602] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000&lt;BR /&gt;[ 0.003627] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]&lt;BR /&gt;[ 0.004054] Detected VIPT I-cache on CPU3&lt;BR /&gt;[ 0.004072] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000&lt;BR /&gt;[ 0.004094] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]&lt;BR /&gt;[ 0.004150] smp: Brought up 1 node, 4 CPUs&lt;BR /&gt;[ 0.004163] SMP: Total of 4 processors activated.&lt;BR /&gt;[ 0.004172] CPU features: detected: 32-bit EL0 Support&lt;BR /&gt;[ 0.004178] CPU features: detected: CRC32 instructions&lt;BR /&gt;[ 0.004186] CPU features: detected: 32-bit EL1 Support&lt;BR /&gt;[ 0.012510] CPU: All CPU(s) started at EL2&lt;BR /&gt;[ 0.012533] alternatives: patching kernel code&lt;BR /&gt;[ 0.013650] devtmpfs: initialized&lt;BR /&gt;[ 0.018811] KASLR disabled due to lack of seed&lt;BR /&gt;[ 0.018970] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns&lt;BR /&gt;[ 0.018985] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)&lt;BR /&gt;[ 0.020109] pinctrl core: initialized pinctrl subsystem&lt;BR /&gt;[ 0.020619] DMI not present or invalid.&lt;BR /&gt;[ 0.021011] NET: Registered protocol family 16&lt;BR /&gt;[ 0.027856] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations&lt;BR /&gt;[ 0.028754] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations&lt;BR /&gt;[ 0.029628] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations&lt;BR /&gt;[ 0.029721] audit: initializing netlink subsys (disabled)&lt;BR /&gt;[ 0.029954] audit: type=2000 audit(0.028:1): state=initialized audit_enabled=0 res=1&lt;BR /&gt;[ 0.030517] thermal_sys: Registered thermal governor 'step_wise'&lt;BR /&gt;[ 0.030521] thermal_sys: Registered thermal governor 'power_allocator'&lt;BR /&gt;[ 0.030719] cpuidle: using governor menu&lt;BR /&gt;[ 0.030887] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.&lt;BR /&gt;[ 0.030968] ASID allocator initialised with 65536 entries&lt;BR /&gt;[ 0.031757] Serial: AMBA PL011 UART driver&lt;BR /&gt;[ 0.031813] imx mu driver is registered.&lt;BR /&gt;[ 0.031835] imx rpmsg driver is registered.&lt;BR /&gt;[ 0.054775] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/pdmgrp&lt;BR /&gt;[ 0.054803] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai1grp&lt;BR /&gt;[ 0.054819] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai1grp_dsd&lt;BR /&gt;[ 0.054837] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai2grp&lt;BR /&gt;[ 0.054851] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai3grp&lt;BR /&gt;[ 0.054867] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/sai5grp&lt;BR /&gt;[ 0.054912] imx8mm-pinctrl 30330000.pinctrl: Invalid fsl,pins or pins property in node /soc@0/bus@30000000/pinctrl@30330000/usdhc2grpgpiogrp&lt;BR /&gt;[ 0.054940] imx8mm-pinctrl 30330000.pinctrl: no fsl,pins and pins property in node /soc@0/bus@30000000/pinctrl@30330000/lexi-imx8mm-gpio&lt;BR /&gt;[ 0.054965] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver&lt;BR /&gt;[ 0.071087] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.071101] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.071109] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.071117] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages&lt;BR /&gt;[ 0.072033] cryptd: max_cpu_qlen set to 1000&lt;BR /&gt;[ 0.074923] ACPI: Interpreter disabled.&lt;BR /&gt;[ 0.075463] iommu: Default domain type: Translated&lt;BR /&gt;[ 0.075606] vgaarb: loaded&lt;BR /&gt;[ 0.075908] SCSI subsystem initialized&lt;BR /&gt;[ 0.076217] usbcore: registered new interface driver usbfs&lt;BR /&gt;[ 0.076251] usbcore: registered new interface driver hub&lt;BR /&gt;[ 0.076277] usbcore: registered new device driver usb&lt;BR /&gt;[ 0.077251] mc: Linux media interface: v0.10&lt;BR /&gt;[ 0.077291] videodev: Linux video capture interface: v2.00&lt;BR /&gt;[ 0.077356] pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;[ 0.077363] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;giometti@linux.it&amp;gt;&lt;BR /&gt;[ 0.077377] PTP clock support registered&lt;BR /&gt;[ 0.077505] EDAC MC: Ver: 3.0.0&lt;BR /&gt;[ 0.078412] FPGA manager framework&lt;BR /&gt;[ 0.078486] Advanced Linux Sound Architecture Driver Initialized.&lt;BR /&gt;[ 0.079066] Bluetooth: Core ver 2.22&lt;BR /&gt;[ 0.079094] NET: Registered protocol family 31&lt;BR /&gt;[ 0.079100] Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;[ 0.079112] Bluetooth: HCI socket layer initialized&lt;BR /&gt;[ 0.079121] Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;[ 0.079136] Bluetooth: SCO socket layer initialized&lt;BR /&gt;[ 0.079752] clocksource: Switched to clocksource arch_sys_counter&lt;BR /&gt;[ 0.080034] VFS: Disk quotas dquot_6.6.0&lt;BR /&gt;[ 0.080081] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)&lt;BR /&gt;[ 0.080253] pnp: PnP ACPI: disabled&lt;BR /&gt;[ 0.085882] NET: Registered protocol family 2&lt;BR /&gt;[ 0.086255] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 8192 bytes, linear)&lt;BR /&gt;[ 0.086280] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)&lt;BR /&gt;[ 0.086366] TCP bind hash table entries: 8192 (order: 5, 131072 bytes, linear)&lt;BR /&gt;[ 0.086480] TCP: Hash tables configured (established 8192 bind 8192)&lt;BR /&gt;[ 0.086559] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.086586] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)&lt;BR /&gt;[ 0.086697] NET: Registered protocol family 1&lt;BR /&gt;[ 0.086983] RPC: Registered named UNIX socket transport module.&lt;BR /&gt;[ 0.086989] RPC: Registered udp transport module.&lt;BR /&gt;[ 0.086995] RPC: Registered tcp transport module.&lt;BR /&gt;[ 0.087002] RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;[ 0.087702] PCI: CLS 0 bytes, default 64&lt;BR /&gt;[ 0.087899] Unpacking initramfs...&lt;BR /&gt;[ 0.795563] Freeing initrd memory: 14564K&lt;BR /&gt;[ 0.796278] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available&lt;BR /&gt;[ 0.796858] kvm [1]: IPA Size Limit: 40 bits&lt;BR /&gt;[ 0.798192] kvm [1]: GICv3: no GICV resource entry&lt;BR /&gt;[ 0.798198] kvm [1]: disabling GICv2 emulation&lt;BR /&gt;[ 0.798218] kvm [1]: GIC system register CPU interface enabled&lt;BR /&gt;[ 0.798287] kvm [1]: vgic interrupt IRQ9&lt;BR /&gt;[ 0.798399] kvm [1]: Hyp mode initialized successfully&lt;BR /&gt;[ 0.801376] Initialise system trusted keyrings&lt;BR /&gt;[ 0.801510] workingset: timestamp_bits=42 max_order=18 bucket_order=0&lt;BR /&gt;[ 0.806983] squashfs: version 4.0 (2009/01/31) Phillip Lougher&lt;BR /&gt;[ 0.807567] NFS: Registering the id_resolver key type&lt;BR /&gt;[ 0.807594] Key type id_resolver registered&lt;BR /&gt;[ 0.807600] Key type id_legacy registered&lt;BR /&gt;[ 0.807675] nfs4filelayout_init: NFSv4 File Layout Driver Registering...&lt;BR /&gt;[ 0.807682] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...&lt;BR /&gt;[ 0.807702] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;[ 0.808075] 9p: Installing v9fs 9p2000 file system support&lt;BR /&gt;[ 0.845249] Key type asymmetric registered&lt;BR /&gt;[ 0.845258] Asymmetric key parser 'x509' registered&lt;BR /&gt;[ 0.845293] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)&lt;BR /&gt;[ 0.845301] io scheduler mq-deadline registered&lt;BR /&gt;[ 0.845306] io scheduler kyber registered&lt;BR /&gt;[ 0.850226] EINJ: ACPI disabled.&lt;BR /&gt;[ 0.858724] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2&lt;BR /&gt;[ 0.858740] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin&lt;BR /&gt;[ 0.866343] mxs-dma 33000000.dma-controller: initialized&lt;BR /&gt;[ 0.868105] Bus freq driver module loaded&lt;BR /&gt;[ 0.873263] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled&lt;BR /&gt;[ 0.875356] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 39, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 0.875992] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 40, base_baud = 5000000) is a IMX&lt;BR /&gt;[ 0.876518] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 41, base_baud = 1500000) is a IMX&lt;BR /&gt;[ 1.963903] printk: console [ttymxc1] enabled&lt;BR /&gt;[ 1.968768] Internal error: synchronous external abort: 96000210 [#1] PREEMPT SMP&lt;BR /&gt;[ 1.976251] Modules linked in:&lt;BR /&gt;[ 1.979314] CPU: 3 PID: 1 Comm: swapper/0 Not tainted 5.10.35+gef3f2cfc6010 #31&lt;BR /&gt;[ 1.986622] Hardware name: FSL i.MX8MM EVK board (DT)&lt;BR /&gt;[ 1.991675] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[ 1.997688] pc : imx_uart_probe+0x2c0/0x7e4&lt;BR /&gt;[ 2.001873] lr : imx_uart_probe+0x2b0/0x7e4&lt;BR /&gt;[ 2.006055] sp : ffff800011cdbb50&lt;BR /&gt;[ 2.009369] x29: ffff800011cdbb50 x28: 0000000000000000&lt;BR /&gt;[ 2.014686] x27: ffff8000117e04e0 x26: ffff00000634b400&lt;BR /&gt;[ 2.020003] x25: 00000000fffffffa x24: 00000000fffffffa&lt;BR /&gt;[ 2.025321] x23: 000000000000002d x22: ffff000006291810&lt;BR /&gt;[ 2.030636] x21: ffff000006291800 x20: 0000000000000000&lt;BR /&gt;[ 2.035951] x19: ffff000006952080 x18: 0000000000000020&lt;BR /&gt;[ 2.041266] x17: 0000000000000000 x16: 0000000000000001&lt;BR /&gt;[ 2.046581] x15: ffff000006080478 x14: ffffffffffffffff&lt;BR /&gt;[ 2.051896] x13: 0000000000000038 x12: 0101010101010101&lt;BR /&gt;[ 2.057214] x11: 0000000000000020 x10: 0101010101010101&lt;BR /&gt;[ 2.062531] x9 : 0000000000000000 x8 : ffff00000634b500&lt;BR /&gt;[ 2.067846] x7 : 0000000000000000 x6 : 000000000000003f&lt;BR /&gt;[ 2.073161] x5 : 0000000000000080 x4 : 0000000000000000&lt;BR /&gt;[ 2.078476] x3 : 0000000000000000 x2 : 0000000000000000&lt;BR /&gt;[ 2.083791] x1 : ffff800012480080 x0 : 0000000000000000&lt;BR /&gt;[ 2.089106] Call trace:&lt;BR /&gt;[ 2.091555] imx_uart_probe+0x2c0/0x7e4&lt;BR /&gt;[ 2.095394] platform_drv_probe+0x54/0xb0&lt;BR /&gt;[ 2.099404] really_probe+0xe4/0x4c0&lt;BR /&gt;[ 2.102981] driver_probe_device+0x58/0xc0&lt;BR /&gt;[ 2.107079] device_driver_attach+0xc0/0xd0&lt;BR /&gt;[ 2.111263] __driver_attach+0x84/0x124&lt;BR /&gt;[ 2.115100] bus_for_each_dev+0x70/0xc0&lt;BR /&gt;[ 2.118938] driver_attach+0x24/0x30&lt;BR /&gt;[ 2.122514] bus_add_driver+0x104/0x1ec&lt;BR /&gt;[ 2.126350] driver_register+0x78/0x130&lt;BR /&gt;[ 2.130186] __platform_driver_register+0x4c/0x60&lt;BR /&gt;[ 2.134893] imx_uart_init+0x3c/0x64&lt;BR /&gt;[ 2.138470] do_one_initcall+0x54/0x1bc&lt;BR /&gt;[ 2.142309] kernel_init_freeable+0x1d4/0x23c&lt;BR /&gt;[ 2.146667] kernel_init+0x14/0x118&lt;BR /&gt;[ 2.150158] ret_from_fork+0x10/0x30&lt;BR /&gt;[ 2.153738] Code: 2a0003f4 35001d40 f9400a61 91020021 (b9400021)&lt;BR /&gt;[ 2.159842] ---[ end trace d132e31f7226938a ]---&lt;BR /&gt;[ 2.164506] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b&lt;BR /&gt;[ 2.172164] SMP: stopping secondary CPUs&lt;BR /&gt;[ 2.176092] Kernel Offset: disabled&lt;BR /&gt;[ 2.179581] CPU features: 0x0240002,2000200c&lt;BR /&gt;[ 2.183850] Memory Limit: none&lt;BR /&gt;[ 2.186908] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b ]---&lt;/P&gt;</description>
      <pubDate>Wed, 20 Apr 2022 11:20:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-when-using-cpio-gz-u-boot/m-p/1446375#M189522</guid>
      <dc:creator>raymondman</dc:creator>
      <dc:date>2022-04-20T11:20:05Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel panic when using cpio.gz.u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-when-using-cpio-gz-u-boot/m-p/1571930#M198945</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I have a custom board with 1G LPDDR4. I made some custom on dts. The release used was 5.15.32-2.0.0. The system works except of:&lt;/P&gt;&lt;P&gt;[ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma'&lt;/P&gt;&lt;P&gt;If you fix your problem I really appreciate any tips.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Dec 2022 13:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic-when-using-cpio-gz-u-boot/m-p/1571930#M198945</guid>
      <dc:creator>oprata</dc:creator>
      <dc:date>2022-12-19T13:27:50Z</dc:date>
    </item>
  </channel>
</rss>