<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8mm kernel Lock</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8mm-kernel-Lock/m-p/1445669#M189476</link>
    <description>&lt;P&gt;Hi NXP&lt;BR /&gt;&lt;BR /&gt;I am using Yocto Kernel Version 5.4.3&amp;nbsp;on the original board.&lt;BR /&gt;When drawing with the QT Window application, the symptom that the kernel is locked occurs.&lt;BR /&gt;At this time, no debug log is output.&lt;BR /&gt;（Kernel panic logs such as oob and spin_lock are not output either.）&lt;BR /&gt;&lt;BR /&gt;１．The information in IMX8MM_0N87W.pdf includes ERR050044. If this phenomenon occurs, will the 　　above symptoms occur?&lt;BR /&gt;&lt;BR /&gt;２．Is there a patch for ERR050044?&lt;BR /&gt;&lt;BR /&gt;３．When I run the QT application with the iMX8mm warmed with a dryer, the phenomenon does not 　　occur.&lt;/P&gt;&lt;P&gt;　　What should we investigate from the above?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Koji Okuda&lt;/P&gt;</description>
    <pubDate>Tue, 19 Apr 2022 09:50:35 GMT</pubDate>
    <dc:creator>okuda</dc:creator>
    <dc:date>2022-04-19T09:50:35Z</dc:date>
    <item>
      <title>i.MX8mm kernel Lock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8mm-kernel-Lock/m-p/1445669#M189476</link>
      <description>&lt;P&gt;Hi NXP&lt;BR /&gt;&lt;BR /&gt;I am using Yocto Kernel Version 5.4.3&amp;nbsp;on the original board.&lt;BR /&gt;When drawing with the QT Window application, the symptom that the kernel is locked occurs.&lt;BR /&gt;At this time, no debug log is output.&lt;BR /&gt;（Kernel panic logs such as oob and spin_lock are not output either.）&lt;BR /&gt;&lt;BR /&gt;１．The information in IMX8MM_0N87W.pdf includes ERR050044. If this phenomenon occurs, will the 　　above symptoms occur?&lt;BR /&gt;&lt;BR /&gt;２．Is there a patch for ERR050044?&lt;BR /&gt;&lt;BR /&gt;３．When I run the QT application with the iMX8mm warmed with a dryer, the phenomenon does not 　　occur.&lt;/P&gt;&lt;P&gt;　　What should we investigate from the above?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Koji Okuda&lt;/P&gt;</description>
      <pubDate>Tue, 19 Apr 2022 09:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8mm-kernel-Lock/m-p/1445669#M189476</guid>
      <dc:creator>okuda</dc:creator>
      <dc:date>2022-04-19T09:50:35Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8mm kernel Lock</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8mm-kernel-Lock/m-p/1454834#M190136</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="okuda_0-1652084427534.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179174i9D45CFE0733D53B6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="okuda_0-1652084427534.png" alt="okuda_0-1652084427534.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;okuda_0-1652084427534.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;IMX8MM_0N87W.pdf recognizes that MIMX8MM6CVTKZAA is the applicable product.&lt;BR /&gt;The image above is the one I'm using this time, but I'm not sure if it's "MIMX8MM6CVTKZAA" or "MIMX8MM6CVIKZAA".&lt;BR /&gt;In the image above, which is "MIMX8MM6CVTKZAA" or "MIMX8MM6CVIKZAA"?&lt;BR /&gt;&lt;BR /&gt;For MIMX8MM6CVTKZAA, do I need to deal with ERR050044 errata in software processing?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 May 2022 08:36:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8mm-kernel-Lock/m-p/1454834#M190136</guid>
      <dc:creator>okuda</dc:creator>
      <dc:date>2022-05-09T08:36:21Z</dc:date>
    </item>
  </channel>
</rss>