<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックError when using hardware timestamp in ptp</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-using-hardware-timestamp-in-ptp/m-p/1445073#M189428</link>
    <description>&lt;P&gt;Error occured when ptp using hardware timestamp, does anyone met the same before and how it be fixed?&lt;/P&gt;&lt;P&gt;root@imx8mqevk:~# ethtool -T eth0&lt;BR /&gt;Time stamping parameters for eth0:&lt;BR /&gt;Capabilities:&lt;BR /&gt;hardware-transmit (SOF_TIMESTAMPING_TX_HARDWARE)&lt;BR /&gt;software-transmit (SOF_TIMESTAMPING_TX_SOFTWARE)&lt;BR /&gt;hardware-receive (SOF_TIMESTAMPING_RX_HARDWARE)&lt;BR /&gt;software-receive (SOF_TIMESTAMPING_RX_SOFTWARE)&lt;BR /&gt;software-system-clock (SOF_TIMESTAMPING_SOFTWARE)&lt;BR /&gt;hardware-raw-clock (SOF_TIMESTAMPING_RAW_HARDWARE)&lt;BR /&gt;PTP Hardware Clock: 0&lt;BR /&gt;Hardware Transmit Timestamp Modes:&lt;BR /&gt;off (HWTSTAMP_TX_OFF)&lt;BR /&gt;on (HWTSTAMP_TX_ON)&lt;BR /&gt;Hardware Receive Filter Modes:&lt;BR /&gt;none (HWTSTAMP_FILTER_NONE)&lt;BR /&gt;all (HWTSTAMP_FILTER_ALL)&lt;BR /&gt;root@imx8mqevk:~# sudo ptp4l -i eth0 -m -H&lt;BR /&gt;ptp4l[2861.116]: selected /dev/ptp0 as PTP clock&lt;BR /&gt;ptp4l[2861.117]: driver changed our HWTSTAMP options&lt;BR /&gt;ptp4l[2861.117]: tx_type 1 not 1&lt;BR /&gt;ptp4l[2861.117]: rx_filter 1 not 12&lt;BR /&gt;ptp4l[2861.118]: port 1: INITIALIZING to LISTENING on INITIALIZE&lt;BR /&gt;ptp4l[2861.118]: port 0: INITIALIZING to LISTENING on INITIALIZE&lt;BR /&gt;ptp4l[2861.118]: port 1: link up&lt;BR /&gt;ptp4l[2868.709]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES&lt;BR /&gt;ptp4l[2868.709]: selected best master clock e6b036.fffe.a0450a&lt;BR /&gt;ptp4l[2868.709]: assuming the grand master role&lt;BR /&gt;ptp4l[2869.711]: timed out while polling for tx timestamp&lt;BR /&gt;ptp4l[2869.711]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bug&lt;BR /&gt;ptp4l[2869.711]: port 1: send sync failed&lt;BR /&gt;ptp4l[2869.711]: port 1: MASTER to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)&lt;BR /&gt;ptp4l[2885.713]: driver changed our HWTSTAMP options&lt;BR /&gt;ptp4l[2885.713]: tx_type 1 not 1&lt;BR /&gt;ptp4l[2885.713]: rx_filter 1 not 12&lt;BR /&gt;ptp4l[2885.713]: port 1: FAULTY to LISTENING on FAULT_CLEARED&lt;BR /&gt;ptp4l[2893.506]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES&lt;BR /&gt;ptp4l[2893.506]: selected best master clock e6b036.fffe.a0450a&lt;BR /&gt;ptp4l[2893.506]: assuming the grand master role&lt;BR /&gt;ptp4l[2895.508]: timed out while polling for tx timestamp&lt;BR /&gt;ptp4l[2895.508]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bug&lt;BR /&gt;ptp4l[2895.508]: port 1: send sync failed&lt;BR /&gt;ptp4l[2895.508]: port 1: MASTER to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)&lt;/P&gt;</description>
    <pubDate>Mon, 18 Apr 2022 10:36:16 GMT</pubDate>
    <dc:creator>shenfungping</dc:creator>
    <dc:date>2022-04-18T10:36:16Z</dc:date>
    <item>
      <title>Error when using hardware timestamp in ptp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-using-hardware-timestamp-in-ptp/m-p/1445073#M189428</link>
      <description>&lt;P&gt;Error occured when ptp using hardware timestamp, does anyone met the same before and how it be fixed?&lt;/P&gt;&lt;P&gt;root@imx8mqevk:~# ethtool -T eth0&lt;BR /&gt;Time stamping parameters for eth0:&lt;BR /&gt;Capabilities:&lt;BR /&gt;hardware-transmit (SOF_TIMESTAMPING_TX_HARDWARE)&lt;BR /&gt;software-transmit (SOF_TIMESTAMPING_TX_SOFTWARE)&lt;BR /&gt;hardware-receive (SOF_TIMESTAMPING_RX_HARDWARE)&lt;BR /&gt;software-receive (SOF_TIMESTAMPING_RX_SOFTWARE)&lt;BR /&gt;software-system-clock (SOF_TIMESTAMPING_SOFTWARE)&lt;BR /&gt;hardware-raw-clock (SOF_TIMESTAMPING_RAW_HARDWARE)&lt;BR /&gt;PTP Hardware Clock: 0&lt;BR /&gt;Hardware Transmit Timestamp Modes:&lt;BR /&gt;off (HWTSTAMP_TX_OFF)&lt;BR /&gt;on (HWTSTAMP_TX_ON)&lt;BR /&gt;Hardware Receive Filter Modes:&lt;BR /&gt;none (HWTSTAMP_FILTER_NONE)&lt;BR /&gt;all (HWTSTAMP_FILTER_ALL)&lt;BR /&gt;root@imx8mqevk:~# sudo ptp4l -i eth0 -m -H&lt;BR /&gt;ptp4l[2861.116]: selected /dev/ptp0 as PTP clock&lt;BR /&gt;ptp4l[2861.117]: driver changed our HWTSTAMP options&lt;BR /&gt;ptp4l[2861.117]: tx_type 1 not 1&lt;BR /&gt;ptp4l[2861.117]: rx_filter 1 not 12&lt;BR /&gt;ptp4l[2861.118]: port 1: INITIALIZING to LISTENING on INITIALIZE&lt;BR /&gt;ptp4l[2861.118]: port 0: INITIALIZING to LISTENING on INITIALIZE&lt;BR /&gt;ptp4l[2861.118]: port 1: link up&lt;BR /&gt;ptp4l[2868.709]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES&lt;BR /&gt;ptp4l[2868.709]: selected best master clock e6b036.fffe.a0450a&lt;BR /&gt;ptp4l[2868.709]: assuming the grand master role&lt;BR /&gt;ptp4l[2869.711]: timed out while polling for tx timestamp&lt;BR /&gt;ptp4l[2869.711]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bug&lt;BR /&gt;ptp4l[2869.711]: port 1: send sync failed&lt;BR /&gt;ptp4l[2869.711]: port 1: MASTER to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)&lt;BR /&gt;ptp4l[2885.713]: driver changed our HWTSTAMP options&lt;BR /&gt;ptp4l[2885.713]: tx_type 1 not 1&lt;BR /&gt;ptp4l[2885.713]: rx_filter 1 not 12&lt;BR /&gt;ptp4l[2885.713]: port 1: FAULTY to LISTENING on FAULT_CLEARED&lt;BR /&gt;ptp4l[2893.506]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES&lt;BR /&gt;ptp4l[2893.506]: selected best master clock e6b036.fffe.a0450a&lt;BR /&gt;ptp4l[2893.506]: assuming the grand master role&lt;BR /&gt;ptp4l[2895.508]: timed out while polling for tx timestamp&lt;BR /&gt;ptp4l[2895.508]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bug&lt;BR /&gt;ptp4l[2895.508]: port 1: send sync failed&lt;BR /&gt;ptp4l[2895.508]: port 1: MASTER to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)&lt;/P&gt;</description>
      <pubDate>Mon, 18 Apr 2022 10:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-when-using-hardware-timestamp-in-ptp/m-p/1445073#M189428</guid>
      <dc:creator>shenfungping</dc:creator>
      <dc:date>2022-04-18T10:36:16Z</dc:date>
    </item>
  </channel>
</rss>