<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: apt-update - The repository is not signed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1443466#M189264</link>
    <description>&lt;P&gt;I had already tried this way, but without success. I attach the two outputs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also tried to exclude problematic packages during the upgrade, but this causes a corruption of the operating system, which can no longer boot up.&lt;/P&gt;</description>
    <pubDate>Wed, 13 Apr 2022 14:09:21 GMT</pubDate>
    <dc:creator>fpasino</dc:creator>
    <dc:date>2022-04-13T14:09:21Z</dc:date>
    <item>
      <title>apt-update - The repository is not signed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1440597#M189053</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I cannot update the list of available packages and therefore cannot install new packages on a i.MX 8M Nano EVK board. I use Linux version 5.10.72 installed on eMMC (imx-image-full-imx8mnevk.wic found &lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_self"&gt;here&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;Here the output of &lt;FONT face="andale mono,times"&gt;cat /etc/apt/sources.list.d/debian-10.list&lt;/FONT&gt;&lt;EM&gt; :&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="andale mono,times"&gt;deb &lt;A href="http://ftp.debian.org/debian" target="_blank"&gt;http://ftp.debian.org/debian&lt;/A&gt; buster main contrib non-free&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="andale mono,times"&gt;deb &lt;A href="http://ftp.debian.org/debian" target="_blank"&gt;http://ftp.debian.org/debian&lt;/A&gt; buster-updates main contrib non-free&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is the &lt;FONT face="andale mono,times"&gt;sudo apt update &lt;/FONT&gt;log.&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Apr 2022 12:55:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1440597#M189053</guid>
      <dc:creator>fpasino</dc:creator>
      <dc:date>2022-04-07T12:55:57Z</dc:date>
    </item>
    <item>
      <title>Re: apt-update - The repository is not signed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1442593#M189195</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_10" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198119" target="_self" aria-label="View Profile of fpasino"&gt;&lt;SPAN class=""&gt;fpasino&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;The debian-10.list is just a demo. Please have a try to touch sources.list under /etc/apt/, and then modify it as required.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please let me know if you have any further question.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Apr 2022 09:41:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1442593#M189195</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2022-04-12T09:41:46Z</dc:date>
    </item>
    <item>
      <title>Re: apt-update - The repository is not signed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1443022#M189232</link>
      <description>&lt;P&gt;Hi Fpasino&lt;/P&gt;&lt;P&gt;I have tested on iMX8M Nano refer to &lt;A href="https://askubuntu.com/questions/732985/force-update-from-unsigned-repository" target="_blank" rel="noopener"&gt;https://askubuntu.com/questions/732985/force-update-from-unsigned-repository&lt;/A&gt;&lt;/P&gt;&lt;P&gt;apt update &lt;SPAN class=""&gt;--allow-insecure-repositories&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Apr 2022 02:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1443022#M189232</guid>
      <dc:creator>karl1688</dc:creator>
      <dc:date>2022-04-13T02:57:04Z</dc:date>
    </item>
    <item>
      <title>Re: apt-update - The repository is not signed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1443466#M189264</link>
      <description>&lt;P&gt;I had already tried this way, but without success. I attach the two outputs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also tried to exclude problematic packages during the upgrade, but this causes a corruption of the operating system, which can no longer boot up.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Apr 2022 14:09:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1443466#M189264</guid>
      <dc:creator>fpasino</dc:creator>
      <dc:date>2022-04-13T14:09:21Z</dc:date>
    </item>
    <item>
      <title>Re: apt-update - The repository is not signed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1444552#M189375</link>
      <description>&lt;P&gt;I confirm that source.list in /etc/apt/sources.list.d/debian-10.list isn't a problem to fix this. As you can see output from 'apt update', warning messages are pointing to gpgv gpgv1 gpgv2 GNU Privacy Guard.&lt;/P&gt;&lt;P&gt;After installing some debian packages 'apt update' output change to no public key, refer to attachment.&lt;/P&gt;&lt;P&gt;Err:1 &lt;A href="http://security.debian.org" target="_blank"&gt;http://security.debian.org&lt;/A&gt; buster/updates InRelease&lt;BR /&gt;The following signatures couldn't be verified because the public key is not available: NO_PUBKEY 112695A0E562B32A NO_PUBKEY 54404762BBB6E853&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;GNU Privacy Guard on my iMX8MN&lt;/P&gt;&lt;P&gt;root@imx8mn-ddr4-evk:~# gpgv --version&lt;BR /&gt;gpgv (GnuPG) 2.2.27&lt;BR /&gt;libgcrypt 1.8.4&lt;BR /&gt;Copyright (C) 2021 Free Software Foundation, Inc.&lt;BR /&gt;License GNU GPL-3.0-or-later &amp;lt;&lt;A href="https://gnu.org/licenses/gpl.html" target="_blank"&gt;https://gnu.org/licenses/gpl.html&lt;/A&gt;&amp;gt;&lt;BR /&gt;This is free software: you are free to change and redistribute it.&lt;BR /&gt;There is NO WARRANTY, to the extent permitted by law.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Apr 2022 09:58:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1444552#M189375</guid>
      <dc:creator>karl1688</dc:creator>
      <dc:date>2022-04-15T09:58:58Z</dc:date>
    </item>
    <item>
      <title>Re: apt-update - The repository is not signed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1444791#M189408</link>
      <description>&lt;P&gt;Hi Fpasino&lt;/P&gt;&lt;P&gt;I attach everything in debian_pkgs.zip in the meantime share 'apt update logs' in attached.&lt;/P&gt;&lt;P&gt;You can start with installing 'dpkg -i gpgv_2.2.27-2~bpo10+1_arm64.deb', if any dependency problem occur you might look for then(.deb) in zip.&lt;/P&gt;&lt;P&gt;And if you have load library issue because PATH is missing, then you might export PATH by following example in ld_path.txt in zip&lt;/P&gt;&lt;P&gt;Finally NO_PUBLIC keys issue you can fix it by following example in apgv.txt in zip&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Apr 2022 02:09:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1444791#M189408</guid>
      <dc:creator>karl1688</dc:creator>
      <dc:date>2022-04-18T02:09:36Z</dc:date>
    </item>
    <item>
      <title>Re: apt-update - The repository is not signed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1445812#M189489</link>
      <description>&lt;P&gt;You can have a try that&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188961"&gt;@karl1688&lt;/a&gt;&amp;nbsp;provides. As we have enhanced the security certificate of the debian10 repo. So for no harmful to your system, we recommend to build a internal package repo, and then create a sources.list.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Tue, 19 Apr 2022 13:40:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1445812#M189489</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2022-04-19T13:40:59Z</dc:date>
    </item>
    <item>
      <title>Re: apt-update - The repository is not signed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1488133#M192431</link>
      <description>&lt;P&gt;any solution for this issue please? , I want to install&amp;nbsp; some deb packages , so i added the sources.list file to /etc/apt but the update fails for the reason of gpg, gpgv .. not installed . can someone help me&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 12:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1488133#M192431</guid>
      <dc:creator>mariemkort</dc:creator>
      <dc:date>2022-07-12T12:32:59Z</dc:date>
    </item>
    <item>
      <title>Re: apt-update - The repository is not signed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1564323#M198327</link>
      <description>&lt;P&gt;Hi Karl1688&lt;/P&gt;&lt;P&gt;when we make a yocto build, the images will be under /tmp/deploy/images/imx/ . Where should we add the debian packages ..gpgv_2.2.27*.deb under debian_pkgs.zip (is it under /tmp/deploy/deb/imx7).&lt;/P&gt;&lt;P&gt;I still get same warning as &lt;EM&gt;&lt;FONT face="lucida sans unicode,lucida sans"&gt;GPG error: gpgv, gpgv2 or gpgv1 required for verification, but neither seems installed&lt;/FONT&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;what should i do&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Dec 2022 10:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/apt-update-The-repository-is-not-signed/m-p/1564323#M198327</guid>
      <dc:creator>Jeffy</dc:creator>
      <dc:date>2022-12-05T10:01:55Z</dc:date>
    </item>
  </channel>
</rss>