<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Booting IMXRT1170 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Booting-IMXRT1170/m-p/1443240#M189253</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) FlexSPI 1 in boot configuration and it is basically booting from the QSPI Flash (S25WP128-JBLE) but what is the use of the Octal Flash here (MX25UM51345GXDI00)&lt;BR /&gt;-- The RT MCU can boot from the Octal Flash besides QSPI flash.&lt;BR /&gt;2) If I am correct the application has to be downloaded the first time using J-Link and serial download mode (01) to the QSPI Flash; booting configuration are not required to be changed for Jtag connection.&lt;BR /&gt;-- No, I don't think so.&lt;BR /&gt;3) For our board we are also looking to boot from serial download (01) into the NAND Flash using USB OTG1 or UART and MCU BootUtility ? is this Possible?&lt;BR /&gt;-- Yes, it's possible.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 13 Apr 2022 08:02:54 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2022-04-13T08:02:54Z</dc:date>
    <item>
      <title>Booting IMXRT1170</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-IMXRT1170/m-p/1442804#M189217</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;For our customized board I would like to verify the booting process. I understand that the boot mode has to be 10 for internal mode; FlexSPI 1 in boot configuration and it is basically booting from the QSPI Flash (S25WP128-JBLE) but what is the use of the Octal Flash here (MX25UM51345GXDI00) ?&lt;/P&gt;&lt;P&gt;If I am correct the application has to be downloaded the first time using J-Link and serial download mode (01) to the QSPI Flash; booting configuration are not required to be changed for Jtag connection.&lt;/P&gt;&lt;P&gt;For our board we are also looking to boot from serial download (01) into the NAND Flash using USB OTG1 or UART and MCU BootUtility ? is this Possible?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;TM&lt;/P&gt;</description>
      <pubDate>Tue, 12 Apr 2022 15:02:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-IMXRT1170/m-p/1442804#M189217</guid>
      <dc:creator>TM_MI</dc:creator>
      <dc:date>2022-04-12T15:02:49Z</dc:date>
    </item>
    <item>
      <title>Re: Booting IMXRT1170</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-IMXRT1170/m-p/1443240#M189253</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) FlexSPI 1 in boot configuration and it is basically booting from the QSPI Flash (S25WP128-JBLE) but what is the use of the Octal Flash here (MX25UM51345GXDI00)&lt;BR /&gt;-- The RT MCU can boot from the Octal Flash besides QSPI flash.&lt;BR /&gt;2) If I am correct the application has to be downloaded the first time using J-Link and serial download mode (01) to the QSPI Flash; booting configuration are not required to be changed for Jtag connection.&lt;BR /&gt;-- No, I don't think so.&lt;BR /&gt;3) For our board we are also looking to boot from serial download (01) into the NAND Flash using USB OTG1 or UART and MCU BootUtility ? is this Possible?&lt;BR /&gt;-- Yes, it's possible.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 13 Apr 2022 08:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-IMXRT1170/m-p/1443240#M189253</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-04-13T08:02:54Z</dc:date>
    </item>
  </channel>
</rss>