<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8M mini MIPI_DSI DRM device not loading</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-mini-MIPI-DSI-DRM-device-not-loading/m-p/1441398#M189097</link>
    <description>&lt;P&gt;HI ,&lt;/P&gt;&lt;P&gt;We have custom IMX8M board with ILI9881C panel.&lt;/P&gt;&lt;P&gt;I have&amp;nbsp; Modified kconfig and compiled with ili988c Driver&lt;/P&gt;&lt;P&gt;I have also&amp;nbsp; Enabled ili device node in DTS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;amp;mipi_dsi {&lt;BR /&gt;status = "okay";&lt;BR /&gt;panel1: panel@0 {&lt;BR /&gt;reg = &amp;lt;1&amp;gt;;&lt;BR /&gt;compatible = "bananapi,lhr050h41","ilitek,ili9881c";&lt;BR /&gt;reset-gpios = &amp;lt;&amp;amp;gpio3 12 1&amp;gt;;&lt;BR /&gt;power-supply = &amp;lt;&amp;amp;reg_mipi_phy&amp;gt;;&lt;BR /&gt;backlight = &amp;lt;&amp;amp;backlight&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;I don't see any kind of error while booting on drm/mipi/ or ili,&lt;/P&gt;&lt;P&gt;When i checked the code I could see that the device attach is not working properly saying that the drm_mipi bus has no device .&lt;/P&gt;&lt;P&gt;The device driver is unchanged . Only change I did was to enable it in dts.&lt;BR /&gt;&lt;BR /&gt;root@imx8mm:~# dmesg |grep drm&lt;BR /&gt;[ 1.677021] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu on minor 0&lt;BR /&gt;root@imx8mm:~#&lt;/P&gt;</description>
    <pubDate>Fri, 08 Apr 2022 15:28:20 GMT</pubDate>
    <dc:creator>nivednk14</dc:creator>
    <dc:date>2022-04-08T15:28:20Z</dc:date>
    <item>
      <title>IMX8M mini MIPI_DSI DRM device not loading</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-mini-MIPI-DSI-DRM-device-not-loading/m-p/1441398#M189097</link>
      <description>&lt;P&gt;HI ,&lt;/P&gt;&lt;P&gt;We have custom IMX8M board with ILI9881C panel.&lt;/P&gt;&lt;P&gt;I have&amp;nbsp; Modified kconfig and compiled with ili988c Driver&lt;/P&gt;&lt;P&gt;I have also&amp;nbsp; Enabled ili device node in DTS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;amp;mipi_dsi {&lt;BR /&gt;status = "okay";&lt;BR /&gt;panel1: panel@0 {&lt;BR /&gt;reg = &amp;lt;1&amp;gt;;&lt;BR /&gt;compatible = "bananapi,lhr050h41","ilitek,ili9881c";&lt;BR /&gt;reset-gpios = &amp;lt;&amp;amp;gpio3 12 1&amp;gt;;&lt;BR /&gt;power-supply = &amp;lt;&amp;amp;reg_mipi_phy&amp;gt;;&lt;BR /&gt;backlight = &amp;lt;&amp;amp;backlight&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;I don't see any kind of error while booting on drm/mipi/ or ili,&lt;/P&gt;&lt;P&gt;When i checked the code I could see that the device attach is not working properly saying that the drm_mipi bus has no device .&lt;/P&gt;&lt;P&gt;The device driver is unchanged . Only change I did was to enable it in dts.&lt;BR /&gt;&lt;BR /&gt;root@imx8mm:~# dmesg |grep drm&lt;BR /&gt;[ 1.677021] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu on minor 0&lt;BR /&gt;root@imx8mm:~#&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 15:28:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-mini-MIPI-DSI-DRM-device-not-loading/m-p/1441398#M189097</guid>
      <dc:creator>nivednk14</dc:creator>
      <dc:date>2022-04-08T15:28:20Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M mini MIPI_DSI DRM device not loading</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-mini-MIPI-DSI-DRM-device-not-loading/m-p/1441964#M189148</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I need all changes you do, including your defconfig change, kconfig change&lt;/P&gt;</description>
      <pubDate>Mon, 11 Apr 2022 09:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-mini-MIPI-DSI-DRM-device-not-loading/m-p/1441964#M189148</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-04-11T09:02:42Z</dc:date>
    </item>
  </channel>
</rss>