<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to ajust imx6ull dma aging timer</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-ajust-imx6ull-dma-aging-timer/m-p/1441230#M189085</link>
    <description>&lt;P&gt;Hi, NXP experts：&lt;/P&gt;&lt;P&gt;I find a note in imx-uart driver drivers/tty/serial/imx.c says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;* There are two kinds of RX DMA interrupts(such as in the MX6Q):&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* [1] the RX DMA buffer is full.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* [2] the &lt;STRONG&gt;aging timer expires&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;*&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* Condition [2] is triggered when a character has been sitting in the FIFO&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* for at least &lt;STRONG&gt;8 byte durations&lt;/STRONG&gt;.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So how&amp;nbsp;to ajust imx6ull dma aging durations shorter?&lt;/P&gt;</description>
    <pubDate>Fri, 08 Apr 2022 10:32:22 GMT</pubDate>
    <dc:creator>changbaoma</dc:creator>
    <dc:date>2022-04-08T10:32:22Z</dc:date>
    <item>
      <title>How to ajust imx6ull dma aging timer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-ajust-imx6ull-dma-aging-timer/m-p/1441230#M189085</link>
      <description>&lt;P&gt;Hi, NXP experts：&lt;/P&gt;&lt;P&gt;I find a note in imx-uart driver drivers/tty/serial/imx.c says:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;* There are two kinds of RX DMA interrupts(such as in the MX6Q):&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* [1] the RX DMA buffer is full.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* [2] the &lt;STRONG&gt;aging timer expires&lt;/STRONG&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;*&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* Condition [2] is triggered when a character has been sitting in the FIFO&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;* for at least &lt;STRONG&gt;8 byte durations&lt;/STRONG&gt;.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So how&amp;nbsp;to ajust imx6ull dma aging durations shorter?&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 10:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-ajust-imx6ull-dma-aging-timer/m-p/1441230#M189085</guid>
      <dc:creator>changbaoma</dc:creator>
      <dc:date>2022-04-08T10:32:22Z</dc:date>
    </item>
  </channel>
</rss>