<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MXRT 1050 can work with 1440x240 LCD in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MXRT-1050-can-work-with-1440x240-LCD/m-p/1440976#M189068</link>
    <description>&lt;P&gt;Hello community&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm trying to figure out if a 1440x240 LCD display can work with an IMXRT 1050.&lt;BR /&gt;According to the datasheet of the IMX RT1050, the maximum resolution of LCD is WXGA 1366 x 768. I wonder if H is greater than 1366 or V is greater than 768 it will not be supported right?&lt;BR /&gt;Or is the total HxV greater than 1366x768 not supported?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank all&lt;/P&gt;</description>
    <pubDate>Fri, 08 Apr 2022 03:35:55 GMT</pubDate>
    <dc:creator>hiectai</dc:creator>
    <dc:date>2022-04-08T03:35:55Z</dc:date>
    <item>
      <title>MXRT 1050 can work with 1440x240 LCD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MXRT-1050-can-work-with-1440x240-LCD/m-p/1440976#M189068</link>
      <description>&lt;P&gt;Hello community&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm trying to figure out if a 1440x240 LCD display can work with an IMXRT 1050.&lt;BR /&gt;According to the datasheet of the IMX RT1050, the maximum resolution of LCD is WXGA 1366 x 768. I wonder if H is greater than 1366 or V is greater than 768 it will not be supported right?&lt;BR /&gt;Or is the total HxV greater than 1366x768 not supported?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank all&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 03:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MXRT-1050-can-work-with-1440x240-LCD/m-p/1440976#M189068</guid>
      <dc:creator>hiectai</dc:creator>
      <dc:date>2022-04-08T03:35:55Z</dc:date>
    </item>
    <item>
      <title>Re: MXRT 1050 can work with 1440x240 LCD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MXRT-1050-can-work-with-1440x240-LCD/m-p/1441201#M189083</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/163325"&gt;@hiectai&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) I wonder if H is greater than 1366 or V is greater than 768 it will not be supported right?&lt;BR /&gt;-- No, it supports, however, the fresh rate will decrease quickly if the resolution is too big.&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 09:39:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MXRT-1050-can-work-with-1440x240-LCD/m-p/1441201#M189083</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-04-08T09:39:31Z</dc:date>
    </item>
    <item>
      <title>Re: MXRT 1050 can work with 1440x240 LCD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MXRT-1050-can-work-with-1440x240-LCD/m-p/1442967#M189228</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN class=""&gt;Jeremyzhou&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks so much for your answer.&lt;/P&gt;&lt;P&gt;We will connect IMXRT1050 to 1440x240 LCD and evaluate the performance.&lt;/P&gt;&lt;P&gt;Have a nice day.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Apr 2022 01:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MXRT-1050-can-work-with-1440x240-LCD/m-p/1442967#M189228</guid>
      <dc:creator>hiectai</dc:creator>
      <dc:date>2022-04-13T01:15:20Z</dc:date>
    </item>
  </channel>
</rss>