<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic U-boot for imx8mm Mini Evaluation kit in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-for-imx8mm-Mini-Evaluation-kit/m-p/1438984#M188972</link>
    <description>&lt;P&gt;To track boot-time of&amp;nbsp; U-boot (proper) i am using U-boot's internal bootstage facility which records boot-time for different stages as booting up progress. in imx8mm_evk_defconfig file configured the following parameters.&amp;nbsp;&lt;/P&gt;&lt;P&gt;CONFIG_BOOTSTAGE =y&lt;/P&gt;&lt;P&gt;CONFIG_BOOTSTAGE_REPORT =y&lt;/P&gt;&lt;P&gt;and then built and created flash.bin image. it worked fine and shows the bootstage report in (micro-secs) of different stages.&lt;/P&gt;&lt;P&gt;but, when tried to use bootstage for U-boot SPL it does not give SPL stages time records. it still shows only U-boot (proper) stages time records only and does not include SPL start and SPL end time markings.&lt;/P&gt;&lt;P&gt;the following configurations were done:&lt;/P&gt;&lt;P&gt;CONFIG_SPL_BOOTSTAGE =Y&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Moreover, the image failed to flash when BOOTSTAGE_STASH =Y&amp;nbsp; was configured.&lt;/P&gt;&lt;P&gt;it kept resetting the cpu and could not flash (flash.bin) to evk board through uuu-utility for usb serial download.&lt;/P&gt;&lt;P&gt;stash start address - 0x0&amp;nbsp; { I have doubt here.. what should be stash start address for imx8mm Mini board)&lt;/P&gt;&lt;P&gt;statsh size - 0x1000 (4096)&lt;/P&gt;&lt;P&gt;please clarify and resolve the query.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 05 Apr 2022 15:27:53 GMT</pubDate>
    <dc:creator>KJ_Mehta</dc:creator>
    <dc:date>2022-04-05T15:27:53Z</dc:date>
    <item>
      <title>U-boot for imx8mm Mini Evaluation kit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-for-imx8mm-Mini-Evaluation-kit/m-p/1438984#M188972</link>
      <description>&lt;P&gt;To track boot-time of&amp;nbsp; U-boot (proper) i am using U-boot's internal bootstage facility which records boot-time for different stages as booting up progress. in imx8mm_evk_defconfig file configured the following parameters.&amp;nbsp;&lt;/P&gt;&lt;P&gt;CONFIG_BOOTSTAGE =y&lt;/P&gt;&lt;P&gt;CONFIG_BOOTSTAGE_REPORT =y&lt;/P&gt;&lt;P&gt;and then built and created flash.bin image. it worked fine and shows the bootstage report in (micro-secs) of different stages.&lt;/P&gt;&lt;P&gt;but, when tried to use bootstage for U-boot SPL it does not give SPL stages time records. it still shows only U-boot (proper) stages time records only and does not include SPL start and SPL end time markings.&lt;/P&gt;&lt;P&gt;the following configurations were done:&lt;/P&gt;&lt;P&gt;CONFIG_SPL_BOOTSTAGE =Y&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Moreover, the image failed to flash when BOOTSTAGE_STASH =Y&amp;nbsp; was configured.&lt;/P&gt;&lt;P&gt;it kept resetting the cpu and could not flash (flash.bin) to evk board through uuu-utility for usb serial download.&lt;/P&gt;&lt;P&gt;stash start address - 0x0&amp;nbsp; { I have doubt here.. what should be stash start address for imx8mm Mini board)&lt;/P&gt;&lt;P&gt;statsh size - 0x1000 (4096)&lt;/P&gt;&lt;P&gt;please clarify and resolve the query.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Apr 2022 15:27:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-for-imx8mm-Mini-Evaluation-kit/m-p/1438984#M188972</guid>
      <dc:creator>KJ_Mehta</dc:creator>
      <dc:date>2022-04-05T15:27:53Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot for imx8mm Mini Evaluation kit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-boot-for-imx8mm-Mini-Evaluation-kit/m-p/1443067#M189238</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199113"&gt;@KJ_Mehta&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer this AN:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13369.pdf" target="_self"&gt;Boot Time Measurements Methodology&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Apr 2022 04:38:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-boot-for-imx8mm-Mini-Evaluation-kit/m-p/1443067#M189238</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-04-13T04:38:32Z</dc:date>
    </item>
  </channel>
</rss>