<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKernel Crash while updating board using Swupdate</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Crash-while-updating-board-using-Swupdate/m-p/1437701#M188891</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using IMX8MQ EVK and trying to do Firmware Upgrade using Swupdate utility (version 2020.04) . Board is running on yocto Linux 5.4-zeus distribution and while upgrading the board, swupdate flash progress reaches 95% and then generates kernel crash. Below are the different kernel crash attached logs we are getting with each time we execute the firmware upgrade.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, we have seen that our RAM is 3GB and it's working as expected and also there's no full memory utilization.&lt;/P&gt;&lt;P&gt;So, please review attached logs and provide the support for the same.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Aakash&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 01 Apr 2022 13:41:46 GMT</pubDate>
    <dc:creator>Aakash_Sharma</dc:creator>
    <dc:date>2022-04-01T13:41:46Z</dc:date>
    <item>
      <title>Kernel Crash while updating board using Swupdate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Crash-while-updating-board-using-Swupdate/m-p/1437701#M188891</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using IMX8MQ EVK and trying to do Firmware Upgrade using Swupdate utility (version 2020.04) . Board is running on yocto Linux 5.4-zeus distribution and while upgrading the board, swupdate flash progress reaches 95% and then generates kernel crash. Below are the different kernel crash attached logs we are getting with each time we execute the firmware upgrade.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, we have seen that our RAM is 3GB and it's working as expected and also there's no full memory utilization.&lt;/P&gt;&lt;P&gt;So, please review attached logs and provide the support for the same.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Aakash&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Apr 2022 13:41:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Crash-while-updating-board-using-Swupdate/m-p/1437701#M188891</guid>
      <dc:creator>Aakash_Sharma</dc:creator>
      <dc:date>2022-04-01T13:41:46Z</dc:date>
    </item>
  </channel>
</rss>