<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: SCFW Testing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1437510#M188872</link>
    <description>&lt;P&gt;I run clean build, and I got output on SCU Debug Monitor. Thank you for you time.&lt;BR /&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Fri, 01 Apr 2022 07:50:53 GMT</pubDate>
    <dc:creator>vzeric</dc:creator>
    <dc:date>2022-04-01T07:50:53Z</dc:date>
    <item>
      <title>SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1433431#M188578</link>
      <description>&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;I am using iMX8QM MEK.&lt;BR /&gt;I have built flash.bin file using imx-mkimage running the command&lt;BR /&gt;&lt;STRONG&gt;make SOC=iMX8QM flash_scfw_test&lt;/STRONG&gt;&lt;BR /&gt;I copied scfw_tests.bin and scfw_tcm.bin in imx-mkimage/iMX8QM which I got running&lt;BR /&gt;&lt;STRONG&gt;make qm R=B0 B=mek T=all&lt;/STRONG&gt;&lt;BR /&gt;Also, I have copied mx8qmb0-ahab-container.img from firmaware/seco to imx-mkimage/iMX8QM&lt;BR /&gt;There is no problems during the build, but I cannnot flash the board using Universal Update Utility.&lt;BR /&gt;After runnning&lt;STRONG&gt; uuu -V -b emmc flash.bin&lt;/STRONG&gt; process goes to 100% and stucks here forever. Also I am not sure how am I supposed to run SCFW test?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Vanja&lt;/P&gt;</description>
      <pubDate>Thu, 24 Mar 2022 11:23:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1433431#M188578</guid>
      <dc:creator>vzeric</dc:creator>
      <dc:date>2022-03-24T11:23:49Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1433467#M188581</link>
      <description>&lt;P&gt;Actually I need to add flash.bin to OCRAM at 0x00100000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Mar 2022 13:02:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1433467#M188581</guid>
      <dc:creator>vzeric</dc:creator>
      <dc:date>2022-03-24T13:02:50Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1433474#M188583</link>
      <description>&lt;P&gt;Because flash board needs u-boot fastboot. The scfw test flash.bin has no u-boot. So you need a regular flash.bin as arg0 and scfw test flash.bin as arg1&lt;/P&gt;
&lt;P&gt;uuu [-d -m -v] -b[run] &amp;lt;emmc|emmc_all|fat_write|nand|qspi|sd|sd_all|spl&amp;gt; arg...&lt;BR /&gt;Run Built-in scripts&lt;BR /&gt;emmc burn boot loader to eMMC boot partition&lt;BR /&gt;arg0: _flash.bin bootloader&lt;BR /&gt;arg1: _image[Optional] image burn to emmc, default is the same as bootloader&lt;/P&gt;</description>
      <pubDate>Thu, 24 Mar 2022 13:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1433474#M188583</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2022-03-24T13:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1436947#M188811</link>
      <description>&lt;P&gt;Hi, me again. I managed to write the image to the emmc and I have enabled SCU Debug Monitor, and I built "dsc" test for now, but when I run the board everything looks good, but I cannot see the output of the "dsc" test. Am I supposed to run ti somehow or it should be run automatically with or without output? I can't see if it passes or fails.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 09:19:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1436947#M188811</guid>
      <dc:creator>vzeric</dc:creator>
      <dc:date>2022-03-31T09:19:48Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1436965#M188813</link>
      <description>&lt;P&gt;Please&amp;nbsp; try add T=dsc&amp;nbsp; during compile the scfw.&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BTW， you don't need to flash to emmc to do the test.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;just uuu&amp;nbsp; flash.bin&amp;nbsp; &amp;nbsp;is enough.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 09:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1436965#M188813</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2022-03-31T09:42:49Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1436991#M188819</link>
      <description>&lt;P&gt;Yes, I added T=dsc.&lt;BR /&gt;I tested, uuu flash.bin passes, and where can I see the output?&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 10:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1436991#M188819</guid>
      <dc:creator>vzeric</dc:creator>
      <dc:date>2022-03-31T10:16:01Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1437286#M188843</link>
      <description>&lt;P&gt;Have you use the M=1 to enable the scfw debug monitor?&lt;/P&gt;
&lt;P&gt;Do you have debug uart for scfw on hardware?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Apr 2022 01:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1437286#M188843</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2022-04-01T01:04:35Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1437417#M188864</link>
      <description>&lt;P&gt;Yes, I have compiled with option M=1 and I have enabled SCU Debug Monitor and moved SW4 to position ON to enable UART&lt;/P&gt;&lt;P&gt;Command:&lt;BR /&gt;make qm R=B0 D=1 M=1 B=mek U=2 T=dsc&lt;/P&gt;&lt;P&gt;after that imx-mkimage runs:&lt;BR /&gt;make SOC=iMX8QM flash_spl&lt;/P&gt;</description>
      <pubDate>Fri, 01 Apr 2022 05:52:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1437417#M188864</guid>
      <dc:creator>vzeric</dc:creator>
      <dc:date>2022-04-01T05:52:01Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1437510#M188872</link>
      <description>&lt;P&gt;I run clean build, and I got output on SCU Debug Monitor. Thank you for you time.&lt;BR /&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Apr 2022 07:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1437510#M188872</guid>
      <dc:creator>vzeric</dc:creator>
      <dc:date>2022-04-01T07:50:53Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1437700#M188890</link>
      <description>&lt;P&gt;New problem that I am facing, but I am not sure that's my mistake:&lt;BR /&gt;When I try to build SCFW Tests with option T=all, I am getting error that m_text sector is overflowed by 2000+ bytes&lt;/P&gt;&lt;P&gt;Edit:&lt;/P&gt;&lt;P&gt;region `m_text' overflowed by 2752 bytes&lt;/P&gt;</description>
      <pubDate>Fri, 01 Apr 2022 13:39:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1437700#M188890</guid>
      <dc:creator>vzeric</dc:creator>
      <dc:date>2022-04-01T13:39:23Z</dc:date>
    </item>
    <item>
      <title>Re: SCFW Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1439347#M188995</link>
      <description>&lt;P&gt;It is not your problem.&lt;/P&gt;
&lt;P&gt;option all is too big.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Apr 2022 04:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCFW-Testing/m-p/1439347#M188995</guid>
      <dc:creator>BiyongSUN</dc:creator>
      <dc:date>2022-04-06T04:49:05Z</dc:date>
    </item>
  </channel>
</rss>