<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MFGTool Updater Error 0x500 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MFGTool-Updater-Error-0x500/m-p/1437247#M188837</link>
    <description>&lt;P&gt;On a windows 7 machine, I am trying to use MFGTool to download a Linux profile (i.e. MX28 Linux Update) via USB to a TX28-4031 development board. The output option was set to "Singlechip NAND". But when I clicked "Start", it would eventually fail with the following error message:&lt;/P&gt;&lt;P&gt;"Updater Error 0x500 (1280) - The current thread has already been converted to a fiber".&lt;/P&gt;&lt;P&gt;If the output option is set to SD (with uboot) or SD (without uboot), the writing will be successful.&lt;/P&gt;&lt;P&gt;Any thoughts on how to fix the issue with "Singlechip NAND" as an output option? Thanks for your kind help in advance!&lt;/P&gt;</description>
    <pubDate>Thu, 31 Mar 2022 22:20:48 GMT</pubDate>
    <dc:creator>yuanming</dc:creator>
    <dc:date>2022-03-31T22:20:48Z</dc:date>
    <item>
      <title>MFGTool Updater Error 0x500</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MFGTool-Updater-Error-0x500/m-p/1437247#M188837</link>
      <description>&lt;P&gt;On a windows 7 machine, I am trying to use MFGTool to download a Linux profile (i.e. MX28 Linux Update) via USB to a TX28-4031 development board. The output option was set to "Singlechip NAND". But when I clicked "Start", it would eventually fail with the following error message:&lt;/P&gt;&lt;P&gt;"Updater Error 0x500 (1280) - The current thread has already been converted to a fiber".&lt;/P&gt;&lt;P&gt;If the output option is set to SD (with uboot) or SD (without uboot), the writing will be successful.&lt;/P&gt;&lt;P&gt;Any thoughts on how to fix the issue with "Singlechip NAND" as an output option? Thanks for your kind help in advance!&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 22:20:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MFGTool-Updater-Error-0x500/m-p/1437247#M188837</guid>
      <dc:creator>yuanming</dc:creator>
      <dc:date>2022-03-31T22:20:48Z</dc:date>
    </item>
  </channel>
</rss>