<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT106F Devices File in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106F-Devices-File/m-p/1437241#M188836</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm targeting a new board build with Zephyr for the RT106F (MIMXRT106FCVL5B to be specific).&lt;BR /&gt;I notice that there are several device specific files generated per processor variation in the mcux sdk here:&lt;BR /&gt;&lt;A href="https://github.com/NXPmicro/mcux-sdk/blob/main/devices/" target="_blank"&gt;https://github.com/NXPmicro/mcux-sdk/blob/main/devices/&lt;/A&gt;, but from what I can tell there's no explicit support for the MIMXRT106F currently (I see a RT1062 and a RT1064).&lt;/P&gt;&lt;P&gt;From the &lt;A href="https://www.nxp.com/docs/en/nxp/data-sheets/IMXRT1060CEC.pdf" target="_self"&gt;datasheet&lt;/A&gt;, it looks like the RT106F is largely the same as the RT1062. The RT1062 is purported to be "Full-feature", whereas the RT106F has "facial recognition".&amp;nbsp;&lt;/P&gt;&lt;P&gt;Am I okay to just use the RT1062 cpu devices folder for my board? (We won't be making use of the facial recognition feature in any case). If not, how can I request support for the RT106F in the MCUX SDK?&lt;/P&gt;</description>
    <pubDate>Thu, 31 Mar 2022 21:57:31 GMT</pubDate>
    <dc:creator>nickolas_at_whisper</dc:creator>
    <dc:date>2022-03-31T21:57:31Z</dc:date>
    <item>
      <title>MIMXRT106F Devices File</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106F-Devices-File/m-p/1437241#M188836</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm targeting a new board build with Zephyr for the RT106F (MIMXRT106FCVL5B to be specific).&lt;BR /&gt;I notice that there are several device specific files generated per processor variation in the mcux sdk here:&lt;BR /&gt;&lt;A href="https://github.com/NXPmicro/mcux-sdk/blob/main/devices/" target="_blank"&gt;https://github.com/NXPmicro/mcux-sdk/blob/main/devices/&lt;/A&gt;, but from what I can tell there's no explicit support for the MIMXRT106F currently (I see a RT1062 and a RT1064).&lt;/P&gt;&lt;P&gt;From the &lt;A href="https://www.nxp.com/docs/en/nxp/data-sheets/IMXRT1060CEC.pdf" target="_self"&gt;datasheet&lt;/A&gt;, it looks like the RT106F is largely the same as the RT1062. The RT1062 is purported to be "Full-feature", whereas the RT106F has "facial recognition".&amp;nbsp;&lt;/P&gt;&lt;P&gt;Am I okay to just use the RT1062 cpu devices folder for my board? (We won't be making use of the facial recognition feature in any case). If not, how can I request support for the RT106F in the MCUX SDK?&lt;/P&gt;</description>
      <pubDate>Thu, 31 Mar 2022 21:57:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106F-Devices-File/m-p/1437241#M188836</guid>
      <dc:creator>nickolas_at_whisper</dc:creator>
      <dc:date>2022-03-31T21:57:31Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT106F Devices File</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106F-Devices-File/m-p/1437996#M188914</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198738"&gt;@nickolas_at_whisper&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; A good news to you, RT106F is totally the same for RT1060 chip, so you totally can use the&amp;nbsp;&lt;SPAN&gt;RT1062&amp;nbsp;situation.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;RT106F just can use the face recognition feature, as the software is verified by the RT106F, you can consider RT106F IP is totally the same as the RT1062, just have possibility to use the face recognition feature, if you use other normal function, just take it as RT1062.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Wish it helps you!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;kerry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 02 Apr 2022 10:15:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT106F-Devices-File/m-p/1437996#M188914</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2022-04-02T10:15:37Z</dc:date>
    </item>
  </channel>
</rss>