<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 8QM GPIO interrupt in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QM-GPIO-interrupt/m-p/1436147#M188783</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a project that uses the spear-mx8 board on a VAR-SP8Customboard. I have Linux running on the Cortex A cores and I am able to run some bare metal C code on the cortex M4 co-processors using the MCUXpresso SDK.&lt;/P&gt;&lt;P&gt;Now I want to configure a GPIO pin as input and use this pin to trigger an interrupt in the M4. I have seen examples of interrupts with timers, but I am unable to find some example or even some good documentation. Has anyone already used a GPIO as an interrupt on the cortex M4 or is there some documentation about this?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 30 Mar 2022 11:38:06 GMT</pubDate>
    <dc:creator>jens0501</dc:creator>
    <dc:date>2022-03-30T11:38:06Z</dc:date>
    <item>
      <title>i.MX 8QM GPIO interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QM-GPIO-interrupt/m-p/1436147#M188783</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a project that uses the spear-mx8 board on a VAR-SP8Customboard. I have Linux running on the Cortex A cores and I am able to run some bare metal C code on the cortex M4 co-processors using the MCUXpresso SDK.&lt;/P&gt;&lt;P&gt;Now I want to configure a GPIO pin as input and use this pin to trigger an interrupt in the M4. I have seen examples of interrupts with timers, but I am unable to find some example or even some good documentation. Has anyone already used a GPIO as an interrupt on the cortex M4 or is there some documentation about this?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 30 Mar 2022 11:38:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8QM-GPIO-interrupt/m-p/1436147#M188783</guid>
      <dc:creator>jens0501</dc:creator>
      <dc:date>2022-03-30T11:38:06Z</dc:date>
    </item>
  </channel>
</rss>