<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックfalconboot on imx8</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/falconboot-on-imx8/m-p/1436131#M188782</link>
    <description>&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am trying to enable the falcon boot mode on the imx8, i got it working on the imx6, however on the imx8evk after adding line&amp;nbsp;#define CONFIG_SPL_OS_BOOT&amp;nbsp; board stops after spl doesn't boot into the uboot.&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-49995-g7ffdddacd2-dirty (Mar 30 2022 - 15:27:14 +0530)&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/P&gt;&lt;P&gt;if i remove the line&amp;nbsp;#define CONFIG_SPL_OS_BOOT from my config file i can boot the board without any problem.&amp;nbsp;&lt;/P&gt;&lt;P&gt;how can i make the board to load the uboot when the spl_os_boot is enabled.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Krisj&lt;/P&gt;</description>
    <pubDate>Wed, 30 Mar 2022 11:06:15 GMT</pubDate>
    <dc:creator>KrisJ</dc:creator>
    <dc:date>2022-03-30T11:06:15Z</dc:date>
    <item>
      <title>falconboot on imx8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/falconboot-on-imx8/m-p/1436131#M188782</link>
      <description>&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am trying to enable the falcon boot mode on the imx8, i got it working on the imx6, however on the imx8evk after adding line&amp;nbsp;#define CONFIG_SPL_OS_BOOT&amp;nbsp; board stops after spl doesn't boot into the uboot.&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-49995-g7ffdddacd2-dirty (Mar 30 2022 - 15:27:14 +0530)&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/P&gt;&lt;P&gt;if i remove the line&amp;nbsp;#define CONFIG_SPL_OS_BOOT from my config file i can boot the board without any problem.&amp;nbsp;&lt;/P&gt;&lt;P&gt;how can i make the board to load the uboot when the spl_os_boot is enabled.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Krisj&lt;/P&gt;</description>
      <pubDate>Wed, 30 Mar 2022 11:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/falconboot-on-imx8/m-p/1436131#M188782</guid>
      <dc:creator>KrisJ</dc:creator>
      <dc:date>2022-03-30T11:06:15Z</dc:date>
    </item>
  </channel>
</rss>