<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Setting SDRAM clock on i.mxRT1176</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Setting-SDRAM-clock-on-i-mxRT1176/m-p/1434479#M188654</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Firstly, assume you use the DCD to initialize the SDRAM, it's unnecessary to update the clock of SEMC actually.&lt;BR /&gt;Next, back to your below question, &lt;BR /&gt;1) Could you provide the example for 166MHz SDRAM or clearfy why I am unable to reduce the SDRAM clock?&lt;BR /&gt;-- I'd like to suggest you to modify the semc which resides in the ~\boards\evkmimxrt1170\driver_examples\semc to implement access the SDRAM on your board, after that, you can adjust the DCD by referring to the detailed values of the SEMC's registers.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Mon, 28 Mar 2022 02:17:07 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2022-03-28T02:17:07Z</dc:date>
    <item>
      <title>Setting SDRAM clock on i.mxRT1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Setting-SDRAM-clock-on-i-mxRT1176/m-p/1433971#M188623</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Currently, we use the i.mxRT1172 for LCD project. I use emwin for SDK example code.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;As I know SDK's emwin project setting the max SDRAM bandwidth of RT1170 is 200x2 = 400 MB/s,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;However, we need to change the clock from SDRAM setting form 200MHz to 166MH,&amp;nbsp;base on our SDRAM's spec.&lt;/P&gt;&lt;P&gt;Could you provide the example for 166MHz SDRAM or clearfy why I am unable to reduce the SDRAM clock?&lt;/P&gt;&lt;P&gt;The following is my dcd setting&lt;/P&gt;&lt;P&gt;#include "dcd.h"&lt;/P&gt;&lt;P&gt;/* Component ID definition, used by tools. */&lt;BR /&gt;#ifndef FSL_COMPONENT_ID&lt;BR /&gt;#define FSL_COMPONENT_ID "platform.drivers.xip_board"&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#if defined(XIP_BOOT_HEADER_ENABLE) &amp;amp;&amp;amp; (XIP_BOOT_HEADER_ENABLE == 1)&lt;BR /&gt;#if defined(XIP_BOOT_HEADER_DCD_ENABLE) &amp;amp;&amp;amp; (XIP_BOOT_HEADER_DCD_ENABLE == 1)&lt;BR /&gt;#if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__)&lt;BR /&gt;__attribute__((section(".boot_hdr.dcd_data"), used))&lt;BR /&gt;#elif defined(__ICCARM__)&lt;BR /&gt;#pragma location = ".boot_hdr.dcd_data"&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************&lt;BR /&gt;!!GlobalInfo&lt;BR /&gt;product: DCDx V2.0&lt;BR /&gt;processor: MIMXRT1176xxxxx&lt;BR /&gt;package_id: MIMXRT1176DVMAA&lt;BR /&gt;mcu_data: ksdk2_0&lt;BR /&gt;processor_version: 0.0.0&lt;BR /&gt;output_format: c_array&lt;BR /&gt;* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/&lt;BR /&gt;/* COMMENTS BELOW ARE USED AS SETTINGS FOR DCD DATA */&lt;BR /&gt;const uint8_t dcd_data[] = {&lt;BR /&gt;/* HEADER */&lt;BR /&gt;/* Tag */&lt;BR /&gt;0xD2,&lt;BR /&gt;/* Image Length */&lt;BR /&gt;0x05, 0x08,&lt;BR /&gt;/* Version */&lt;BR /&gt;0x41,&lt;/P&gt;&lt;P&gt;/* COMMANDS */&lt;/P&gt;&lt;P&gt;/* group: 'Imported Commands' */&lt;BR /&gt;/* #1.1-139, command header bytes for merged 'Write - value' command */&lt;BR /&gt;0xCC, 0x04, 0x5C, 0x04,&lt;BR /&gt;/* #1.1, command: write_value, address: CCM_CLOCK_ROOT4_CONTROL, value: 0x703, size: 4 */&lt;BR /&gt;0x40, 0xCC, 0x02, 0x00, 0x00, 0x00, 0x07, 0x03,//0x09,//0x07,//0x03,&lt;BR /&gt;/* #1.2, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_00, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x10, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.3, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_01, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x14, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.4, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_02, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x18, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.5, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_03, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x1C, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.6, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_04, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x20, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.7, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_05, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x24, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.8, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_06, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x28, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.9, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_07, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x2C, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.10, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_08, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x30, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.11, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_09, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x34, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.12, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_10, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x38, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.13, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_11, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x3C, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.14, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_12, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x40, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.15, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_13, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x44, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.16, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_14, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x48, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.17, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_15, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x4C, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.18, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_16, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x50, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.19, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_17, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x54, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.20, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_18, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x58, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.21, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_19, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x5C, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.22, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_20, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x60, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.23, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_21, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x64, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.24, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_22, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x68, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.25, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_23, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x6C, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.26, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_24, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x70, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.27, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_25, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x74, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.28, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_26, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x78, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.29, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_27, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x7C, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.30, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_28, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.31, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_29, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x84, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.32, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_30, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x88, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.33, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_31, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x8C, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.34, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_32, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x90, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.35, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_33, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x94, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.36, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_34, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x98, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.37, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_35, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0x9C, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.38, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_36, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xA0, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.39, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_37, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xA4, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.40, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_38, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xA8, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.41, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_39, value: 0x10, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xAC, 0x00, 0x00, 0x00, 0x10,&lt;BR /&gt;/* #1.42, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_40, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xB0, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.43, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_41, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xB4, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.44, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_00, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xB8, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.45, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_01, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xBC, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.46, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_02, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xC0, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.47, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_03, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xC4, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.48, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_04, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xC8, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.49, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_05, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xCC, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.50, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_06, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xD0, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.51, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_07, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xD4, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.52, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_08, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xD8, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.53, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_09, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xDC, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.54, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_10, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xE0, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.55, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_11, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xE4, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.56, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_12, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xE8, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.57, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_13, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xEC, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.58, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_14, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xF0, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.59, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_15, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xF4, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.60, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_16, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xF8, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.61, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_17, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x80, 0xFC, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.62, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_18, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x81, 0x00, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.63, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_19, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x81, 0x04, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.64, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_20, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x81, 0x08, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.65, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_00, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x54, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.66, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_01, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x58, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.67, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_02, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x5C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.68, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_03, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x60, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.69, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_04, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x64, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.70, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_05, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x68, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.71, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_06, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x6C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.72, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_07, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x70, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.73, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_08, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x74, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.74, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_09, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x78, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.75, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_10, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x7C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.76, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_11, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x80, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.77, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_12, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x84, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.78, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_13, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x88, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.79, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_14, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x8C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.80, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_15, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x90, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.81, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_16, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x94, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.82, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_17, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x98, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.83, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_18, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0x9C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.84, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_19, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xA0, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.85, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_20, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xA4, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.86, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_21, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xA8, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.87, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_22, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xAC, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.88, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_23, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xB0, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.89, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_24, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xB4, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.90, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_25, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xB8, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.91, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_26, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xBC, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.92, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_27, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xC0, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.93, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_28, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xC4, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.94, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_29, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xC8, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.95, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_30, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xCC, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.96, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_31, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xD0, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.97, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_32, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xD4, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.98, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_33, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xD8, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.99, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_34, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xDC, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.100, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_35, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xE0, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.101, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_36, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xE4, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.102, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_37, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xE8, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.103, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_38, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xEC, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.104, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_39, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xF0, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.105, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_40, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xF4, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.106, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_41, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xF8, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.107, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_00, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x82, 0xFC, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.108, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_01, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x00, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.109, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_02, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x04, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.110, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_03, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x08, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.111, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_04, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x0C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.112, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_05, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x10, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.113, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_06, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x14, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.114, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_07, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x18, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.115, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_08, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x1C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.116, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_09, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x20, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.117, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_10, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x24, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.118, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_11, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x28, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.119, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_12, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x2C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.120, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_13, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x30, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.121, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_14, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x34, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.122, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_15, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x38, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.123, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_16, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x83, 0x3C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.124, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_02, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x84, 0x00, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.125, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_03, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x84, 0x04, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.126, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_04, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x84, 0x08, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.127, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_05, value: 0x08, size: 4 */&lt;BR /&gt;0x40, 0x0E, 0x84, 0x0C, 0x00, 0x00, 0x00, 0x08,&lt;BR /&gt;/* #1.128, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x00, 0x10, 0x00, 0x00, 0x04,&lt;BR /&gt;/* #1.129, command: write_value, address: SEMC_BMCR0, value: 0x81, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x08, 0x00, 0x00, 0x00, 0x81,&lt;BR /&gt;/* #1.130, command: write_value, address: SEMC_BMCR1, value: 0x81, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x0C, 0x00, 0x00, 0x00, 0x81,&lt;BR /&gt;/* #1.131, command: write_value, address: SEMC_BR0, value: 0x8000001D, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x10, 0x80, 0x00, 0x00, 0x1D,&lt;BR /&gt;/* #1.132, command: write_value, address: SEMC_SDRAMCR0, value: 0xF32, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x40, 0x00, 0x00, 0x0F, 0x31,/*0x32,*/&lt;BR /&gt;/* #1.133, command: write_value, address: SEMC_SDRAMCR1, value: 0x772A22, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x44, 0x00, 0x77, 0x2A, 0x22,&lt;BR /&gt;/* #1.134, command: write_value, address: SEMC_SDRAMCR2, value: 0x10A0D, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x48, 0x00, 0x01, 0x0A, 0x0D,&lt;BR /&gt;/* #1.135, command: write_value, address: SEMC_SDRAMCR3, value: 0x21210408, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x4C, 0x21, 0x21, 0x05/*0x04*/, 0x08,&lt;BR /&gt;/* #1.136, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x90, 0x80, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.137, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x94, 0x00, 0x00, 0x00, 0x02,&lt;BR /&gt;/* #1.138, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x98, 0x00, 0x00, 0x00, 0x00,&lt;BR /&gt;/* #1.139, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0F,&lt;BR /&gt;/* #2, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #3, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #4, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #5, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #6, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #7.1-2, command header bytes for merged 'Write - value' command */&lt;BR /&gt;0xCC, 0x00, 0x14, 0x04,&lt;BR /&gt;/* #7.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,&lt;BR /&gt;/* #7.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,&lt;BR /&gt;/* #8, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #9, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #10, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #11, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #12, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #13.1-2, command header bytes for merged 'Write - value' command */&lt;BR /&gt;0xCC, 0x00, 0x14, 0x04,&lt;BR /&gt;/* #13.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,&lt;BR /&gt;/* #13.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,&lt;BR /&gt;/* #14, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #15, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #16, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #17, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #18, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #19.1-3, command header bytes for merged 'Write - value' command */&lt;BR /&gt;0xCC, 0x00, 0x1C, 0x04,&lt;BR /&gt;/* #19.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,&lt;BR /&gt;/* #19.2, command: write_value, address: SEMC_IPTXDAT, value: 0x33, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0xA0, 0x00, 0x00, 0x00, 0x33,&lt;BR /&gt;/* #19.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0A,&lt;BR /&gt;/* #20, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #21, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #22, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #23, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #24, command: nop */&lt;BR /&gt;0xC0, 0x00, 0x04, 0x00,&lt;BR /&gt;/* #25.1-2, command header bytes for merged 'Write - value' command */&lt;BR /&gt;0xCC, 0x00, 0x14, 0x04,&lt;BR /&gt;/* #25.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,&lt;BR /&gt;/* #25.2, command: write_value, address: SEMC_SDRAMCR3, value: 0x21210409, size: 4 */&lt;BR /&gt;0x40, 0x0D, 0x40, 0x4C, 0x21, 0x21, 0x05/*0x04*/, 0x09&lt;BR /&gt;};&lt;BR /&gt;/* BE CAREFUL MODIFYING THIS SETTINGS - IT IS YAML SETTINGS FOR TOOLS */&lt;/P&gt;&lt;P&gt;#else&lt;BR /&gt;const uint8_t dcd_data[] = {0x00};&lt;BR /&gt;#endif /* XIP_BOOT_HEADER_DCD_ENABLE */&lt;BR /&gt;#endif /* XIP_BOOT_HEADER_ENABLE */&lt;/P&gt;&lt;P&gt;And I also have another testing for clock_config.c&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="revolutesea_0-1648195668991.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174847i6F4557C7C49A5A77/image-size/medium?v=v2&amp;amp;px=400" role="button" title="revolutesea_0-1648195668991.png" alt="revolutesea_0-1648195668991.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Just wanna SDRAM clock get any change..&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="revolutesea_1-1648195689032.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174848i488A9DC77DDBB02F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="revolutesea_1-1648195689032.png" alt="revolutesea_1-1648195689032.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Mar 2022 08:09:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Setting-SDRAM-clock-on-i-mxRT1176/m-p/1433971#M188623</guid>
      <dc:creator>revolutesea</dc:creator>
      <dc:date>2022-03-25T08:09:28Z</dc:date>
    </item>
    <item>
      <title>Re: Setting SDRAM clock on i.mxRT1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Setting-SDRAM-clock-on-i-mxRT1176/m-p/1434479#M188654</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Firstly, assume you use the DCD to initialize the SDRAM, it's unnecessary to update the clock of SEMC actually.&lt;BR /&gt;Next, back to your below question, &lt;BR /&gt;1) Could you provide the example for 166MHz SDRAM or clearfy why I am unable to reduce the SDRAM clock?&lt;BR /&gt;-- I'd like to suggest you to modify the semc which resides in the ~\boards\evkmimxrt1170\driver_examples\semc to implement access the SDRAM on your board, after that, you can adjust the DCD by referring to the detailed values of the SEMC's registers.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 28 Mar 2022 02:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Setting-SDRAM-clock-on-i-mxRT1176/m-p/1434479#M188654</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-03-28T02:17:07Z</dc:date>
    </item>
    <item>
      <title>Re: Setting SDRAM clock on i.mxRT1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Setting-SDRAM-clock-on-i-mxRT1176/m-p/1434830#M188681</link>
      <description>&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Mon, 28 Mar 2022 13:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Setting-SDRAM-clock-on-i-mxRT1176/m-p/1434830#M188681</guid>
      <dc:creator>revolutesea</dc:creator>
      <dc:date>2022-03-28T13:18:58Z</dc:date>
    </item>
  </channel>
</rss>