<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Support use QSPI nor flash on  i.MXRT1050 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Support-use-QSPI-nor-flash-on-i-MXRT1050/m-p/1430390#M188346</link>
    <description>&lt;P&gt;&lt;BR /&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you. &lt;BR /&gt;1. I built code in IAR and use external QSPI flash (IS25LP256D). I want to ask i can read, write or erase with external flash while the processor is running (XIP) on it ??&lt;BR /&gt;-- Firstly, your proposal is able to make it, next, it needs to relocate the FlexSPI driver into the internal RAM prior to reading or writing the data section, I'd like to suggest you refer to the polling_transfer (~\boards\evkbimxrt1050\driver_examples\flexspi\nor\polling_transfer) in the SDK library.&lt;BR /&gt;2. ROM APIs is available on i.MXRT1050 ? Have document explant detail about it? &lt;BR /&gt;-- No, the i.MXRT1050 doesn't support the ROM API feature.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 18 Mar 2022 02:01:07 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2022-03-18T02:01:07Z</dc:date>
    <item>
      <title>Support use QSPI nor flash on  i.MXRT1050</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Support-use-QSPI-nor-flash-on-i-MXRT1050/m-p/1429921#M188323</link>
      <description>&lt;P&gt;I use&amp;nbsp;i.MX RT 1050. I have two questions:&lt;/P&gt;&lt;P&gt;1. I built code in IAR and use external QSPI flash (IS25LP256D). I want to ask i can read, write or erase with external flash while the processor is running (XIP) on it ??&lt;/P&gt;&lt;P&gt;2. ROM APIs is available on&amp;nbsp;i.MXRT1050 ? Have document explant detail about it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for support !&lt;/P&gt;</description>
      <pubDate>Thu, 17 Mar 2022 07:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Support-use-QSPI-nor-flash-on-i-MXRT1050/m-p/1429921#M188323</guid>
      <dc:creator>WolfAlpha2</dc:creator>
      <dc:date>2022-03-17T07:41:20Z</dc:date>
    </item>
    <item>
      <title>Re: Support use QSPI nor flash on  i.MXRT1050</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Support-use-QSPI-nor-flash-on-i-MXRT1050/m-p/1430390#M188346</link>
      <description>&lt;P&gt;&lt;BR /&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you. &lt;BR /&gt;1. I built code in IAR and use external QSPI flash (IS25LP256D). I want to ask i can read, write or erase with external flash while the processor is running (XIP) on it ??&lt;BR /&gt;-- Firstly, your proposal is able to make it, next, it needs to relocate the FlexSPI driver into the internal RAM prior to reading or writing the data section, I'd like to suggest you refer to the polling_transfer (~\boards\evkbimxrt1050\driver_examples\flexspi\nor\polling_transfer) in the SDK library.&lt;BR /&gt;2. ROM APIs is available on i.MXRT1050 ? Have document explant detail about it? &lt;BR /&gt;-- No, the i.MXRT1050 doesn't support the ROM API feature.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 18 Mar 2022 02:01:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Support-use-QSPI-nor-flash-on-i-MXRT1050/m-p/1430390#M188346</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-03-18T02:01:07Z</dc:date>
    </item>
  </channel>
</rss>