<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUse iMX8M Plus as USB Gadget</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Use-iMX8M-Plus-as-USB-Gadget/m-p/1429356#M188292</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on iMX8M plus custom board and I want to use this board as gadget to access the stored data. I am able to detect the device on GUI as gadget and can see the data available in the eMMC. But every time I need to restart/reboot the device while creating/deleting the new file. what should I do to reflect the changes at run time.&lt;/P&gt;&lt;P&gt;E.g.&lt;/P&gt;&lt;P&gt;1. Run Gadget mode&lt;/P&gt;&lt;P&gt;2. Create new file say "test.txt" using command line and save it.&lt;/P&gt;&lt;P&gt;3. unable to see the file at GUI.&lt;/P&gt;&lt;P&gt;4. Reboot the device. and run the gadget mode.&lt;/P&gt;&lt;P&gt;5. now able to see the "test.txt" file in GUI.&lt;/P&gt;&lt;P&gt;can anyone face this issue earlier and have idea what need to be done.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 16 Mar 2022 14:19:15 GMT</pubDate>
    <dc:creator>swapnilturambekar</dc:creator>
    <dc:date>2022-03-16T14:19:15Z</dc:date>
    <item>
      <title>Use iMX8M Plus as USB Gadget</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-iMX8M-Plus-as-USB-Gadget/m-p/1429356#M188292</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on iMX8M plus custom board and I want to use this board as gadget to access the stored data. I am able to detect the device on GUI as gadget and can see the data available in the eMMC. But every time I need to restart/reboot the device while creating/deleting the new file. what should I do to reflect the changes at run time.&lt;/P&gt;&lt;P&gt;E.g.&lt;/P&gt;&lt;P&gt;1. Run Gadget mode&lt;/P&gt;&lt;P&gt;2. Create new file say "test.txt" using command line and save it.&lt;/P&gt;&lt;P&gt;3. unable to see the file at GUI.&lt;/P&gt;&lt;P&gt;4. Reboot the device. and run the gadget mode.&lt;/P&gt;&lt;P&gt;5. now able to see the "test.txt" file in GUI.&lt;/P&gt;&lt;P&gt;can anyone face this issue earlier and have idea what need to be done.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 14:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-iMX8M-Plus-as-USB-Gadget/m-p/1429356#M188292</guid>
      <dc:creator>swapnilturambekar</dc:creator>
      <dc:date>2022-03-16T14:19:15Z</dc:date>
    </item>
  </channel>
</rss>