<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8M Mini PCIe PLL PLL lock failure in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-PCIe-PLL-PLL-lock-failure/m-p/1428789#M188246</link>
    <description>&lt;P&gt;I am using an IMX8MM on a custom board design and have an issue with PCIe PLL lock using an external clock source.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[    2.532274] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[    2.538174] imx6q-pcie 33800000.pcie: GPR15=6188ffff
[    2.564533] imx6q-pcie 33800000.pcie: PCIe PLL lock timeout&lt;/LI-CODE&gt;&lt;P&gt;I understand from other similar posts that we may have an issue with our external clock getting to the IMX8 and we are actively investigating this. However, I noticed that when that when the PLL lock fails the boot hangs shortly after. When I disable the pcie0 node in the device tree then the boot is successful.&lt;/P&gt;&lt;P&gt;Is it typical for the IMX8 to appear to "hang" after PCIe PLL lock failure? Can this hang be caused by a poor PCIE CLK signal?&lt;/P&gt;&lt;P&gt;Thank you for the assistance,&lt;BR /&gt;Matt&lt;/P&gt;</description>
    <pubDate>Tue, 15 Mar 2022 23:47:27 GMT</pubDate>
    <dc:creator>pikorn</dc:creator>
    <dc:date>2022-03-15T23:47:27Z</dc:date>
    <item>
      <title>IMX8M Mini PCIe PLL PLL lock failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-PCIe-PLL-PLL-lock-failure/m-p/1428789#M188246</link>
      <description>&lt;P&gt;I am using an IMX8MM on a custom board design and have an issue with PCIe PLL lock using an external clock source.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[    2.532274] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[    2.538174] imx6q-pcie 33800000.pcie: GPR15=6188ffff
[    2.564533] imx6q-pcie 33800000.pcie: PCIe PLL lock timeout&lt;/LI-CODE&gt;&lt;P&gt;I understand from other similar posts that we may have an issue with our external clock getting to the IMX8 and we are actively investigating this. However, I noticed that when that when the PLL lock fails the boot hangs shortly after. When I disable the pcie0 node in the device tree then the boot is successful.&lt;/P&gt;&lt;P&gt;Is it typical for the IMX8 to appear to "hang" after PCIe PLL lock failure? Can this hang be caused by a poor PCIE CLK signal?&lt;/P&gt;&lt;P&gt;Thank you for the assistance,&lt;BR /&gt;Matt&lt;/P&gt;</description>
      <pubDate>Tue, 15 Mar 2022 23:47:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-PCIe-PLL-PLL-lock-failure/m-p/1428789#M188246</guid>
      <dc:creator>pikorn</dc:creator>
      <dc:date>2022-03-15T23:47:27Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M Mini PCIe PLL PLL lock failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-PCIe-PLL-PLL-lock-failure/m-p/1434964#M188692</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes it is possible to cause a hang as you have seen from other threads, so yes you should look into the PCIe CLK signal.&lt;BR /&gt;&lt;BR /&gt;Also, I think this should be a good reference:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Use-PI6CFGL201BZDIEX-as-PCIe-REF-CLK/m-p/1290940" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Use-PI6CFGL201BZDIEX-as-PCIe-REF-CLK/m-p/1290940&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-CLK-Generator-Clocking-Issue/m-p/1258056" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-CLK-Generator-Clocking-Issue/m-p/1258056&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Mar 2022 18:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-PCIe-PLL-PLL-lock-failure/m-p/1434964#M188692</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-03-28T18:13:46Z</dc:date>
    </item>
  </channel>
</rss>