<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Model Voltage error when simulating i.MX8 QM LPDDR4 interface with Hyperlynx in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Model-Voltage-error-when-simulating-i-MX8-QM-LPDDR4-interface/m-p/1427979#M188194</link>
    <description>&lt;P&gt;Hello. I have a design where I'm using the same LPDDR4 chips as the NXP eval board and in fact I have the same layout (pulled it in from the ODB++ files). It should work but I wanted to run a simulation to check. The models I'm using are:&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;i.MX8QM: imx8qm_29x29_rev1_25.ibs&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;MT53E768M32D4DT LPDDR4: z1am_200b-qdp_x32.ebd&lt;/P&gt;&lt;P&gt;The micron model within that ebd file is set to z1am_0p6V_st.ibs&lt;/P&gt;&lt;P&gt;When I set up the DDRx Batch Mode test in Hyperlynx, I get the following error:&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;There are nets with IBIS model voltage range compatibility issues:&lt;BR /&gt;Net(s): DDR_CH0_DM0..3, DDR_CH0_DQ0..31, DDR_CH1_DM0..3, DDR_CH1_DQ0..31&lt;BR /&gt;IBIS File: C:\Hyp\ADCMK5\Models\IMX8QM-IBIS\imx8qm_29x29_rev1_25.ibs&lt;BR /&gt;Selector/Model, Voltage: PDDRIO_PAD_DATA / DWC_D5MPL4_40 1.1V&lt;BR /&gt;Device(s): U1&lt;BR /&gt;IBIS File: C:\Hyp\ADCMK5\Models\MT53E768M32D4DT-053_ibis\z1am_0p6v_wt.ibs&lt;BR /&gt;Selector/Model, Voltage: DQ / DQ_PD40_ODT40_VOH50_4266 0.6V&lt;BR /&gt;Device(s): U0_EBD-U4, U2_EBD-U4&lt;/P&gt;&lt;P&gt;Am I trying to use the wrong models?&lt;/P&gt;&lt;P&gt;Thanks so much!&lt;/P&gt;&lt;P&gt;Rich&lt;/P&gt;</description>
    <pubDate>Mon, 14 Mar 2022 20:57:35 GMT</pubDate>
    <dc:creator>RichG</dc:creator>
    <dc:date>2022-03-14T20:57:35Z</dc:date>
    <item>
      <title>Model Voltage error when simulating i.MX8 QM LPDDR4 interface with Hyperlynx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Model-Voltage-error-when-simulating-i-MX8-QM-LPDDR4-interface/m-p/1427979#M188194</link>
      <description>&lt;P&gt;Hello. I have a design where I'm using the same LPDDR4 chips as the NXP eval board and in fact I have the same layout (pulled it in from the ODB++ files). It should work but I wanted to run a simulation to check. The models I'm using are:&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;i.MX8QM: imx8qm_29x29_rev1_25.ibs&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;MT53E768M32D4DT LPDDR4: z1am_200b-qdp_x32.ebd&lt;/P&gt;&lt;P&gt;The micron model within that ebd file is set to z1am_0p6V_st.ibs&lt;/P&gt;&lt;P&gt;When I set up the DDRx Batch Mode test in Hyperlynx, I get the following error:&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;There are nets with IBIS model voltage range compatibility issues:&lt;BR /&gt;Net(s): DDR_CH0_DM0..3, DDR_CH0_DQ0..31, DDR_CH1_DM0..3, DDR_CH1_DQ0..31&lt;BR /&gt;IBIS File: C:\Hyp\ADCMK5\Models\IMX8QM-IBIS\imx8qm_29x29_rev1_25.ibs&lt;BR /&gt;Selector/Model, Voltage: PDDRIO_PAD_DATA / DWC_D5MPL4_40 1.1V&lt;BR /&gt;Device(s): U1&lt;BR /&gt;IBIS File: C:\Hyp\ADCMK5\Models\MT53E768M32D4DT-053_ibis\z1am_0p6v_wt.ibs&lt;BR /&gt;Selector/Model, Voltage: DQ / DQ_PD40_ODT40_VOH50_4266 0.6V&lt;BR /&gt;Device(s): U0_EBD-U4, U2_EBD-U4&lt;/P&gt;&lt;P&gt;Am I trying to use the wrong models?&lt;/P&gt;&lt;P&gt;Thanks so much!&lt;/P&gt;&lt;P&gt;Rich&lt;/P&gt;</description>
      <pubDate>Mon, 14 Mar 2022 20:57:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Model-Voltage-error-when-simulating-i-MX8-QM-LPDDR4-interface/m-p/1427979#M188194</guid>
      <dc:creator>RichG</dc:creator>
      <dc:date>2022-03-14T20:57:35Z</dc:date>
    </item>
  </channel>
</rss>