<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Where to submit patch for linux-imx? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-submit-patch-for-linux-imx/m-p/1426217#M188068</link>
    <description>&lt;P&gt;you can post it here let us trying it and discuss , if good , nxp will take into nxt version?&lt;/P&gt;</description>
    <pubDate>Thu, 10 Mar 2022 14:34:51 GMT</pubDate>
    <dc:creator>josephzhou1</dc:creator>
    <dc:date>2022-03-10T14:34:51Z</dc:date>
    <item>
      <title>Where to submit patch for linux-imx?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-submit-patch-for-linux-imx/m-p/1426128#M188063</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have found a bug in the sdma driver: imx-sdma.c&lt;/P&gt;&lt;P&gt;Git repo: &lt;A href="https://source.codeaurora.org/external/imx/linux-imx.git" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/linux-imx.git&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Branch/tag: lf-5.10.72-2.2.0&lt;/P&gt;&lt;P&gt;I can't figure where to submit the patch? Could you help me please?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Mogens&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 12:18:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-to-submit-patch-for-linux-imx/m-p/1426128#M188063</guid>
      <dc:creator>mogenslauridsen</dc:creator>
      <dc:date>2022-03-10T12:18:12Z</dc:date>
    </item>
    <item>
      <title>Re: Where to submit patch for linux-imx?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-submit-patch-for-linux-imx/m-p/1426217#M188068</link>
      <description>&lt;P&gt;you can post it here let us trying it and discuss , if good , nxp will take into nxt version?&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 14:34:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-to-submit-patch-for-linux-imx/m-p/1426217#M188068</guid>
      <dc:creator>josephzhou1</dc:creator>
      <dc:date>2022-03-10T14:34:51Z</dc:date>
    </item>
    <item>
      <title>Re: Where to submit patch for linux-imx?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-submit-patch-for-linux-imx/m-p/1426224#M188069</link>
      <description>&lt;P&gt;Here is a description of the problem and the fix.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In the end of sdma_probe the driver is set "active" (autosuspend/resume), but it's actually not ready. sdma-&amp;gt;bp0 and clk isn't initialized and will only be initialized by sdma_runtime_resume (and sdma_request_channel0, which is called from sdma_runtime_resume). Since autosuspend has a timeout of 8000ms (pm_runtime_set_autosuspend_delay), sdma will be in a broken state from sdma driver load time and the next 8000ms. If sdma is used in this 8000ms time window, the kernel will panic. See below.&lt;BR /&gt;After that time window sdma_runtime_resume will be called when sdma is needed.&lt;/P&gt;&lt;P&gt;[ 6.548779] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000000&lt;BR /&gt;[ 6.557578] Mem abort info:&lt;BR /&gt;[ 6.560376] ESR = 0x96000044&lt;BR /&gt;[ 6.563444] EC = 0x25: DABT (current EL), IL = 32 bits&lt;BR /&gt;[ 6.568773] SET = 0, FnV = 0&lt;BR /&gt;[ 6.571845] EA = 0, S1PTW = 0&lt;BR /&gt;[ 6.574997] Data abort info:&lt;BR /&gt;[ 6.577892] ISV = 0, ISS = 0x00000044&lt;BR /&gt;[ 6.581728] CM = 0, WnR = 1&lt;BR /&gt;[ 6.584706] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000106246000&lt;BR /&gt;[ 6.591167] [0000000000000000] pgd=0000000000000000, p4d=0000000000000000&lt;BR /&gt;[ 6.597982] Internal error: Oops: 96000044 [#1] PREEMPT SMP&lt;BR /&gt;[ 6.603567] Modules linked in: g_ffs fsl_jr_uio caam_jr caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine rng_core authenc libdes crct10dif_ce tmp117 tmp103 ina2xx caam secvio error fuse&lt;BR /&gt;[ 6.620914] CPU: 3 PID: 450 Comm: b_audio_stream Not tainted 5.10.72-lts-5.10.y #3&lt;BR /&gt;[ 6.628492] Hardware name: NXP i.MX8MPlus Blackbird board (DT)&lt;BR /&gt;[ 6.634342] pstate: 80000085 (Nzcv daIf -PAN -UAO -TCO BTYPE=--)&lt;BR /&gt;[ 6.640357] pc : sdma_transfer_init+0x140/0x350&lt;BR /&gt;[ 6.644887] lr : sdma_transfer_init+0xf4/0x350&lt;BR /&gt;[ 6.649326] sp : ffff8000128b3ab0&lt;BR /&gt;[ 6.652640] x29: ffff8000128b3ab0 x28: 0000000000020002&lt;BR /&gt;[ 6.657954] x27: ffff0000c185c6a8 x26: ffff800011d2d200&lt;BR /&gt;[ 6.663270] x25: 0000000000000000 x24: 0000000000000002&lt;BR /&gt;[ 6.668582] x23: 0000000000000080 x22: 000000000000037d&lt;BR /&gt;[ 6.673894] x21: ffff0000c1858080 x20: ffff0000c6a0a100&lt;BR /&gt;[ 6.679205] x19: ffff0000c18584a8 x18: 0000000000000000&lt;BR /&gt;[ 6.684520] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[ 6.689830] x15: 0000000000000000 x14: 0000000000000000&lt;BR /&gt;[ 6.695140] x13: 0000000000000000 x12: 0000000000000000&lt;BR /&gt;[ 6.700452] x11: 0000000000000000 x10: 00000000ffffffff&lt;BR /&gt;[ 6.705765] x9 : 0000000000000000 x8 : ffff800011d2d280&lt;BR /&gt;[ 6.711075] x7 : 0000000000000000 x6 : 000000000000003f&lt;BR /&gt;[ 6.716387] x5 : 0000000000000040 x4 : 0000000000000000&lt;BR /&gt;[ 6.721699] x3 : 0000000000000004 x2 : 0000000000000040&lt;BR /&gt;[ 6.727023] x1 : 0000000000000000 x0 : 0000000001830020&lt;BR /&gt;[ 6.732343] Call trace:&lt;BR /&gt;[ 6.734793] sdma_transfer_init+0x140/0x350&lt;BR /&gt;[ 6.738975] sdma_prep_dma_cyclic+0x8c/0x340&lt;BR /&gt;[ 6.743248] snd_dmaengine_pcm_trigger+0xec/0x1c0&lt;BR /&gt;[ 6.747952] dmaengine_pcm_trigger+0x18/0x24&lt;BR /&gt;[ 6.752220] snd_soc_pcm_component_trigger+0x48/0xf0&lt;BR /&gt;[ 6.757184] soc_pcm_trigger+0xa8/0xd0&lt;BR /&gt;[ 6.760933] snd_pcm_do_start+0x38/0x44&lt;BR /&gt;[ 6.764767] snd_pcm_action_single+0x48/0xac&lt;BR /&gt;[ 6.769036] snd_pcm_action+0x7c/0x9c&lt;BR /&gt;[ 6.772698] snd_pcm_start+0x24/0x30&lt;BR /&gt;[ 6.776273] __snd_pcm_lib_xfer+0x694/0x7a0&lt;BR /&gt;[ 6.780456] snd_pcm_common_ioctl+0xf60/0x1220&lt;BR /&gt;[ 6.784898] snd_pcm_ioctl+0x34/0x50&lt;BR /&gt;[ 6.788474] __arm64_sys_ioctl+0xa8/0xf0&lt;BR /&gt;[ 6.792398] el0_svc_common.constprop.0+0x78/0x1c4&lt;BR /&gt;[ 6.797188] do_el0_svc+0x28/0x9c&lt;BR /&gt;[ 6.800503] el0_svc+0x14/0x20&lt;BR /&gt;[ 6.803556] el0_sync_handler+0xa4/0x130&lt;BR /&gt;[ 6.807479] el0_sync+0x180/0x1c0&lt;BR /&gt;[ 6.810797] Code: b9002740 52800400 531b6b02 72a03060 (b9000320)&lt;BR /&gt;[ 6.816895] ---[ end trace 738ced21fe29585e ]---&lt;BR /&gt;[ 6.821511] Kernel panic - not syncing: Oops: Fatal exception&lt;BR /&gt;[ 6.827255] SMP: stopping secondary CPUs&lt;BR /&gt;[ 6.831180] Kernel Offset: disabled&lt;BR /&gt;[ 6.834668] CPU features: 0x0240002,2000200c&lt;BR /&gt;[ 6.838935] Memory Limit: none&lt;BR /&gt;[ 6.841991] Rebooting in 1 seconds..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;+--- a/drivers/dma/imx-sdma.c&lt;BR /&gt;++++ b/drivers/dma/imx-sdma.c&lt;BR /&gt;+@@ -2610,7 +2610,6 @@ static int sdma_probe(struct platform_device *pdev)&lt;BR /&gt;+ pm_runtime_set_autosuspend_delay(&amp;amp;pdev-&amp;gt;dev, 8000);&lt;BR /&gt;+ pm_runtime_use_autosuspend(&amp;amp;pdev-&amp;gt;dev);&lt;BR /&gt;+ pm_runtime_mark_last_busy(&amp;amp;pdev-&amp;gt;dev);&lt;BR /&gt;+- pm_runtime_set_active(&amp;amp;pdev-&amp;gt;dev);&lt;BR /&gt;+ }&lt;BR /&gt;+&lt;BR /&gt;+ pm_runtime_enable(&amp;amp;pdev-&amp;gt;dev);&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Mogens&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 14:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-to-submit-patch-for-linux-imx/m-p/1426224#M188069</guid>
      <dc:creator>mogenslauridsen</dc:creator>
      <dc:date>2022-03-10T14:46:26Z</dc:date>
    </item>
  </channel>
</rss>