<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8M-Plus CSI1 maximum resolution in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CSI1-maximum-resolution/m-p/1425366#M188016</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;There are 2 CSI interfaces on the imx8mp: CSI0 and CSI1.&lt;/P&gt;&lt;P&gt;As you can see in the picture attached, the second imx8mp CSI interface (CSI1) runs with a 266Mhz pixel clock.&lt;/P&gt;&lt;P&gt;Does this have limitations in terms of maximum image resolution? So is it possible to transmit 4K@30fps images (3840x2160) on this CSI1?&lt;/P&gt;&lt;P&gt;The usage scenario: Use either CSI0 or CSI1 (only one at a time and stop the unused interface).&lt;/P&gt;&lt;P&gt;BR, MC&lt;/P&gt;</description>
    <pubDate>Wed, 09 Mar 2022 15:15:29 GMT</pubDate>
    <dc:creator>malik_cisse</dc:creator>
    <dc:date>2022-03-09T15:15:29Z</dc:date>
    <item>
      <title>i.MX8M-Plus CSI1 maximum resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CSI1-maximum-resolution/m-p/1425366#M188016</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;There are 2 CSI interfaces on the imx8mp: CSI0 and CSI1.&lt;/P&gt;&lt;P&gt;As you can see in the picture attached, the second imx8mp CSI interface (CSI1) runs with a 266Mhz pixel clock.&lt;/P&gt;&lt;P&gt;Does this have limitations in terms of maximum image resolution? So is it possible to transmit 4K@30fps images (3840x2160) on this CSI1?&lt;/P&gt;&lt;P&gt;The usage scenario: Use either CSI0 or CSI1 (only one at a time and stop the unused interface).&lt;/P&gt;&lt;P&gt;BR, MC&lt;/P&gt;</description>
      <pubDate>Wed, 09 Mar 2022 15:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CSI1-maximum-resolution/m-p/1425366#M188016</guid>
      <dc:creator>malik_cisse</dc:creator>
      <dc:date>2022-03-09T15:15:29Z</dc:date>
    </item>
  </channel>
</rss>